Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Unable to see the copper pour on the PAD though the thermels is off
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Answers 2 answers
  • Subscribers 189 subscribers
  • Views 2044 views
  • Users 0 members are here
  • eagle cad
  • eagle help
Related

Unable to see the copper pour on the PAD though the thermels is off

siddharthtaunk
siddharthtaunk over 9 years ago

Hi,

 

I am designing a power supply PCB I have a polygon covering the PAD of one of the ICs There are several small PADS and a big PAD. Now when polygon on the top of the small pads and have the thermals off I see that the polygon fills only the small PADS completely but there is a problem with the large PAD.

 

How do I resolve this.

Here is the picture for the same

 

 

Thanks and regards.

Siddharth

image

  • Sign in to reply
  • Cancel
Parents
  • niteowl12
    0 niteowl12 over 9 years ago

    Look at the Isolate setting on the polygon. I have had it set so high that it wont even make a connection to a pin.

     

    I would also check the layout of the pad itself. There is a check box for thermals there too.

     

    -Jason

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • siddharthtaunk
    0 siddharthtaunk over 9 years ago in reply to niteowl12

    Hi,

     

    Thanks for the response.

    I got the reason behind those polygons not filling the complete area near the PADS. the reason being the "Dimensions". Due to that dimensions lines It is only allowing the trace not the polygons to fill. How do I overcome from this?

     

    Thanks and regards.

    Siddharth

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • siddharthtaunk
    0 siddharthtaunk over 9 years ago in reply to niteowl12

    Hi,

     

    Thanks for the response.

    I got the reason behind those polygons not filling the complete area near the PADS. the reason being the "Dimensions". Due to that dimensions lines It is only allowing the trace not the polygons to fill. How do I overcome from this?

     

    Thanks and regards.

    Siddharth