Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) ratsnest does not create GND plane
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 2 answers
  • Subscribers 189 subscribers
  • Views 4282 views
  • Users 0 members are here
  • ratsnest
Related

ratsnest does not create GND plane

hennessey12
hennessey12 over 8 years ago

I am currently working on a board right now and I cannot make a GND plane. What am I supposed to do with the gnd terminals of the components of the board

Also, when I try to create a polygon and naming it GND it would still not create a gnd plane because when I click ratsnest it says there are airwires not connected so I connect the airwires using route then after I connected the GND terminals the ratsnest says there is nothing to do. Please help me!

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 8 years ago

    Am 24.04.2018 um 06:17 schrieb Hennessey Balbin:

    I am currently working on a board right now and I cannot make a GND plane. What am I supposed to do with the gnd terminals of the components of the board

    Also, when I try to create a polygon and naming it GND it would still not create a gnd plane because when I click ratsnest it says there are airwires not connected so I connect the airwires using route then after I connected the GND terminals the ratsnest says there is nothing to do. Please help me!

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/238741

     

     

    Route the GNDs together, don't let ratsnest do it. (After that you can

    use ratsnest)

    Name your polygon the same name GND.

    In case of multilayer board your GND polygon must be on the same layer

    with the other GND connections. Provide a via if necessary.

    Possibly use command:SET POLYGON_RATSNEST ON

    (or OFF) the same way as written in capital letters.

    (I have both commands on keys in the board layout.)

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • hennessey12
    0 hennessey12 over 8 years ago in reply to autodeskguest

    Thank you for helping but when I do it the resulting ground plane looks like this. see attached photo plsimage

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • hennessey12
    0 hennessey12 over 8 years ago in reply to autodeskguest

    Thank you for helping but when I do it the resulting ground plane looks like this. see attached photo plsimage

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • autodeskguest
    0 autodeskguest over 8 years ago in reply to hennessey12

    On 24/04/2018 7:06 p.m., Hennessey Balbin wrote:

    one more thing, that gnd plane appeared only when I checked orphan in polygon properties but if I do not check the orphan the plane won't appear.

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/238747

     

     

    For the fast answer to what is occurring

    Zip up the board file and attached it.

     

    Warren

     

    --

    ... use NNTP://news.cadsoft.de and a functional news reader like

    Thunderbird!

     

    ---

    This email has been checked for viruses by Avast antivirus software.

    https://www.avast.com/antivirus

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • hennessey12
    0 hennessey12 over 8 years ago in reply to autodeskguest

    one more thing, that gnd plane appeared only when I checked orphan in polygon properties but if I do not check the orphan the plane won't appear.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 8 years ago in reply to hennessey12

    On 24.04.2018 08:52, Hennessey Balbin wrote:

    Thank you for helping but when I do it the resulting ground plane looks like this. see attached photo pls

     

    Wow this looks weird. I suspect you have stuff at the hidden dimension

    layer? You can see the fill trying to keep an extreme distance to some

    features. If you try to find the center of those circular shapes, you

    should be able to track it down. Show all layers, and you will most

    likely see it.