EAGLE User Support (English) What is the right width of trace should I choose for 220VAC
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
  • State Suggested Answer
  • Replies 15 replies
  • Answers 10 answers
  • Subscribers 182 subscribers
  • Views 5240 views
  • Users 0 members are here
  • high voltage
  • trace-width
  • pcb trace
  • eagle 9.0.0
Related

What is the right width of trace should I choose for 220VAC

anthonylauly
anthonylauly over 7 years ago

image

Hi, I want to design a pcb that convert AC (220VAC) to DC (10 V), so I would use a wider trace for the Neutral and Line. First I would like to know what is the measurement unit use in the radius and width toolbox, second what is the difference of the radius and width of the trace, because when I increase the radius, nothing is happen. Third, what is the right number of radius and width for 220 VAC, thank you.

  • Sign in to reply
  • Cancel

Top Replies

  • autodeskguest
    autodeskguest over 7 years ago +7 suggested
    On 6/21/2018 7:15 AM, Anthony Lauly wrote: Hi, I want to design a pcb that convert AC (220VAC) to DC (10 V), so I would use a wider trace for the Neutral and Line. First I would like to know what is the…
  • rachaelp
    rachaelp over 7 years ago +7 suggested
    Hi Anthony, I'm going to start by a very strong word of caution. Please be extremely careful when working with mains voltages. If you don't know you can do something safely or are unsure in any way then…
  • jw0752
    jw0752 over 7 years ago in reply to anthonylauly +4 suggested
    Hi Anthony, I have copied your schematic and left off the regulator for simplification. If all you want is voltage the voltage divider works very well but if you want current it doesn't work well. Current…
  • anthonylauly
    0 anthonylauly over 7 years ago in reply to jw0752

    Yes sir, all I need is the voltage. theoritically I have considered that calculation though. But sir when I test it on breadboard that the output of the lm317 is connected to attiny85 its alll diferent. I only got around 8 to 12 V DC (I forgot the exact number). And I didn't got till 160 V DC. Do you think something wrong with the addition of attiny because the voltage drop is so big (although it is really helpul).

     

    Also sir, the calculation of the current, can I directly divide the output voltage of diode bridge with 110K Ohms without considering the 120 K Ohms ?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 7 years ago in reply to anthonylauly

    anthonylauly  wrote:

     

    If I have this kind of circuit  :

    image

    That what is the trace width should I use from the N and L that is connected to the diode bridge ? Because I cannot measure the current flow. The output for the diode bridge is 2 Ampere. Then what is the trace width should I choose ?

    Hi Anthony,

     

    Why do you say the output of the diode bridge is 2A? That will only be 2A if you are drawing 2A elsewhere which you cannot simply because of the circuit you have drawn. The absolute maximum current is limited by the series combination of R1 and R3 and as John quite rightly pointed out, the maximum current which would be flowing would be 2.8mA (actually less if you also consider the regulator).

     

    I'm assuming you probably really want a few tens or hundreds of mA at some lower voltage derived by some other regulator after this circuit as you mention an ATTiny so I am guessing you have some simple low voltage circuit there. Without knowing what you are actually wanting to power with this though it's hard to make accurate estimates.

     

    But, I really think you should do as John suggests and consider using a commercially available plug in power supply to give you your 10V output. What you have drawn above will not do what you appear to require.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 7 years ago in reply to anthonylauly

    anthonylauly  wrote:

     

    ...when I test it on breadboard... And I didn't got till 160 V DC...

    Anthony, are you building a mains connected device (in this case not isolated) on a breadboard?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 7 years ago in reply to anthonylauly

    On 24/06/2018 7:54 p.m., Anthony Lauly wrote:

    Yes sir, all I need is the voltage. theoritically I have considered that calculation though. But sir when I test it on breadboard that the output of the lm317 is connected to attiny85 its alll diferent. I only got around 8 to 12 V DC (I forgot the exact number). And I didn't got till 160 V DC. Do you think something wrong with the addition of attiny because the voltage drop is so big (although it is really helpul).

     

    Also sir, the calculation of the current, can I directly divide the output voltage of diode bridge with 110K Ohms without considering the 120 K Ohms ?

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/241355

     

     

    A few thoughts.

    This forum is for suggestions for the Eagle CAD program so this

    discussion is inappropriate here and should be on a basic electronics

    forum elsewhere.

     

    Your design is bad, dangerous and should not be continued with.

     

    John showed the input resistors limit the input current to 2.5mA and so

    the LM317 minimum input current needs have not been met and so the LM317

    cannot be expected to function correctly.

     

    If you read the data sheet for the LM317 you will see it can have a

    maximum of 40volts between input and output. You have subjected it to

    155volts so it may have been damaged. Any output voltage is likely to be

    the result of R5 in parallel with R2. You could confirm this by removing

    the LM317 and metering between  the IN and ADJ pins. I suspect you will

    find very low ohms. The LM317 is robust and contains a lot of protection

    circuitry so you may have been lucky but I would be surprised if it is

    still good.

     

    There is a technique where you can create a transformerless power supply

    but... it looks simple but requires a great understanding of all the

    factors involved. You may care to read articles on the subject.

    This one below is something to get you started on understanding the

    risks to yourself and the repercussions when components fail.

     

    https://hackaday.com/2017/04/04/the-shocking-truth-about-transformerless-power-supplies/

     

    Hope this helps

     

    Warren

     

    --

    ... use NNTP://news.cadsoft.de and a functional news reader like

    Thunderbird!

     

    ---

    This email has been checked for viruses by Avast antivirus software.

    https://www.avast.com/antivirus

     

     

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 7 years ago in reply to autodeskguest

    Hi Warren,

    Thanks for your good input. FYI these EAGLE questions also show up on the element 14 forum where we routinely answer nuts and bolts questions. Most of the times they are about CAD problems but sometimes, like this one, they demand a response.

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
<