Hi,
I have hired a contractor to do some eagle work for me as I'm not yet up to speed enough to meet a deadline. Anyway, so I'd still like to help and be involved in the process but I don't see how the two of us can work on the same file without creating a real mess. I can solve the shared access issue by granting him VPN to our file server, but I highly doubt that eagle will be too happy if we both are editing the file at the same time. THe only option I can think of is to use version control or a basic "Are you working right now? No? OK, then I will for awhile and will email you when I'm done" type approach.
Anyone here who works or has worked in a multiuser scenario have any tips for me?
Thanks for reading,
Steve