Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Shared access to schematic/project
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 2 answers
  • Subscribers 188 subscribers
  • Views 533 views
  • Users 0 members are here
  • eagle
  • question
Related

Shared access to schematic/project

e14 Contributor
e14 Contributor over 14 years ago

Hi,

 

I have hired a contractor to do some eagle work for me as I'm not yet up to speed enough to meet a deadline.  Anyway, so I'd still like to help and be involved in the process but I don't see how the two of us can work on the same file without creating a real mess.  I can solve the shared access issue by granting him VPN to our file server, but I highly doubt that eagle will be too happy if we both are editing the file at the same time.  THe only option I can think of is to use version control or a basic "Are you working right now?  No? OK, then I will for awhile and will email you when I'm done" type approach.

 

Anyone here who works or has worked in a multiuser scenario have any tips for me?

 

Thanks for reading,

Steve

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    On 9/2/11 12:41 AM, Steve Klett wrote:

    Hi,

     

    I have hired a contractor to do some eagle work for me as I'm not yet up to speed enough to meet a deadline.  Anyway, so I'd still like to help and be involved in the process but I don't see how the two of us can work on the same file without creating a real mess.  I can solve the shared access issue by granting him VPN to our file server, but I highly doubt that eagle will be too happy if we both are editing the file at the same time.  THe only option I can think of is to use version control or a basic "Are you working right now?  No? OK, then I will for awhile and will email you when I'm done" type approach.

     

    Anyone here who works or has worked in a multiuser scenario have any tips for me?

     

    Frankly, my tip is to let your contractor do all the work image

     

    If you want to help and be involved, ask to review the work and make

    comments on it by e-mail but do not modify the files.

     

    Schematics/PCB's require a certain "mental picture" to be formed by the

    designer, and if someone else modifies things the mental picture starts

    to break down and mistakes or oversights occur. Unless, that is, you can

    split up the work into well-defined parts of minimal interaction.

     

    As a contractor that does Eagle work, I much prefer "owning" the files

    until the design is done and not having changes made on me by the client.

     

     

    Thanks for reading,

    Steve

     

     

    Andrew.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    I think your advice is very sound and I know exactly what you mean about the mental plan.  Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    I think your advice is very sound and I know exactly what you mean about the mental plan.  Thanks