Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) USB routing problems : D+/- length issues
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 30 replies
  • Answers 2 answers
  • Subscribers 191 subscribers
  • Views 3542 views
  • Users 0 members are here
  • length
  • d-
  • autorouter
  • usb
  • parallelism
  • d+
Related

USB routing problems : D+/- length issues

e14 Contributor
e14 Contributor over 14 years ago

Hello everyone

 

I'm a user of Eagle for 2 years now, and i'm trying to make USB with an Overo and a dsPIC.

The thing is that I had read somewhere (http://www.usb.org/developers/docs/hs_usb_pdg_r1_0.pdf) that the signals D+ and D- must have the same length (they talk about non parallelism page 10 figure 5)

 

But here is the point : how you do that on Eagle , to force 2 wire to have the same length (or being parallel all the way), in autorouter mode of course but even in manual mode.

 

Thanks for the help .

 

Best Regards

  • Sign in to reply
  • Cancel
  • kcadsoft
    0 kcadsoft over 14 years ago in reply to e14 Contributor

    On 23.09.2011 15:47, Morten Leikvoll wrote:

    "Klaus Schmidinger"<Klaus.Schmidinger@cadsoft.de>  wrote in message

    news:j5hdh5$va6$1@cheetah.cadsoft.de...

    >> In V6 the (manual) ROUTE command will treat signals that have the

    >> same net class and the same name (one ending with '+' and the other

    >> with '-') as "differential pairs". When picking up one airwire of such

    >> a pair, both signals will be routed in parallel, keeping the distance

    >> as defined in the net class.

     

    You should be a bit careful about using the + and - signs. It works as long

    as you dont export netfiles to other tools, but + and - in names are often a

    source of confusion and problems. As an example, we export netnames

    connected to FPGA's and feed them into the pin assignment files. That tool

    will not allow + and - and simply replacing it with something else is a

    potential source of conflict.

     

    We could just as well use something more exotic, like "_P" and "_N".

     

    Klaus Schmidinger

    --

    _______________________________________________________________

     

    Klaus Schmidinger                       Phone: +49-8635-6989-10

    CadSoft Computer GmbH                   Fax:   +49-8635-6989-40

    Pleidolfweg 15                          Email:   kls@cadsoft.de

    D-84568 Pleiskirchen, Germany           URL:     www.cadsoft.de

    _______________________________________________________________

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kcadsoft
    0 kcadsoft over 14 years ago in reply to e14 Contributor

    On 23.09.2011 16:31, Olin Lathrop wrote:

    Klaus Schmidinger wrote on Fri, 23 September 2011 03:46

    >> In V6 the (manual) ROUTE command will treat signals that have the

    >> same net class and the same name (one ending with '+' and the other

    >> with '-') as "differential pairs". When picking up one airwire of such

    >> a pair, both signals will be routed in parallel, keeping the distance

    >> as defined in the net class.

    >

    It's good that you are adding the capbility to keep traces together, but

    this should not be driven from the net names.  Automatic features like that

    may seem like they are saving time, but in the long run always cause

    trouble.  If two signals are to be routed together, I want to tell Eagle

    that explicitly and never have it think it knows somehow on its own.  For

    example, I have some existing designs with signal names D+ and D-, but I

    don't necessarily want them routed together.

     

    Within the existing Eagle framework, it's probably best if this were a

    property of net classes.  When this property is set, then all signals in

    the class will be routed together.  It's up to me to explicitly put such

    signals in their own net class and then enable the property.  Please,

    nothing automatic.

     

    That would mean you need one net class for each differential pair.

    Not very practical.

     

    There has to be some way of identifying which two signals form

    a differential pair, and that's going to be via the signal names.

    We can discuss which way this is done, so if '+' and '-' appear

    inappropriate, we could use "_P" and "_N".

     

    Klaus Schmidinger

    --

    _______________________________________________________________

     

    Klaus Schmidinger                       Phone: +49-8635-6989-10

    CadSoft Computer GmbH                   Fax:   +49-8635-6989-40

    Pleidolfweg 15                          Email:   kls@cadsoft.de

    D-84568 Pleiskirchen, Germany           URL:     www.cadsoft.de

    _______________________________________________________________

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    (for some reason my phone nntp reader doesnt quote some msgs)

    I think a simple external list of complementary(diff) or grouped(buses)

    netnames would handle this issue nicely. It does not have to be tied to any

    objects.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to kcadsoft

    Klaus Schmidinger wrote on Fri, 23 September 2011 03:46

    In V6 the (manual) ROUTE command will treat signals that have the

    same net class and the same name (one ending with '+' and the other

    with '-') as "differential pairs". When picking up one airwire of such

    a pair, both signals will be routed in parallel, keeping the distance

    as defined in the net class.

     

     

    It's good that you are adding the capbility to keep traces together, but

    this should not be driven from the net names.  Automatic features like that

    may seem like they are saving time, but in the long run always cause

    trouble.  If two signals are to be routed together, I want to tell Eagle

    that explicitly and never have it think it knows somehow on its own.  For

    example, I have some existing designs with signal names D+ and D-, but I

    don't necessarily want them routed together.

     

    Within the existing Eagle framework, it's probably best if this were a

    property of net classes.  When this property is set, then all signals in

    the class will be routed together.  It's up to me to explicitly put such

    signals in their own net class and then enable the property.  Please,

    nothing automatic.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to kcadsoft

    Klaus Schmidinger wrote on Fri, 23 September 2011 03:46

    This can't guarantee the same length for both signals, so there

    will also be a new command that generates "meanders" to compensate

    for length differences, or to create a fixed total length of a

    differential pair.

     

     

    Klaus, will this new command that adds "meanders" be able to take a list of

    signals, not just a diff pair?  If so, it could be used to equalize trace

    lengths across a bus like DDR, DDR2,  etc.

     

    You may also want to make sure you add parameters for the tolerance allowed

    for difference in lengths, both longer and shorter.  Once it's good enough

    then the function can stop, where "good enough" is a parameter to the

    command.

     

    Cheers,

     

    James.

    --

    James Morrison  ~~~  Stratford Digital

     

    Specializing in CadSoft EAGLE

    • Online Sales to North America

    • Electronic Design Services

    • EAGLE Enterprise Toolkit

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to kcadsoft

    "Klaus Schmidinger" <Klaus.Schmidinger@cadsoft.de> wrote in message

    news:j5hdh5$va6$1@cheetah.cadsoft.de...

    In V6 the (manual) ROUTE command will treat signals that have the

    same net class and the same name (one ending with '+' and the other

    with '-') as "differential pairs". When picking up one airwire of such

    a pair, both signals will be routed in parallel, keeping the distance

    as defined in the net class.

     

    You should be a bit careful about using the + and - signs. It works as long

    as you dont export netfiles to other tools, but + and - in names are often a

    source of confusion and problems. As an example, we export netnames

    connected to FPGA's and feed them into the pin assignment files. That tool

    will not allow + and - and simply replacing it with something else is a

    potential source of conflict.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kcadsoft
    0 kcadsoft over 14 years ago in reply to e14 Contributor

    On 09/23/11 12:12, Christian Bohrer wrote:

    "Klaus Schmidinger"<Klaus.Schmidinger@cadsoft.de>  a écrit dans le message de news:

    j5hdh5$va6$1@cheetah.cadsoft.de...

    >> On 09/23/11 08:08, Tilmann Reh wrote:

    >>> ...

    >>> In EAGLE, there is no way to /force/ an equally long differential pair

    >>> during routing, neither manually nor by autorouter. Maybe V6 will add

    >>> something new here, but I don't know.

    >>

    >> In V6 the (manual) ROUTE command will treat signals that have the

    >> same net class and the same name (one ending with '+' and the other

    >> with '-') as "differential pairs". When picking up one airwire of such

    >> a pair, both signals will be routed in parallel, keeping the distance

    >> as defined in the net class.

     

    does that mean there will be more than 7 net classes?

     

    We were thinking about increasing this number to 16.

     

    Klaus Schmidinger

    --

    _______________________________________________________________

     

    Klaus Schmidinger                       Phone: +49-8635-6989-10

    CadSoft Computer GmbH                   Fax:   +49-8635-6989-40

    Pleidolfweg 15                          Email:   kls@cadsoft.de

    D-84568 Pleiskirchen, Germany           URL:     www.cadsoft.de

    _______________________________________________________________

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to kcadsoft

     

    "Klaus Schmidinger" <Klaus.Schmidinger@cadsoft.de> a écrit dans le message de news:

    j5hdh5$va6$1@cheetah.cadsoft.de...

    On 09/23/11 08:08, Tilmann Reh wrote:

    >> ...

    >> In EAGLE, there is no way to /force/ an equally long differential pair

    >> during routing, neither manually nor by autorouter. Maybe V6 will add

    >> something new here, but I don't know.

     

    In V6 the (manual) ROUTE command will treat signals that have the

    same net class and the same name (one ending with '+' and the other

    with '-') as "differential pairs". When picking up one airwire of such

    a pair, both signals will be routed in parallel, keeping the distance

    as defined in the net class.

     

    does that mean there will be more than 7 net classes?

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kcadsoft
    0 kcadsoft over 14 years ago in reply to e14 Contributor

    On 09/23/11 08:08, Tilmann Reh wrote:

    ...

    In EAGLE, there is no way to /force/ an equally long differential pair

    during routing, neither manually nor by autorouter. Maybe V6 will add

    something new here, but I don't know.

     

    In V6 the (manual) ROUTE command will treat signals that have the

    same net class and the same name (one ending with '+' and the other

    with '-') as "differential pairs". When picking up one airwire of such

    a pair, both signals will be routed in parallel, keeping the distance

    as defined in the net class.

     

    This can't guarantee the same length for both signals, so there

    will also be a new command that generates "meanders" to compensate

    for length differences, or to create a fixed total length of a

    differential pair.

     

    Klaus Schmidinger

    --

    _______________________________________________________________

     

    Klaus Schmidinger                       Phone: +49-8635-6989-10

    CadSoft Computer GmbH                   Fax:   +49-8635-6989-40

    Pleidolfweg 15                          Email:   kls@cadsoft.de

    D-84568 Pleiskirchen, Germany           URL:     www.cadsoft.de

    _______________________________________________________________

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Vincent Vittori schrieb:

     

    I'm a user of Eagle for 2 years now, and i'm trying to make USB with

    an Overo and a dsPIC. The thing is that I had read somewhere

    (http://www.usb.org/developers/docs/hs_usb_pdg_r1_0.pdf) that the

    signals D+ and D- must have the same length (they talk about non

    parallelism page 10 figure 5)

     

    But here is the point : how you do that on Eagle , to force 2 wire to

    have the same length (or being parallel all the way), in autorouter

    mode of course but even in manual mode.

     

    First of all, I would never use the autorouter for this. (I don't use it

    at all... but here it's essential.)

     

    Then, simply (manually) route your tracks as parallel as possible. You

    can check their length with an ULP and correct them if necessary.

     

    In EAGLE, there is no way to /force/ an equally long differential pair

    during routing, neither manually nor by autorouter. Maybe V6 will add

    something new here, but I don't know.

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
<