Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) USB routing problems : D+/- length issues
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 30 replies
  • Answers 2 answers
  • Subscribers 191 subscribers
  • Views 3528 views
  • Users 0 members are here
  • length
  • d-
  • autorouter
  • usb
  • parallelism
  • d+
Related

USB routing problems : D+/- length issues

e14 Contributor
e14 Contributor over 14 years ago

Hello everyone

 

I'm a user of Eagle for 2 years now, and i'm trying to make USB with an Overo and a dsPIC.

The thing is that I had read somewhere (http://www.usb.org/developers/docs/hs_usb_pdg_r1_0.pdf) that the signals D+ and D- must have the same length (they talk about non parallelism page 10 figure 5)

 

But here is the point : how you do that on Eagle , to force 2 wire to have the same length (or being parallel all the way), in autorouter mode of course but even in manual mode.

 

Thanks for the help .

 

Best Regards

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to kcadsoft

    Klaus Schmidinger wrote on Sat, 24 September 2011 05:04

    And what about whole busses that should be routed together?

     

    The differential pair feature we are currently implementing is

    only about two signals being routed in parallel.

     

     

    I think this is the crux of the debate here.  From what I've read (and

    posted), many of us are trying to extend this tool to match length across

    signals on a bus.  Also, there appears to be two tools that Klaus is

    discussing:  differential pair routing and automatic length matching.  As

    we haven't see the beta none of us outsiders have seen how this is

    implemented and how tightly the two tools are tied together.

     

    So I would say, that even though you aren't intending to allow length

    matching across a bus you should allow a way to specify signals in a diff

    pair that is scalable to an entire bus.  This way you could (and should)

    expand the function in the future.

     

    This way, it will also make sure they don't get implemented in such a way

    as it won't be extendable in the future.  The diff pair routing tool and

    the bus length matching tool should be independent tools, in my opinion.

     

    With these criteria in mind, I don't think identifying them via signal name

    makes sense.

     

    I would prefer to make this a bus property and say that diff pairs need to

    defined as their own bus.  You can unlimited number of busses (unlike net

    classes).  This also expands nicely to trace length matching across a bus.

    Maybe you have a bus flag called "differential" that you set to trigger the

    diff pair routing.

     

    Also note, I don't want the tool to just start routing things it thinks

    are differential.  I should have to explicitly tell it that the two signals

    are differential. This bus methodology above respects that.

     

    Cheers,

     

    James.

    --

    James Morrison  ~~~  Stratford Digital

     

    Specializing in CadSoft EAGLE

    • Online Sales to North America

    • Electronic Design Services

    • EAGLE Enterprise Toolkit

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to Johann.Glaser@gmx.at

    Johann Glaser <Johann.Glaser@gmx.at> wrote:

    Hi!

     

    Am Freitag, den 23.09.2011, 18:24 +0200 schrieb Klaus Schmidinger:

    >> On 23.09.2011 15:47, Morten Leikvoll wrote:

    >>> "Klaus Schmidinger"<Klaus.Schmidinger@cadsoft.de>  wrote in message

    >>> news:j5hdh5$va6$1@cheetah.cadsoft.de...

    >>>> In V6 the (manual) ROUTE command will treat signals that have the

    >>>> same net class and the same name (one ending with '+' and the other

    >>>> with '-') as "differential pairs". When picking up one airwire of such

    >>>> a pair, both signals will be routed in parallel, keeping the distance

    >>>> as defined in the net class.

    >>>

    >>> You should be a bit careful about using the + and - signs. It works as long

    >>> as you dont export netfiles to other tools, but + and - in names are often a

    >>> source of confusion and problems. As an example, we export netnames

    >>> connected to FPGA's and feed them into the pin assignment files. That tool

    >>> will not allow + and - and simply replacing it with something else is a

    >>> potential source of conflict.

    >>

    >> We could just as well use something more exotic, like "_P" and "_N".

     

    I second the thoughts on the '+' and '-' chars in names.

     

    As you have written, you don't like to add another kind of a setting to

    specify which signals belong together, we might only have the naming.

     

    What do you think of making the naming configurable? The default could

    be:

    - '-' / '+'

    - '_n' / '_p'

    (both, but only within its little groups). But this should be possible

    to change with a dialog or "set" command. If somebody wants signals with

    that name ending, but not have them routed together, just remove the

    setting for that schematic/board. If somebody wants special name endings

    for differential pairs, e.g. '_PLUS' and '_MINUS', he simply sets it

    accordingly.

     

    So it would be nice to have zero to "a few" pair name ends to be setup.

     

    You also have to consider that its not always practical to have this in the

    suffix. A prefix is just as logical. Also somewhere in the middle. Think

    for example an lvds BUS where you want an numeric index as prefix.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to kcadsoft

    On 9/24/11 5:18 AM, Klaus Schmidinger wrote:

    I don't like this.

    The fact that two signals are paired has to be a property of these

    two signals, and the easiest and most straight forward way to

    do it is through their names, since each signal must have a way

    of knowing its "companion".

    >

    Klaus Schmidinger

     

    I don't like this because it reuses one feature for a different purpose.

    Think about how the 'static' keyword in the C/C++ programming languages

    has so many different uses (to mark functions, variables, class

    variables, etc.) It is confusing.

     

    This is my preferred interface:

     

    • In the Edit menu there is an item called "Differential Pairs"

    • The item presents a list of differential pairs, which have ARBITRARY

    names.

    • There is an ADD button which lets you select any two nets in the

    existing design (sorted by name) to be considered differential

    • There is an EDIT button which lets you set the property of this

    differential pair (spacing, line width, layer(s) that are allowed for

    routing, maximum trace length mismatch for DRC, etc.)

    • There is a DELETE button

     

    That's it. It has no relationship to net classes, it has no relationship

    to net names. It is simply one place on one menu that COMPLETELY

    configures differential pairs and does not rely on any implicit/implied

    things like names or net classes.

     

    Andrew.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to kcadsoft

    Klaus Schmidinger wrote on Sat, 24 September 2011 05:04

    Net classes have a parameter that defines the minimum distance

    between either two of them, which results in a (triangular)

    matrix. That matrix would become rather bulky with a large

    number of net classes.

     

    I see, it's a squared problem.  I agree, net classes isn't how to define

    this then.

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • KE5FX
    0 KE5FX over 14 years ago in reply to Johann.Glaser@gmx.at

    Would it be reasonable to make this a bus property, rather than a property of net classes or of individual signals?  As long as you allow nets to be part of more than one logical bus, it's not a big hardship to require users to associate a bus with signals that need to be routed for minimal timing skew.

     

    Using bus notation would permit groups of more than two signals to be routed for equal length, which IMHO is required for this feature to be of any real use.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Johann.Glaser@gmx.at
    0 Johann.Glaser@gmx.at over 14 years ago in reply to kcadsoft

    Hi!

     

    Am Freitag, den 23.09.2011, 18:24 +0200 schrieb Klaus Schmidinger:

    On 23.09.2011 15:47, Morten Leikvoll wrote:

    "Klaus Schmidinger"<Klaus.Schmidinger@cadsoft.de>  wrote in message

    news:j5hdh5$va6$1@cheetah.cadsoft.de...

    >> In V6 the (manual) ROUTE command will treat signals that have the

    >> same net class and the same name (one ending with '+' and the other

    >> with '-') as "differential pairs". When picking up one airwire of such

    >> a pair, both signals will be routed in parallel, keeping the distance

    >> as defined in the net class.

     

    You should be a bit careful about using the + and - signs. It works as long

    as you dont export netfiles to other tools, but + and - in names are often a

    source of confusion and problems. As an example, we export netnames

    connected to FPGA's and feed them into the pin assignment files. That tool

    will not allow + and - and simply replacing it with something else is a

    potential source of conflict.

     

    We could just as well use something more exotic, like "_P" and "_N".

     

    I second the thoughts on the '+' and '-' chars in names.

     

    As you have written, you don't like to add another kind of a setting to

    specify which signals belong together, we might only have the naming.

     

    What do you think of making the naming configurable? The default could

    be:

    - '-' / '+'

    - '_n' / '_p'

    (both, but only within its little groups). But this should be possible

    to change with a dialog or "set" command. If somebody wants signals with

    that name ending, but not have them routed together, just remove the

    setting for that schematic/board. If somebody wants special name endings

    for differential pairs, e.g. '_PLUS' and '_MINUS', he simply sets it

    accordingly.

     

    So it would be nice to have zero to "a few" pair name ends to be setup.

     

    Thanks

      Hansi

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kcadsoft
    0 kcadsoft over 14 years ago in reply to e14 Contributor

    On 23.09.2011 21:27, Warren Brayshaw wrote:

    Klaus Schmidinger wrote:

     

    >>

    >> There has to be some way of identifying which two signals form

    >> a differential pair, and that's going to be via the signal names.

    >> We can discuss which way this is done, so if '+' and '-' appear

    >> inappropriate, we could use "_P" and "_N".

    >>

    >

    As the feature is only for manual routing I would favour a 'gather' command

    in which you specify the pair/pairs

    This could work a number of ways but something like an alias list. You would

    store the signal name pairs in this list and whenever you start to route a

    signal the list is consulted to determine if another signal must be routed.

    Using this method, signal names are irrelevant and negate the need for + -

    _P _N

     

    This list of pairings would need to be stored in the board file

     

    I don't like this.

    The fact that two signals are paired has to be a property of these

    two signals, and the easiest and most straight forward way to

    do it is through their names, since each signal must have a way

    of knowing its "companion".

     

    It would be the simplest method to just use a certain naming convention,

    like '+'/'-' or "_P"/"_N", but if you're afraid this might clash with

    existing projects, we could add a flag to each signal that makes it

    "part of a differential pair". However, this still would mean that the two

    signals forming the differential pair would have to follow a naming

    convention in order to be identified as a pair.

    I'd like to avoid this flag, though, because it makes things unnecessarily

    complex.

     

    Klaus Schmidinger

    --

    _______________________________________________________________

     

    Klaus Schmidinger                       Phone: +49-8635-6989-10

    CadSoft Computer GmbH                   Fax:   +49-8635-6989-40

    Pleidolfweg 15                          Email:   kls@cadsoft.de

    D-84568 Pleiskirchen, Germany           URL:     www.cadsoft.de

    _______________________________________________________________

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kcadsoft
    0 kcadsoft over 14 years ago in reply to e14 Contributor

    On 24.09.2011 00:42, Olin Lathrop wrote:

    Klaus Schmidinger wrote on Fri, 23 September 2011 12:24

    >> That would mean you need one net class for each differential pair.  Not

    >> very practical.

     

    Why?  Does the existance of a new class have a high cost?  Is there some

    reason not to make lots of them?

     

    Net classes have a parameter that defines the minimum distance

    between either two of them, which results in a (triangular)

    matrix. That matrix would become rather bulky with a large

    number of net classes.

     

    Besides, how many differential pairs do

    you envision needing?  Currently I use maybe 4 or 5 net classes at most.

    There seem to be a lot more than I need already.

     

    I don't know how many differential pairs any future layout

    might need. But if we made it so that each and every such pair

    would need its very own net class, that would be the wrong way

    to go.

     

    And what about whole busses that should be routed together?

     

    The differential pair feature we are currently implementing is

    only about two signals being routed in parallel.

     

    Klaus Schmidinger

    --

    _______________________________________________________________

     

    Klaus Schmidinger                       Phone: +49-8635-6989-10

    CadSoft Computer GmbH                   Fax:   +49-8635-6989-40

    Pleidolfweg 15                          Email:   kls@cadsoft.de

    D-84568 Pleiskirchen, Germany           URL:     www.cadsoft.de

    _______________________________________________________________

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to kcadsoft

    Klaus Schmidinger wrote on Fri, 23 September 2011 12:24

    That would mean you need one net class for each differential pair.  Not

    very practical.

     

    Why?  Does the existance of a new class have a high cost?  Is there some

    reason not to make lots of them?  Besides, how many differential pairs do

    you envision needing?  Currently I use maybe 4 or 5 net classes at most.

    There seem to be a lot more than I need already.

     

    And what about whole busses that should be routed together?

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to kcadsoft

    Klaus Schmidinger wrote:

     

     

    There has to be some way of identifying which two signals form

    a differential pair, and that's going to be via the signal names.

    We can discuss which way this is done, so if '+' and '-' appear

    inappropriate, we could use "_P" and "_N".

     

     

    As the feature is only for manual routing I would favour a 'gather' command

    in which you specify the pair/pairs

    This could work a number of ways but something like an alias list. You would

    store the signal name pairs in this list and whenever you start to route a

    signal the list is consulted to determine if another signal must be routed.

    Using this method, signal names are irrelevant and negate the need for + -

    _P _N

     

    This list of pairings would need to be stored in the board file

     

    Warren

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<>