Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) I'm confused about adding NETS
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 10 replies
  • Subscribers 188 subscribers
  • Views 936 views
  • Users 0 members are here
Related

I'm confused about adding NETS

e14 Contributor
e14 Contributor over 14 years ago

I'm confused, should I be using the Wire command to connect components in the schematic or using the Net command. One tutorial says use wire, another says use net. I tried a small schematic using both and then converted the schematic to a board and all wire showed up. I guess I don't understand the difference. Any help would sure be appreciated because I think i am trying to make this more difficult that it should be.

Thanks,

 

Jeff

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Element 14 User wrote on Mon, 10 October 2011 20:58

    I'm confused, should I be using the Wire command to connect components

    in the schematic or using the Net command.

     

    Always use NET to make schematic connections.

     

    The command names in Eagle are perfectly logical.  WIRE is used to draw

    lines except when they respresent wires, then you use NET.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    I'm also learning - I understand the explanation and agree that for

    electrical connections NET is more convenient with "Auto End" and "dot on

    junctions" but at the end of the project is there does not appear to be any

    electrical difference in fact if I draw a new wire by itself then another

    wire to connect into an existing NET it gives the option of using the new

    Net$ name or adopt the name of the N$n to which we are connecting.

     

    So in summary it would appear that if I had earlier in a project used wire

    then I don't need to go back & redraw as long as the N$n ar correctly

    connected.

     

    Well that it how I see it and welcome comment.

     

    This was an excellent question to be raised in the first place.

     

    --

    Regards

     

    Ray B

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    I'm also learning - I understand the explanation and agree that for

    electrical connections NET is more convenient with "Auto End" and "dot on

    junctions" but at the end of the project is there does not appear to be any

    electrical difference in fact if I draw a new wire by itself then another

    wire to connect into an existing NET it gives the option of using the new

    Net$ name or adopt the name of the N$n to which we are connecting.

     

    So in summary it would appear that if I had earlier in a project used wire

    then I don't need to go back & redraw as long as the N$n ar correctly

    connected.

     

    Well that it how I see it and welcome comment.

     

    This was an excellent question to be raised in the first place.

     

    --

    Regards

     

    Ray B

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.