Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Additional import and export features
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 188 subscribers
  • Views 918 views
  • Users 0 members are here
  • cad
  • features
Related

Additional import and export features

e14 Contributor
e14 Contributor over 14 years ago

I badly need 2 items.

 

1.  An import function into librarys that can provide the mechanical structure for components.  Ideally, something like a DXF.importer into the

dimension layer.  Components that have mechanical features in addition to the basic part connection pads need a lot of effort to create.  This

is usually a duplicate effort from a mechanical design done outside of Eagle.

 

2. An export function other than pixels out of the board layout.  Again, ideally DXF.  This would allow more precice integration of the finished

board into exernal CAD programs (That board has to go live someplace after it is done).  Currently I have to do a hack and plot out into HPGL,

then convert it to DXF.  This is imprecise and requires clean-up of the DXF to get critical dimensions correct.

 

Any recommendations?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    On 26.01.2012 01:32, Joe Mickley wrote:

      I badly need 2 items.

     

    1.  An import function into librarys that can provide the mechanical structure for components.  Ideally, something like a DXF.importer into the

    dimension layer.  Components that have mechanical features in addition to the basic part connection pads need a lot of effort to create.  This

    is usually a duplicate effort from a mechanical design done outside of Eagle.

     

     

    There are some tools that allow conversion from DXF to EAGLE script.

    ==> http://www.cadsoft.de/downloads/tools-and-converters

     

    for example

      dxf2scr-1.zip  (for free)

      eagle_pcb_power_tools*.exe

     

     

     

    2. An export function other than pixels out of the board layout.  Again, ideally DXF.  This would allow more precice integration of the finished

    board into exernal CAD programs (That board has to go live someplace after it is done).  Currently I have to do a hack and plot out into HPGL,

    then convert it to DXF.  This is imprecise and requires clean-up of the DXF to get critical dimensions correct.

     

    Any recommendations?

     

     

    Use DXF.ULP.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Am 26.01.2012 16:33, schrieb Richard Hammerl:

    Use DXF.ULP.

     

    The question about DXF output has been asked twelve billion times, and a

    lot of users surely don't know that EAGLE can do a thing like that. And

    why is that so? Because the DXF output is NOT available via the GUI.

    Every user searches for a function like that

      - in the 'save' or 'save as' dialogs and

      - in the 'export' function (that's where it belongs).

    DXF is nowhere mentioned -> Conclusion: EAGLE cannot do that.

     

    For the DXF import, I can understand that CadSoft doesn't want to

    program this, since it's quite some work. But for the DXF output: This

    already HAS been programmed, so why not put it into the program proper

    and make it available with the EXPORT command? Doing things with

    external ULPs is something that the typical user doesn't want to fiddle

    around with ('programming? aargh - I cannot do that!'). And why should

    one be able to export to a bitmap with EXPORT in the first place, but

    not to DXF? This doesn't seem a logical choice. Better to make it clear

    and logical and nice and wonderful and let the user FIND that function

    easily...

     

    Andreas Weidner

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Andreas Weidner wrote on Thu, 26 January 2012 11:30

    Am 26.01.2012 16:33, schrieb Richard Hammerl:

    Use DXF.ULP.

     

    The question about DXF output has been asked twelve billion times, and

    a

    lot of users surely don't know that EAGLE can do a thing like that. And

     

    why is that so? Because the DXF output is NOT available via the GUI.

    Every user searches for a function like that

      - in the 'save' or 'save as' dialogs and

      - in the 'export' function (that's where it belongs).

    DXF is nowhere mentioned -> Conclusion: EAGLE cannot do that.

     

    For the DXF import, I can understand that CadSoft doesn't want to

    program this, since it's quite some work. But for the DXF output: This

     

    already HAS been programmed, so why not put it into the program proper

     

    and make it available with the EXPORT command? Doing things with

    external ULPs is something that the typical user doesn't want to fiddle

     

    around with ('programming? aargh - I cannot do that!'). And why should

     

    one be able to export to a bitmap with EXPORT in the first place, but

    not to DXF? This doesn't seem a logical choice. Better to make it clear

     

    and logical and nice and wonderful and let the user FIND that function

     

    easily...

     

     

    Hello Andreas,

     

    In general, I agree with your analysis.  It's further complicated with the

    "Save As..." option which really can only save with a new name, not any

    other formats.  And then you have the CAM processor which also exports

    data.

     

    I would propose the following:

     

    1)  Rename "Save As" as "Rename Design Files".  There are no options for

    other formats which Save As often implies.  Plus, in SCH and PCB you rename

    both files at the same time which isn't obvious either.

     

    2)  Define a standard interface for ULP's that export design information

    into different formats.  That way each exporting utility can use the same

    interface (see below).  It will need to be dynamic and flexible but should

    be able to be done.

     

    3)  Create a sub-folder "export" in the ULP directory which EAGLE looks

    for.  This should look in the first "export" folder in the ULP path so I

    can create my own.  Or maybe looks in all folders, but then you have to

    decide what to do with ULP's with the same name.  Either way, it should be

    obvious and flexible.

     

    4)  Extend the export current dialog (if you can call it that) when you

    click on File->Export to be a full dialog.  When the export dialog is

    created it can search through that folder and pre-populate the list of

    available exporting options.  By selecting the one you want all the various

    options are presented.

     

    5)  Provide hooks for the CAM processor to be one of the exporting methods

    so it is handled like every other exporting ULP.

     

    With this, it would also be relatively easy to create one button to export

    all required manufacturing data (gerbers, bom, xy data, dxf of outline,

    ..) which is greatly needed.

     

    Now this won't be trivial and will take some thought to do it correctly.

    The interface to an exporting ULP would need to be published so anyone can

    create their own.  I'd suggest a similar interface for importing ULP's as

    well.

     

    It would provide a method for the user to easily add exporting ULP's

    without having to do anything different (other than copy a file to a

    particular place).  The GUI would take care of the rest.

     

    Cheers,

     

    James.

     

     

     

     

    --

    James Morrison  ~~~  Stratford Digital

     

    Specializing in CadSoft EAGLE

    • Online Sales to North America

    • Electronic Design Services

    • EAGLE Enterprise Toolkit

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Am 27.01.2012 00:40, schrieb Warren Brayshaw:

    Then the user selects a conversion type. What happens next depends on how

    this functionality is ultimately implemented.

    1) The ULP could simply run.

     

    The idea of providing a complete programming interface for exports is

    nice, but it is QUITE some work to implement such a thing, and I think

    CadSoft has enough things to do at the moment. Additionally, the GUI

    necessities for every export are DIFFERENT!

     

    E.g., an export into SVG or PDF could have a switch to enable or disable

    transparency, but ALWAYS exports the correct line widths. For DXF, the

    transparency box would NOT be available, but the line width might be

    left out of the exported file (as already implemented by CadSoft). An

    export to a special drilling machine would need lots of other options.

    CadSoft just cannot (and should not) provide a programming interface

    with standardised GUI for that.

     

    The simplest (and, in my opinion, the best) thing would be to provide

    the possibility to include any ULP into the export GUI. Clicking on this

    menu item would just start the ULP, that's it. Primitive, easy, and

    using all possibilities of ULPs...

     

    Andreas Weidner

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Am 27.01.2012 00:40, schrieb Warren Brayshaw:

    Then the user selects a conversion type. What happens next depends on how

    this functionality is ultimately implemented.

    1) The ULP could simply run.

     

    The idea of providing a complete programming interface for exports is

    nice, but it is QUITE some work to implement such a thing, and I think

    CadSoft has enough things to do at the moment. Additionally, the GUI

    necessities for every export are DIFFERENT!

     

    E.g., an export into SVG or PDF could have a switch to enable or disable

    transparency, but ALWAYS exports the correct line widths. For DXF, the

    transparency box would NOT be available, but the line width might be

    left out of the exported file (as already implemented by CadSoft). An

    export to a special drilling machine would need lots of other options.

    CadSoft just cannot (and should not) provide a programming interface

    with standardised GUI for that.

     

    The simplest (and, in my opinion, the best) thing would be to provide

    the possibility to include any ULP into the export GUI. Clicking on this

    menu item would just start the ULP, that's it. Primitive, easy, and

    using all possibilities of ULPs...

     

    Andreas Weidner