Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Newbie Eagle Questions
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 188 subscribers
  • Views 389 views
  • Users 0 members are here
Related

Newbie Eagle Questions

e14 Contributor
e14 Contributor over 14 years ago

Hello,

 

I'm trying to make my first PCB in Eagle, and I have been running into two problems which I think may be related. 

 

I'm using surface mount components, and with some of my parts, I can not get the program to recognize that a trace is connected to the pad.  I am testing if devices are connected by picking up the component after placeing the trace and rotating it to see if the end of the trace "sticks" to the pad.  Sometimes they do and other times they don't, which leads to all sorts of ERC errors (it says the schematic and PCB are inconsistent). 

 

The second problem, which I'm pretty sure is being caused by the first issue, is that I'm getting many DRC Overlap and Stop Mask errors and the points where my traces and pads are supposed to connect (which suggests to me that the program things I'm trying to route the trace on top of the pad instead of connecting to it). 

 

Is there a way for me to get the traces to "snap" to the pad when I try to make a connection?

 

Thanks

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    I think I found it,

     

    If I first use "Define Electrical Connection", to link the pads I want to connect, then use the "Rout Manually" command instead of "Line/Wire", everything seems to work out alright. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    I think I found it,

     

    If I first use "Define Electrical Connection", to link the pads I want to connect, then use the "Rout Manually" command instead of "Line/Wire", everything seems to work out alright. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Am 15.07.2012 20:56, schrieb Brendan Upton:

    I think I found it,

     

    If I first use "Define Electrical Connection", to link the pads I want to connect, then use the "Rout Manually" command instead of "Line/Wire", everything seems to work out alright.

     

     

    I think  you do something generally wrong. Check

    options/setting/miscellaneous and see that the hook is set to "Set

    junctions automatically". You must use NET to make connections between

    parts. Don't use WIRE, because that is just a line.

    Once you have generated a board you must have open BOTH, .sch & .brd to

    keep consistency.

    Once that is lost you must restore it, because otherwise the board can

    not follow the sheet and vice versa when adding or removing parts.

     

    If you have not done layouts in your board, the most easy way is to

    delete it and generate a new one to get back consistency.

    If you don't want to throw away your board you must use the ERC and work

    down the list of inconsistency errors.

    See that the DRC settings fit your suits. The DRC checks only activated

    layers. So deactivate the stop layer for example.

    In the eagle doc directory you can find a manual and a tutorial and the

    eagle help is available by just hitting the F1 key.

     

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag