Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Idea to improve exploration of the EAGLE libraries
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 2 answers
  • Subscribers 188 subscribers
  • Views 681 views
  • Users 0 members are here
Related

Idea to improve exploration of the EAGLE libraries

e14 Contributor
e14 Contributor over 13 years ago

Hello,

 

Incorporating a second vertical bar at each library facilitates the exploration, Because scans independently each library, rather than explore the full vertical bar

 

It is a good idea +1 or -1?

 

Screenshothttp://jaimeza.org/Temp/Request/Request_eagle_cadsoft_multiverticalbar.gif

 

 

Note The vertical bar (main) on the right explores the whole of libraries

 

+1, please vote

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    New animation, now with vertical ellipsis (...) to indicate +/- files or to expand files

     

    http://jaimeza.org/Temp/Request/Request_eagle_cadsoft_multiverticalbar1.gif

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    New animation, now with vertical ellipsis (...) to indicate +/- files or to expand files

     

    http://jaimeza.org/Temp/Request/Request_eagle_cadsoft_multiverticalbar1.gif

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Generally if I open a library, I want to see as much as possible of 'that' library or subsection.

    I can see this approach may be useful if (for example) VRegs were broken into brands so you could compare (say) NatSemi offerings to Linear Tech.

    However, this isn't usually the time I do component selection, so wouldn't really offer anything.

     

    ian

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 13 years ago in reply to e14 Contributor

    I do understand what you're suggesting, but currently I don't understand the use-case. Do you want to compare the contents of two library folders, and hence you wish for both to be open and viewable on the screen at the same time?

    I personally find the opposite to be true, and would rather that open library folders would 'auto-close' if I opened a different folder without closing a previously opened one. There is nothing I usually wish to compare in libraries (but I many be using it differently to you).

    I can see a benefit of your suggestion in that it may speed up scrolling, but an 'auto-close' (or just remembering to close manually) would be

    just as fast for scrolling purposes, and would require no additional scrollbars (and I dislike the multiple sub-panes in general, because it doesn't scale for smaller displays, because then a greater bulk of the view is taken up by the library name header bars and the additional scroll bars.