Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Idea to improve exploration of the EAGLE libraries
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 2 answers
  • Subscribers 188 subscribers
  • Views 680 views
  • Users 0 members are here
Related

Idea to improve exploration of the EAGLE libraries

e14 Contributor
e14 Contributor over 13 years ago

Hello,

 

Incorporating a second vertical bar at each library facilitates the exploration, Because scans independently each library, rather than explore the full vertical bar

 

It is a good idea +1 or -1?

 

Screenshothttp://jaimeza.org/Temp/Request/Request_eagle_cadsoft_multiverticalbar.gif

 

 

Note The vertical bar (main) on the right explores the whole of libraries

 

+1, please vote

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    New animation, now with vertical ellipsis (...) to indicate +/- files or to expand files

     

    http://jaimeza.org/Temp/Request/Request_eagle_cadsoft_multiverticalbar1.gif

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 13 years ago in reply to e14 Contributor

    I do understand what you're suggesting, but currently I don't understand the use-case. Do you want to compare the contents of two library folders, and hence you wish for both to be open and viewable on the screen at the same time?

    I personally find the opposite to be true, and would rather that open library folders would 'auto-close' if I opened a different folder without closing a previously opened one. There is nothing I usually wish to compare in libraries (but I many be using it differently to you).

    I can see a benefit of your suggestion in that it may speed up scrolling, but an 'auto-close' (or just remembering to close manually) would be

    just as fast for scrolling purposes, and would require no additional scrollbars (and I dislike the multiple sub-panes in general, because it doesn't scale for smaller displays, because then a greater bulk of the view is taken up by the library name header bars and the additional scroll bars.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 13 years ago in reply to e14 Contributor

    I do understand what you're suggesting, but currently I don't understand the use-case. Do you want to compare the contents of two library folders, and hence you wish for both to be open and viewable on the screen at the same time?

    I personally find the opposite to be true, and would rather that open library folders would 'auto-close' if I opened a different folder without closing a previously opened one. There is nothing I usually wish to compare in libraries (but I many be using it differently to you).

    I can see a benefit of your suggestion in that it may speed up scrolling, but an 'auto-close' (or just remembering to close manually) would be

    just as fast for scrolling purposes, and would require no additional scrollbars (and I dislike the multiple sub-panes in general, because it doesn't scale for smaller displays, because then a greater bulk of the view is taken up by the library name header bars and the additional scroll bars.