EAGLE User Support (English) Flooded Polygon
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
  • State Verified Answer
  • Replies 6 replies
  • Subscribers 178 subscribers
  • Views 1205 views
  • Users 0 members are here
  • flooding
  • ratsnest
  • polygons
  • grounds
Related

Flooded Polygon

angelus9
angelus9 over 12 years ago

I have an RF design with a RF Power Amp on the board.  I has a GND/thermal pad under an SOIC8 package.

 

In the library part I made, I put the ground pad in the footprint plus I have eight through holes in the ground pad to conduct heat away from the part plus connect the other layer's grounds to this pad.

 

This is a 4 layer PCB.

 

Problems:

 

1) In the library, I would like to name the pad plus the eight through holes to EGND so the ground floods everything and there is no gaps in the ground plane.  Eagle requires all pads to be named uniquely.  I tried EGND@1, EGND@2, etc.  Didn't help.

 

2) So when I  ratsnest the polygons (EGND), clearances are created between the 7 pads named EGND@1, EGND@2.  The one pad named EGND is flooded/connected but the other 7 pads aren't.  The GND under the SOIC has clearances created by the ratnest command, I must have solid flooding of this pad to the polygon EGND.

 

I tried putting a Rectangle over this area which works until your ratsnest again.  So I ratnest first, add the rectangle, then run CAM.  Low and behold the CAM functions ratsnests again and creates new clearances.

 

Ready to run board but this is holding me up.

 

How can I fix this?

 

Thanks,

Don

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 12 years ago

    If you attached your library it would be easier to see where you have gone

    wrong and provide a solution.

     

    Warren

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 12 years ago

    If you attached your library it would be easier to see where you have gone

    wrong and provide a solution.

     

    Warren

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • angelus9
    0 angelus9 over 12 years ago in reply to autodeskguest

    I tried uploading the library but it says "file type not allowed."  Tried to Zip it, same thing.

     

    Any sugestions?

     

    See the MAX2601ESA+ part if I can find a way to upload the library.

     

    Thanks,

    Don

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 12 years ago in reply to angelus9

    Yes, that Element14 site is a bundle of p**! It's only a front end to the

    real forums at Cadsoft which is a newsgroup so you could go directly there

    and post up to 40k file. Or if you like a browser front end you could go to

    EagleCentral, which is also a front end but brilliant. Down side with

    EagleCentral is you need to apply to post there and it takes a day for

    James to set you up. 

     

     

    There are two ways of getting attachments done at Element14. Attachments

    and in-line so make sure you are using the attachment method for a library

    file.

     

    HTH

    Warren

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.