EAGLE User Support (English) Power and Supply Pin Use on Schematics
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
  • State Verified Answer
  • Replies 6 replies
  • Answers 2 answers
  • Subscribers 181 subscribers
  • Views 5883 views
  • Users 0 members are here
  • pins
  • supply
  • connections
  • power
Related

Power and Supply Pin Use on Schematics

Former Member
Former Member over 12 years ago

I've created a schematic design for a digital circuit with an isolated RS422 section. I'm using an isolating power supply for the transceivers and bringing the data lines onto the main board using an optoisolator. From that point, the rest of the board has common power and grounds. I'm using polygons with different names for GND on each section.

 

I'm running into 2 distinct problems.

1) I need to keep the isolated VCC and GND nets separated on the schematic. I'm having some sucess with this as I am using different net names (i.e. GND and -VOUT)

2) Power and Supply pins are more challenging. Some IC's have VCC, others VDD. The isolated section I've given the net name of +VOUT. All are at +5v.

 

When I run ERC, I get warnings of interconnected nets. I believe I'm using Power and Supply pins incorrectly. Simple case - how do I properly connect +5v to VCC and to VDD on the same net?

 

imageimageimage

Slight mess! Yes, VDD has no net as it will generate more errors if I connect it to +5v.

 

I appreciate your time and suggestions!

 

Warm regards.

  • Sign in to reply
  • Cancel
Parents
  • dukepro
    0 dukepro over 12 years ago

    On 09/30/2013 11:27 AM, David Kanazawa wrote:

    ...

    I'm running into 2 distinct problems.

    1) I need to keep the isolated VCC and GND nets separated on the

    schematic. I'm having some sucess with this as I am using different net

    names (i.e. GND and -VOUT)

     

    Use the supply symbols in supply.lbr or supply2.lbr for each of your

    different nets.  i.e. GND, GND1, GND2, etc.

    Eagle will treat these, as it should, as separate nets.  To tie them

    together, use the SHORT device in the attached shorts.lbr.  This is

    merely two pads that overlap each other.  This will produce a DRC error,

    but it can be approved to prevent from being a nuisance.

     

    2) Power and Supply pins are more challenging. Some IC's have VCC,

    others VDD. The isolated section I've given the net name of +VOUT. All

    are at +5v.

     

    You can use the supply symbol +5V from the supply2 library to name the

    net (it conveys more information to the reader).

    When I run ERC, I get warnings of interconnected nets. I believe I'm

    using Power and Supply pins incorrectly. Simple case - how do I properly

    connect +5v to VCC and to VDD on the same net?

    ERC warnings of the type "VCC connected to +5V" can be approved.  All it

    means is that the name of the power pin does not match the name of the

    net to which it's connected.

     

    If you want to connect separate nets, use the SHORT device.

     

    I do this quite often to separate different grounds such as analog

    ground, a noisy high-power ground, and a logic ground.  I want to tie

    them all together eventually, but keep them separate as long as

    possible.  So all the shorts are placed close to the battery connector.

    Since it's an on-board component, I take all shorts out of the BOM.

     

    HTH,

        - Chuck

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 12 years ago in reply to dukepro

    Paul and Chuck,

     

    Thanks very much for taking the time to help (re)explain this issue. It's very helpful to have the concrete examples of devices, the error messages and result of "approving" errors. It would not have occurred to me to search for the SHORT device, so that was particularly useful. I'll give this a go and hopefully it will allow me to complete this section of schematic layout. Nice touch on removing the SHORT from the BOM.

     

    One side note - I'm not clear on why it's necessary to even have the supply and power connections laid out. Is it for clarity of which voltage is being applied to a particular net such as defining the VCC voltage?

     

    And on to the next topic - "Polygons May Have Fallen Apart".

     

    Thank you for helping me understand how to use these tools!

     

    David K.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dukepro
    0 dukepro over 12 years ago in reply to Former Member

    On 10/01/2013 01:29 PM, David Kanazawa wrote:

    One side note - I'm not clear on why it's necessary to even have the

    supply and power connections laid out. Is it for clarity of which

    voltage is being applied to a particular net such as defining the VCC

    voltage?

     

    VCC, of course, stems from the collector voltage, just as VDD refers to

    a drain voltage.  Consider the case where a SUPPLY device called VDD is

    attached to a POWER pin on an IC named VDD.  This certainly avoids the

    DRC warning.

     

    Putting on my philosopher's hat for a moment, the purpose of a schematic

    is to convey the design of a circuit to a reader.  Some may call it art,

    and other may call it the essence of the circuit.  Whatever one chooses

    to call it, a schematic should convey what the circuit is about, and not

    necessarily how the design is manifested on a PCB.

     

    Back to engineering...  So, when a reader sees that a VDD supply is

    connected to VDD pin, it's a real "duh" moment.  The next question is

    "what is VDD?".  So, instead of using a SUPPLY device called VDD,

    consider using a SUPPLY device that conveys what the voltage on that net

    should be.  Something like "5V", "3.3V", or "+15V".  This serves a

    dual purpose in that it immediately conveys to the reader what VDD

    should be, and it produces a DRC warning allowing the designer to verify

    (by approving the error) that the proper voltage supply should indeed be

    connected to VDD of that particular IC.

     

    As far as leaving the power pins off of a schematic, I would recommend

    against it for the simple reason that it hides information from the

    reader.  Many IC's have power and ground pins on the corner (7 and 14,

    or 8 and 16); others have power and ground midway down the sides; and

    QFP's have multiple power pins scattered wherever they're needed.  In

    cases where the power pins are a separate gate from the main schematic

    symbol, I usually stuff them down in a corner of my schematic along with

    a bypass capacitor.  But keep them on the schematic

     

    I would recommend using SHORT devices sparingly in that it, in part,

    defeats the purpose of the DRC.  For example, if one were to connect a

    +5V supply to a GND supply through a SHORT, Eagle would not complain one

    bit.  But as soon as you applied power, your board would certainly

    complain with a puff of smoke.

     

    HTH,

        - Chuck

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • dukepro
    0 dukepro over 12 years ago in reply to Former Member

    On 10/01/2013 01:29 PM, David Kanazawa wrote:

    One side note - I'm not clear on why it's necessary to even have the

    supply and power connections laid out. Is it for clarity of which

    voltage is being applied to a particular net such as defining the VCC

    voltage?

     

    VCC, of course, stems from the collector voltage, just as VDD refers to

    a drain voltage.  Consider the case where a SUPPLY device called VDD is

    attached to a POWER pin on an IC named VDD.  This certainly avoids the

    DRC warning.

     

    Putting on my philosopher's hat for a moment, the purpose of a schematic

    is to convey the design of a circuit to a reader.  Some may call it art,

    and other may call it the essence of the circuit.  Whatever one chooses

    to call it, a schematic should convey what the circuit is about, and not

    necessarily how the design is manifested on a PCB.

     

    Back to engineering...  So, when a reader sees that a VDD supply is

    connected to VDD pin, it's a real "duh" moment.  The next question is

    "what is VDD?".  So, instead of using a SUPPLY device called VDD,

    consider using a SUPPLY device that conveys what the voltage on that net

    should be.  Something like "5V", "3.3V", or "+15V".  This serves a

    dual purpose in that it immediately conveys to the reader what VDD

    should be, and it produces a DRC warning allowing the designer to verify

    (by approving the error) that the proper voltage supply should indeed be

    connected to VDD of that particular IC.

     

    As far as leaving the power pins off of a schematic, I would recommend

    against it for the simple reason that it hides information from the

    reader.  Many IC's have power and ground pins on the corner (7 and 14,

    or 8 and 16); others have power and ground midway down the sides; and

    QFP's have multiple power pins scattered wherever they're needed.  In

    cases where the power pins are a separate gate from the main schematic

    symbol, I usually stuff them down in a corner of my schematic along with

    a bypass capacitor.  But keep them on the schematic

     

    I would recommend using SHORT devices sparingly in that it, in part,

    defeats the purpose of the DRC.  For example, if one were to connect a

    +5V supply to a GND supply through a SHORT, Eagle would not complain one

    bit.  But as soon as you applied power, your board would certainly

    complain with a puff of smoke.

     

    HTH,

        - Chuck

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer