Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) place components on bottom layer without mirroring?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 179 subscribers
  • Views 1546 views
  • Users 0 members are here
Related

place components on bottom layer without mirroring?

Former Member
Former Member over 11 years ago

Hey guys,

I'm sorry for being a noob but every word on the subject I find suggests using the mirror tool.

 

I've created my pcb layout which has zif eprom sockets on the top layer and a DIL28 IC socket which should be underneath the zif socket (slightly offset a little)

So in essence the components are kinda stacked.

 

if I choose mirror it flips the IC socket around which just doesnt seem right to me.

also after trying to mirror the ic socket i would have expected to see the solder pads for it to be on the top but teh solder pads for the zif socket on the bottom.

 

am I being a total idiot?

  • Sign in to reply
  • Cancel
  • Former Member
    0 Former Member over 11 years ago

    I thought it best to accompany my ramblings with a screenshot. lol

     

    So in my mind, the zif sockets are on the top layer (although would be soldered on the bottom layer)

    the 3  DIL IC sockets are offset to the right of each zif socket. those sockets should be on the bottom layer, but soldered on the top layer.

    The switches should all be sat on the top layer and soldered on the bottom.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago

    Brad Holland wrote:

     

    Hey guys,

    I'm sorry for being a noob but every word on the subject I find suggests

    using the mirror tool.

     

    I've created my pcb layout which has zif eprom sockets on the top layer

    and a DIL28 IC socket which should be underneath the zif socket

    (slightly offset a little)

    So in essence the components are kinda stacked.

     

    yes and no 8-)

     

    If you dont mirror the the bottom parts, the pin assignment on them

    will be mirrored regarding the IC you put into the socket.

    That is you would need to bend the IC pins to top by 180° to connect

    them correctly 8-)

    I can't imagine that is wat you want.

     

     

    if I choose mirror it flips the IC socket around which just doesnt seem

    right to me.

     

    well, see above

     

     

    also after trying to mirror the ic socket i would have expected to see

    the solder pads for it to be on the top but teh solder pads for the zif

    socket on the bottom.

     

    I assume you have a one layer setup? In that case you will have Pads

    only on one side of the board (usualy the bottom side, layer 16 that

    is).

     

     

    am I being a total idiot?

     

    no comment (sorry, couldn't resist)

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dukepro
    0 dukepro over 11 years ago in reply to Former Member

    On 02/20/2014 09:17 PM, Brad Holland wrote:

    I thought it best to accompany my ramblings with a screenshot. lol

     

    So in my mind, the zif sockets are on the top layer (although would be

    soldered on the bottom layer)

    the 3  DIL IC sockets are offset to the right of each zif socket. those

    sockets should be on the bottom layer, but soldered on the top layer.

    The switches should all be sat on the top layer and soldered on the

    bottom.

     

    Brad,

     

    Forget about on which side the pins are soldered.  The pads are on both

    the top and bottom layers since the holes are plated through.  Thus,

    when you mirror one of the parts, the only thing that appears to change

    is where the clamp arm is located.

     

    To make it a bit more clear as to what's happening with the mirror, go

    to Options->Set->Misc and make sure the checkbox labeled "Display pad

    names" is turned on.  When the board is viewed, each pad will have the

    pin number in it.  If you also turn off the Drills, Holes, tStop, and

    bStop layers, it will remove some of the clutter on your board.

     

    When deciding whether to mirror a part or not, one should consider from

    which side will the part be installed?  If the ZIF is installed on the

    top of the board, it should NOT be mirrored.  If it is installed on the

    bottom side of the board, it MUST be mirrored.

     

    The easiest example I can think of is to take one of your ZIF sockets

    and set it on the table pins down (top installation).  Note the location

    of pin 1.  Now flip it over horizontally so that the pins are up (bottom

    installation).  Note the location of pin 1.  This is how it's displayed

    in Eagle - viewed from the top down looking through the board.

     

    All in all, it looks like you want the ZIF's installed on the top side

    (not mirrored), and the DIL's installed on the bottom side (mirrored).

    In the image, U15 is properly mirrored, while U11 and U16 are not.

     

    HTH,

        - Chuck

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago

    thanks guys I'm starting to get my head around it a bit more after your replies.

    Lorenz, to what you said about bending up chip legs, I'm not actually putting a chip into the underside ic socket, I have made some flat ribbon cables. so that shouldnt be an issue..?

     

    So just to be sure, mirroring a part doesnt actually make it place pads on top or bottom, wherever drilled pads are there will be conductors on both sides of the board, and as you said, they are plated through (via's?)

     

    Just in case you were wondering, I created a prototype of a hacked drum machine, and a fair few people want one, thing is, this one took me an absolute age to make due to an absolute mountain of wiring as everything is connected by hand soldering.

    I'm trying to get this board made so that I can speed up the making process...

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to Former Member

    On Fri, 21 Feb 2014 15:05:49 GMT, Brad Holland

    <noreply-223697@element14.com> wrote:

     

    So just to be sure, mirroring a part doesnt actually make it place pads

    on top or bottom

     

    Actually, it does. A through-hole part has pads on both sides anyway,

    so the point is moot. But if you mirror a surface mount part, the pads

    WILL be moved to the other side.

     

    What you must remember is that when you look at the bottom layer, you

    see it as viewed from the top. In other words, you will look at the

    underside if the parts that are placed on the bottom layer.

     

    This might sound a bit tricky at first, but it's actually easier done

    than said.

    --

    RoRo

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to autodeskguest

    I think i get you.

    You mean you have to look at it imagining you have x-ray specs on, right? lol

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to Former Member

    Am 22.02.2014 15:00, schrieb Brad Holland:

    I think i get you.

    You mean you have to look at it imagining you have x-ray specs on,

    right? lol

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/104522

     

     

    Yep image

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag