Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Attributes improvements.
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 180 subscribers
  • Views 334 views
  • Users 0 members are here
Related

Attributes improvements.

kikoun
kikoun over 11 years ago

Hi,

 

Attributes is really powerful but sometimes, to define them can be painful, in particular when we had to copy an paste and paste and paste...

 

- For global attributes: we often have to copy from SCH to BRD. In 'New attribute' and 'Change attribute' dialog box, a little option like 'apply in schematic' (or board if edit from schematic), would be welcome. So If we change or add one attribute that must be the same in schematic and board, we don't have to do it twice.

I know, there is already a post about this point... but ARgggg that would be great...

 

- For devices attributes in library editor: This is the most annoying part. If a part have several package variant, it's really painful to edit attributes, in particular with attributes with same

value for all package variant. We must close the Attributes window, select the other package, then open again the attributes window.

 

The best thing will be  a little change in this attributes window, by adding a list of the package variants, in the left bottom corner (on the same line of the NEW, CHANGE DEL OK Cancel Buttons). When we open the attributes window, we can see and edit the attributes of the current package, but we could also see/edit the attributes of the other variant, just by selecting an other package in this list. It would be easier to check and edit the attributes, of ALL the device package variant at once.

 

And (in the same spirit of the suggestion for global attributes) adding a little option to apply to all package in the 'New attribute' and 'Change attribute' dialog box would be useful too.

 

Guillaume Barrey

  • Sign in to reply
  • Cancel
  • anweid
    0 anweid over 11 years ago

    Am 05.08.2014 13:49, schrieb Guillaume barrey:

    - For global attributes: we often have to copy from SCH to BRD. In

    'New attribute' and 'Change attribute' dialog box, a little

    option like 'apply in schematic' (or board if edit from schematic),

    would be welcome. So If we change or add one attribute that must be the

    same in schematic and board, we don't have to do it twice.

    I know, there is already a post about this point... but ARgggg that

    would be great...

     

    The best thing will be  a little change in this attributes window, by

    adding a list of the package variants, in the left bottom corner (on the

    same line of the NEW, CHANGE DEL OK Cancel Buttons). When we open the

    attributes window, we can see and edit the attributes of the current

    package, but we could also see/edit the attributes of the other variant,

    just by selecting an other package in this list. It would be easier to

    check and edit the attributes, of ALL the device package variant at

    once.

     

    And (in the same spirit of the suggestion for global attributes) adding

    a little option to apply to all package in the 'New attribute' and

    'Change attribute' dialog box would be useful too.

     

    for our standard attributes, we do this with a ULP, but yes, PLEASE: The

    above suggestion would make things MUCH easier for the usual

    'non-programmer'.

     

    Andreas Weidner

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kikoun
    0 kikoun over 11 years ago in reply to anweid

    Hi Andreas,

     

    for our standard attributes, we do this with a ULP, but yes, PLEASE: The

    above suggestion would make things MUCH easier for the usual

    'non-programmer'.

     

    Andreas Weidner

     

     

    Thank you for support on this !

     

    I also made a script for my standards global attributes, so when I start a new board, I run it in Sch and in Brd. But when I start a new version of an existing board, I have to make some changes and script is not really helpful ( the time to create the script = time to do it).

     

    For library, I known that some ulp already exist but, they don't necessary correspond to my needs, and you hae to remeber how to use them etc...They also do not let you have a global vision of your the attributes of all package variants. So for checking purposes, ulp doesn't help. Unless someone build a big huges ulp with a nice IHM... but the actual attribute windows is already done. It would be shame that someone spend much time to rebuild this windows since the few adjustment I suggested will be enough (I think).

     

    Guillaume Barrey

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dukepro
    0 dukepro over 11 years ago

    On 08/05/2014 07:49 AM, Guillaume barrey wrote:

    Hi,

     

    Attributes is really powerful but sometimes, to define them can be

    painful, in particular when we had to copy an paste and paste and

    paste...

     

    - For global attributes: we often have to copy from SCH to BRD. In

    'New attribute' and 'Change attribute' dialog box, a little

    option like 'apply in schematic' (or board if edit from schematic),

    would be welcome. So If we change or add one attribute that must be the

    same in schematic and board, we don't have to do it twice.

    I know, there is already a post about this point... but ARgggg that

    would be great...

     

     

    I agree that those buttons would be nice.  A better solution would be

    project level attributes.  When a search for an attribute is done (i.e.

    ">XYZZY"), the search path could start at the variant, then the device,

    file (.sch or .brd), an finally the project.

     

    The term "Global Attributes" is somewhat of a misnomer; it should more

    accurately be called "File Attributes".  The term "Global Attributes" is

    just too unspecific when there's really nothing global about them.  They

    don't apply across files, projects, installation instances, computers,

    networks, companies, nor countries.  Admittedly, I'm bordering on the

    absurd, but so is "Global".

     

    Enjoy,

        - Chuck

     

     

    Attachments:
    5023.att1.html.zip