EAGLE User Support (English) Is there anyway to exclude parts from the PCB
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
  • State Not Answered
  • Replies 29 replies
  • Subscribers 181 subscribers
  • Views 4459 views
  • Users 0 members are here
Related

Is there anyway to exclude parts from the PCB

Former Member
Former Member over 11 years ago

In Eagle Cad, is there anyway to exclude components on the schematic from the board view? I have several parts that will be wired to screw terminals. They still need to be shown in the schematic, but I do not need or want them on the board. I can't leave them outside the board area, so what's a guy to do? Thanks...

  • Sign in to reply
  • Cancel

Top Replies

  • autodeskguest
    autodeskguest over 11 years ago +1
    On 3/26/2015 4:38 AM, Derek Tombrello wrote: In Eagle Cad, is there anyway to exclude components on the schematic from the board view? I have several parts that will be wired to screw terminals. They still…
  • autodeskguest
    autodeskguest over 9 years ago in reply to Former Member +1
    Mark Winters wrote: Hello Jorge. I wonder if you could point me to some documentation that helps me to remove the package as explained. I have made a copy of the component in my own library but return…
Parents
  • autodeskguest
    0 autodeskguest over 10 years ago

    On 27/03/15 06:16, Doug Wellington wrote:

    EAGLE is a two-way process; they call it forward-backward annotation.  That

    ties the board back to the schematic, so that you can make certain changes

    in the board and the schematic gets updated.  I think this is a much better

    way of working on designs that have one schematic and one board, but it's

    not ideal for single schematics with multiple board layouts...

     

    It may not be ideal for that case, but that's a case where nothing's

    ideal. Frankly, I find the KiCad / gEDA method utterly unusable.

     

    Anyway, this whole sub-thread was fired off by a troll who wasn't

    up-to-date with the latest Eagle, as Jorge pointed out in his reply.

    Derek's actual requirement can be supported that way.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to autodeskguest

    "TROLL"?! Excuse me for not being an expert in Eagle. And if you meant that Eagle itself wasn't up to date... I'm one revision behind. So sue me.

     

     

    @Jorge -> I just now saw your reply and I will try that tonight. I do think that that may be step-intensive... but if it works...

     

    @CadSoft Guest -> I have seen kicad in the repositories, but I've never tried playing with it. I may try that this weekend as well.

     

    To those of you who actually had something constructive to add, I truly appreciate your help!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to Former Member

    On 28/03/15 16:22, Derek Tombrello wrote:

    "TROLL"?! Excuse me for not being an expert in Eagle. And if you meant

    that Eagle itself wasn't up to date... I'm one revision behind. So sue

    me.

     

    No, you're not the troll. "Poll-was Poll-was" is a persistent troll who

    hasn't kept up to date. See Jorge's reply (which you now have). I don't

    think it's overly intensive and it's the right way to handle the

    specific issue you began with. This half of the discussion got

    side-tracked onto a different issue.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to Former Member

    On 28/03/15 16:22, Derek Tombrello wrote:

    "TROLL"?! Excuse me for not being an expert in Eagle. And if you meant

    that Eagle itself wasn't up to date... I'm one revision behind. So sue

    me.

     

    No, you're not the troll. "Poll-was Poll-was" is a persistent troll who

    hasn't kept up to date. See Jorge's reply (which you now have). I don't

    think it's overly intensive and it's the right way to handle the

    specific issue you began with. This half of the discussion got

    side-tracked onto a different issue.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 10 years ago in reply to autodeskguest

    Ah... my bad. Thank you image and sorry...