EAGLE User Support (English) Is there anyway to exclude parts from the PCB
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
  • State Not Answered
  • Replies 29 replies
  • Subscribers 181 subscribers
  • Views 4486 views
  • Users 0 members are here
Related

Is there anyway to exclude parts from the PCB

Former Member
Former Member over 11 years ago

In Eagle Cad, is there anyway to exclude components on the schematic from the board view? I have several parts that will be wired to screw terminals. They still need to be shown in the schematic, but I do not need or want them on the board. I can't leave them outside the board area, so what's a guy to do? Thanks...

  • Sign in to reply
  • Cancel

Top Replies

  • autodeskguest
    autodeskguest over 11 years ago +1
    On 3/26/2015 4:38 AM, Derek Tombrello wrote: In Eagle Cad, is there anyway to exclude components on the schematic from the board view? I have several parts that will be wired to screw terminals. They still…
  • autodeskguest
    autodeskguest over 9 years ago in reply to Former Member +1
    Mark Winters wrote: Hello Jorge. I wonder if you could point me to some documentation that helps me to remove the package as explained. I have made a copy of the component in my own library but return…
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to Former Member

    Derek Tombrello wrote on Mon, 30 March 2015 19:36

    Still not seeing any attachment to download....

     

    You can get to the attachment at the Stratford Digital EAGLE Central site.

    All the cool EAGLE kids hang out there instead of at Element14:

     

    http://www.eaglecentral.ca/forums/

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to autodeskguest

    Oh.. well, see... there's the problem! I was never allowed to play with the cool kids! lol... Thank you. I have that downloaded and will try that out in a bit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to autodeskguest

    Doug Wellington wrote:

    You can get to the attachment at the Stratford Digital EAGLE Central site.

    All the cool EAGLE kids hang out there instead of at Element14:

     

    http://www.eaglecentral.ca/forums/

     

    or they use a newsreader and access the eagle newsgroups directly 8-)

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to autodeskguest

    GOT IT!  After looking at the sample library, I figured out what I was doing wrong... Instead of adding _EXTERNAL_ as the attribute, I was adding EXTERNAL - without the underscores. Makes all the difference in the world!  Thanks for all of your help guys image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to autodeskguest

    Lorenz wrote on Tue, 31 March 2015 01:05

    or they use a newsreader and access the eagle newsgroups directly 8)

     

    Some day, maybe I'll be cool enough to graduate to that level, up there

    with you and Jorge...  :d

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago in reply to autodeskguest

    Hello Jorge. I wonder if you could point me to some documentation that helps me to remove the package as explained. I have made a copy of the component in my own library but return an error when I try to remove its package. ????

     

    image

     

    I am a complete novice but Im into it.....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to Former Member

    Perhaps I'm missing something, but if you have a panel mounted volume

    control, you still need pads on the PCB to solder the wires that are

    soldered to the volume control.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to Former Member

    Mark Winters wrote:

     

    Hello Jorge. I wonder if you could point me to some documentation that

    helps me to remove the package as explained. I have made a copy of the

    component in my own library but return an error when I try to remove

    its package. ????

     

     

    I am a complete novice but Im into it.....

     

     

    posting a totally unrelated question into a old tread from april 2015

    won't do you any good.

    --

     

    Lorenz

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to Former Member

    On 7/22/2016 4:47 AM, Mark Winters wrote:

    Hello Jorge. I wonder if you could point me to some documentation that helps me to remove the package as explained. I have made a copy of the component in my own library but return an error when I try to remove its package. ????

     

     

    I am a complete novice but Im into it.....

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/202074

     

     

    Hi Mark,

     

    I hope you're doing well. As Lorenz has pointed out, it's best to start

    a new thread when you have a new question. However, I know Element14

    doesn't make that easy for new users. In the future it might be easier

    for you to use the forum mirror here:

     

    http://eaglecentral.ca/

     

    Now on to your problem. EAGLE will not let you delete a package if it is

    associated with a device. So the first thing you have to do it open the

    device that uses that package. Remove the package from the device by

    first clicking on the connect button at the bottom right of the device

    editor. Undo all of the connections. Then you'll be able to delete the

    package from the device and ultimately from the library if you so wish.

     

    hth,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<