EAGLE User Support (English) Renaming a component error
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
  • State Not Answered
  • Replies 11 replies
  • Subscribers 179 subscribers
  • Views 965 views
  • Users 0 members are here
Related

Renaming a component error

pavanbabut
pavanbabut over 10 years ago

I have a schematic and board that I am going through the names of components. The problem I am having is whenever I try to delete a component in my case a cap (ex: C21) and then replace it with a different type cap, it changes its name to C00021 rather than C21 and when I try to rename it to C21 it gives me error that the component already exists, but when I try 'Show' command it doesn't show it and when I try to Show it on board, it says 'doesn't exist'. Very frustrating, I have few components that I want to replace with different type and its doing for all those.

 

Any ideas or suggestions?

 

thanks

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 10 years ago

    On 15.06.2015 21:00, Pavan Tiruveedhula wrote:

    I have a schematic and board that I am going through the names of

    components. The problem I am having is whenever I try to delete a

    component in my case a cap (ex: C21) and then replace it with a

    different type cap, it changes its name to C00021 rather than C21 and

    when I try to rename it to C21 it gives me error that the component

    already exists, but when I try 'Show' command it doesn't show it and

    when I try to Show it on board, it says 'doesn't exist'. Very

    frustrating, I have few components that I want to replace with different

    type and its doing for all those.

     

    Any ideas or suggestions?

     

    What version and locale are you using?

    Did you try 'show @ C21" in both sch and brd?

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • pavanbabut
    0 pavanbabut over 10 years ago in reply to autodeskguest

    Eagle 6.5.0 standard and when I use Show command, it just pops up a dialog with C21 in there in schematic and it does nothing when I click it and when I use the same command in Board, it gives me error that C21 is no found.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • pavanbabut
    0 pavanbabut over 10 years ago in reply to autodeskguest

    Eagle 6.5.0 standard and when I use Show command, it just pops up a dialog with C21 in there in schematic and it does nothing when I click it and when I use the same command in Board, it gives me error that C21 is no found.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to pavanbabut

    On 17.06.2015 21:41, Pavan Tiruveedhula wrote:

    Eagle 6.5.0 standard and when I use Show command, it just pops up a

    dialog with C21 in there in schematic and it does nothing when I click

    it and when I use the same command in Board, it gives me error that C21

    is no found.

     

    Sounds like C21 is a funny cap with no footprint, but then again, it

    should be visible...

     

    Did you try to type "delete c21" from sch? Then "show c21" again? If its

    gone, do ERC to make sure you have consistancy.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • pavanbabut
    0 pavanbabut over 10 years ago in reply to autodeskguest

    Actually I used C21 as an example, it does the same on any component. Yes I did delete command and then tried show command with same results.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to pavanbabut

    On 18.06.2015 16:15, Pavan Tiruveedhula wrote:

    Actually I used C21 as an example, it does the same on any component.

    Yes I did delete command and then tried show command with same results.

     

    I think we can conclude that your files are corrupt, and that Eagle is

    not able to repair it. Im sure someone at cadsoft could fix it for you

    if its important.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to autodeskguest

    Ouch, are these ascii?