Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) NAME command in ULP
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 189 subscribers
  • Views 3039 views
  • Users 0 members are here
Related

NAME command in ULP

rachaelp
rachaelp over 10 years ago

Hello,

 

I've using NAME within a ULP to automatically rename some busses/wires. It

works great when there is just one occurrence of a wire on a sheet but as

soon as there is a second I get a pop-up asking if I want to change just

the selected segment or all segments in the sheet. Looking at the docs I

can't see a way to make this happen automatically without prompting, does

anybody else know of a way to stop this prompt showing up?

 

If not then maybe the command needs an enhancement to allow the following

optional parameter for naming busses/wires:

 

NAME new_name (x y) T

 

where T = This segment, E = Every segment on sheet and A = All segments on

all sheets

 

Best Regards,

 

Rachael

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
  • ChristyZ
    ChristyZ over 10 years ago in reply to rachaelp

    Apologies for testing in the "live" forum. Please disregard. Just checking

    to see if this reply appends correctly to the right thread on element14's

    side. Carry on.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ChristyZ
    ChristyZ over 10 years ago in reply to rachaelp

    Apologies for testing in the "live" forum. Please disregard. Just checking

    to see if this reply appends correctly to the right thread on element14's

    side. Carry on.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 10 years ago

    Morten Leikvoll wrote on Thu, 19 May 2016 14:33

    Surely there must be some reserved character that can be used to avoid

     

    mixup with any names? Like the character ':', so you could define

    commands like:

     

    NAME :allsheets: <oldname> <newname>;

     

    But maybe allsheets should be explicit on this syntax. Also,

     

    NAME :thissheets: <newname> (x y);

     

    Would work. The position of :<flag>: is kinda relaxed on this syntax,

    so

    even

     

    NAME <oldname> (x y) :thisseg:;

    will be consistant.

     

    Even using multiple independantly placed keywords could work here,

    like

     

    NAME <oldname> :thisseg: (x y) :includepolygons:;

     

     

    This is very easy to interpret for the commant interpreter.

    As shown, I do prefer having some name instead of single character or

    numbers for the selections. They will also work for future added

    keywords.

     

     

    Yep this all seems completely sensible to me image

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 10 years ago

    CadSoft Support wrote on Thu, 19 May 2016 13:30

    To add such options as Rachael suggested is possible, but IMHO not

    so elegant. Think also of signal polygons in the board? There we would

    need additional options like P for Polygon only , or W for whole signal

     

    or something like that....

    We get a number of letters that have to be distinguisable from the

    names.

     

     

    My suggestion of T E and A as the options was only because that is

    consistent with what is stated in the help for the keys to press to select

    these options. I'd much prefer a much more descriptive switch. So I'd vote

    for something like:

     

    NAME --this  (x y)

     

    Omitting the --switch would produce the same behaviour as currently so it

    would not break exisiting functionality.

     

    This syntax would work consistently across all commands regardless of what

    the dialog options were.

     

    CadSoft Support wrote on Thu, 19 May 2016 13:30

    On the other hand for SET CONFIRM we could add some options like

    OPT1, OPT2, OPT3 and preselect/address/confirm the wanted option

    of the dialog. This would work for all dialogs that offer more options

    to choose. It fits better in the current structure of EAGLE.

     

     

    Having to "wrap" every NAME (or any other) command in a pair of "SET

    CONFIRM YES/NO/OFF" commands to get the desired behaviour is IMHO an overly

    verbose cludge image

     

    Best Regards,

     

    Rachael

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago

    On 19.05.2016 14:30, Richard Hammerl wrote:

    Am 19.05.2016 um 11:16 schrieb Morten Leikvoll:

    On 19.05.2016 10:55, Richard Hammerl wrote:

    I think this could be an enhancement of the SET CONFIRM command.

    We will check this....

     

    Now, THAT you have to explain. I think the rest of us would say no. The

    inline option is much better. It does not need to be backward compatible

    as long as no explicit selection opens the requester as before.

     

     

     

    The inline option with the NAME command? It's a bit tricky there

    because of the current syntax.

    You can for example use  NAME oldname newname   or   NAME name (x y)

     

    To add such options as Rachael suggested is possible, but IMHO not

    so elegant. Think also of signal polygons in the board? There we would

    need additional options like P for Polygon only , or W for whole signal

    or something like that....

    We get a number of letters that have to be distinguisable from the

    names.

     

    On the other hand for SET CONFIRM we could add some options like

    OPT1, OPT2, OPT3 and preselect/address/confirm the wanted option

    of the dialog. This would work for all dialogs that offer more options

    to choose. It fits better in the current structure of EAGLE.

     

    For example:

    NAME net

    OPT1  this segment               set confirm opt1; name GND (0 1);

    OPT2  all segments on sheet      set confirm opt2; name GND (0 1);

    OPT3  all segments on all sheets set confirm opt3; name GND (0 1);

     

    NAME polygon

    OPT1 polygon only         set confirm opt1; name GND (0 1);

    OPT2 whole signal         set confirm opt2; name GND (0 1);

     

    And we would be prepared for future dialogs as well.  image

     

    Surely there must be some reserved character that can be used to avoid

    mixup with any names? Like the character ':', so you could define

    commands like:

     

    NAME :allsheets:  :thisseg: (x y) :includepolygons:;

     

     

    This is very easy to interpret for the commant interpreter.

    As shown, I do prefer having some name instead of single character or

    numbers for the selections. They will also work for future added keywords.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago

    Am 19.05.2016 um 11:16 schrieb Morten Leikvoll:

    On 19.05.2016 10:55, Richard Hammerl wrote:

    I think this could be an enhancement of the SET CONFIRM command.

    We will check this....

     

    Now, THAT you have to explain. I think the rest of us would say no. The

    inline option is much better. It does not need to be backward compatible

    as long as no explicit selection opens the requester as before.

     

     

     

    The inline option with the NAME command? It's a bit tricky there

    because of the current syntax.

    You can for example use  NAME oldname newname   or   NAME name (x y)

     

    To add such options as Rachael suggested is possible, but IMHO not

    so elegant. Think also of signal polygons in the board? There we would

    need additional options like P for Polygon only , or W for whole signal

    or something like that....

    We get a number of letters that have to be distinguisable from the

    names.

     

    On the other hand for SET CONFIRM we could add some options like

    OPT1, OPT2, OPT3 and preselect/address/confirm the wanted option

    of the dialog. This would work for all dialogs that offer more options

    to choose. It fits better in the current structure of EAGLE.

     

    For example:

    NAME net

      OPT1  this segment               set confirm opt1; name GND (0 1);

      OPT2  all segments on sheet      set confirm opt2; name GND (0 1);

      OPT3  all segments on all sheets set confirm opt3; name GND (0 1);

     

    NAME polygon

      OPT1 polygon only         set confirm opt1; name GND (0 1);

      OPT2 whole signal         set confirm opt2; name GND (0 1);

     

    And we would be prepared for future dialogs as well.  image

     

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago

    On 19.05.2016 10:55, Richard Hammerl wrote:

    I think this could be an enhancement of the SET CONFIRM command.

    We will check this....

     

    Now, THAT you have to explain. I think the rest of us would say no. The

    inline option is much better. It does not need to be backward compatible

    as long as no explicit selection opens the requester as before.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago

    Am 18.05.2016 um 16:20 schrieb Rachael:

    rachaelp wrote on Wed, 18 May 2016 13:48

    However..... I just installed 7.6.0 and something has changed and what

    used to work perfectly now erroneously puts net names all over my busses

    in some cases..... I'll tidy up my script and generate a simple test

    schematic and pop it over to CadSoft as I think this must be a newly

    introduced bug.

     

    Okay just a quick update, so it wasn't 7.6.0 that changed things, i found

    that with my ULP script when I had busses / nets across multiple pages,

    once I do:

     

    set Cmd.Name.RenameEntireNetByDefault 1

     

    then randomly things go a bit bonkers.... My ULP script is looping through

    lots of objects and hierarchy to build up the final command which changes a

    bunch of names so it must be some conflict with this setting and what I am

    trying to achieve screwing everything up.... I need to investigate

    further....

     

     

    Following this thread I agree that there are missing options that

    allow to choose exactly what to rename.

    I think this could be an enhancement of the SET CONFIRM command.

    We will check this....

     

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 10 years ago

    rachaelp wrote on Wed, 18 May 2016 13:48

    However..... I just installed 7.6.0 and something has changed and what

    used to work perfectly now erroneously puts net names all over my busses

    in some cases..... I'll tidy up my script and generate a simple test

    schematic and pop it over to CadSoft as I think this must be a newly

    introduced bug.

     

     

    Okay just a quick update, so it wasn't 7.6.0 that changed things, i found

    that with my ULP script when I had busses / nets across multiple pages,

    once I do:

     

    set Cmd.Name.RenameEntireNetByDefault 1

     

    then randomly things go a bit bonkers.... My ULP script is looping through

    lots of objects and hierarchy to build up the final command which changes a

    bunch of names so it must be some conflict with this setting and what I am

    trying to achieve screwing everything up.... I need to investigate

    further....

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 10 years ago

    Hi Warren/Lorenz,

     

    Thanks both for pointing me in the direction of:

     

    set Cmd.Name.RenameEntireNetByDefault 1

     

    This does enable me to do most of what I would like now. I'd gone ahead and

    wrapped my individual name commands within SET CONFIRM YES/OFF commands

    already and this seemed to work generally okay so combined with this extra

    command I think I can do what I need. I still think it's a bit of a clumsy

    approach to be having to wrap these commands up with additional directives

    to modify their behaviour. Having a consistent option available for

    commands to specify the option to choose would lead to much cleaner scripts

    in my opinion.

     

    However..... I just installed 7.6.0 and something has changed and what used

    to work perfectly now erroneously puts net names all over my busses in some

    cases..... I'll tidy up my script and generate a simple test schematic and

    pop it over to CadSoft as I think this must be a newly introduced bug.

     

    Many thanks,

     

    Rachael

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>