Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Why do I need to draw the same symbol N times?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 189 subscribers
  • Views 2821 views
  • Users 0 members are here
Related

Why do I need to draw the same symbol N times?

autodeskguest
autodeskguest over 10 years ago

More often than not the same chip is available in different packages,

quite often with different number of pins and the packages with fewer

pins omit some of the lesser used signals.

 

Currently, you need to create a different symbol for every package: if

you have a chip that comes in 5 different packages, with a few pin

differences, you need a symbol drawn for ABC1234-SOIC, ABC1234-BGA,

ABC1234-TSOP and so on. It's the same damn chip, just on some packages

some pins are missing.

 

I wonder if I'm alone with the wish of having just one symbol, with

every possible signal drawn. Then, when it gets placed to the schematic

with a package selected, the not bonded pins grey out and don't allow

wires to be connected to them?

--

Zoltán Kócsi

Bendor Research Pty. Ltd.

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 10 years ago

    On Fri, 23 Sep 2016 08:47:48 +0200

    Morten Leikvoll <mleikvol@yahoo.nospam> wrote:

     

    You dont need to redraw the symbol. You just create a new component

    and add the symbol + all the packages that work with this symbol at

    the same component, then connect them correctly. This works, even if

    some packages have more gnd/shield pins, cause every package is

    connected separately.

     

    As Rik Steenwinkel pointed out, that doesn't work with very many chips.

    Microcontrollers, FPGAs, power supply chips being ominous examples.

    Micros more often than not drop/gain a few port pins between package

    variants. FPGAs ditto. Power supply chips often drop rarely used

    feature pins. SPI FLASH chips tend to have a 'BUSY' signal on the higher

    pincount package, which is dropped if you go to the smallest

    pincount/footprint one. So the list is quite long.

     

    In my original post I was specifically talking about packages with

    different pin counts and signal pins going missing in the smaller

    package.

     

    But currently (7.x), if the symbol differs slightly betweeen

    packages, you have to copy/make a new symbol, and add/remove pins.

     

    Exactly. As it has always been the case. Hence my request: I'd like to

    draw only one symbol and assign a package, even if the symbol has

    more pins than the package. Then the schematics could grey out or even

    completely hide the pins that are not available on the package.

     

    In the software world copy-paste-massage-ing code is one of the cardinal

    sins, and rightly so, why am I forced to do it with my hardware?

    --

    Zoltán Kócsi

    Bendor Research Pty. Ltd.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to autodeskguest

    zoltan wrote on Sun, 25 September 2016 01:53

    Hence my request: I'd like to

    draw only one symbol and assign a package, even if the symbol has

    more pins than the package. Then the schematics could grey out or even

    completely hide the pins that are not available on the package.

     

     

    By the time you specify which pins should be greyed out, you might as well

    have made the minor modifications from the symbol with a little more or

    little less pins.  If you're only changing a few pins, there isn't really a

    problem to solve here.

     

    You don't want Eagle to just assume that you intentionally used a symbol

    with too many pins and not show you the remaining ones.  That would

    circumvent useful error checking.  Also, if a different chip has fewer

    pins, you most likely want to draw the symbol differently.  You may want to

    make it a little smaller, change some of the labeling inside the symbol,

    etc.

     

    A good example is a voltage regulator.  The simple 3-pin variety can be

    drawn more simply and smaller than one with a shutdown input, for example.

    I wouldn't want the simple 3-pin version burdened with a greyed out

    shutdown input.  I also wouldn't want it drawn bigger with inexplicable

    extra space in the 3-pin usage case.

     

    If the symbols are similar except for a few pins, then there isn't really a

    problem here.  Copy and edit works fine.  If the symbols are substantially

    different, then you're going to have to do some work for each case one way

    or the other.

     

    Quote:

    In the software world copy-paste-massage-ing code is one of the

    cardinal

    sins, and rightly so,

     

     

    Exactly.  This is the same thing.  Just like with software, you copy and

    paste, then make a few minor edits to adapt to details of the situation.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dukepro
    dukepro over 10 years ago in reply to autodeskguest

    On 09/25/2016 05:32 PM, Olin Lathrop wrote:

    zoltan wrote on Sun, 25 September 2016 01:53

    Hence my request: I'd like to

    draw only one symbol and assign a package, even if the symbol has

    more pins than the package. Then the schematics could grey out or even

    completely hide the pins that are not available on the package.

     

    By the time you specify which pins should be greyed out, you might as well

    have made the minor modifications from the symbol with a little more or

    little less pins.  If you're only changing a few pins, there isn't really a

    problem to solve here.

     

    Olin,

     

    The implication of extra work is not entirely accurate.  This has

    already been discussed in at least one thread that I started titled

    "Allow and Hide Unconnected Pins." in this newsgroup on December 20th of

    2014

     

    In my case, I was dealing with the MSP430 family of microcontrollers.

    Others have run into this problem on Xylinx, Atmel, and others.  This

    addresses instances where everything on the glass is the same.  The

    difference is that on smaller packages with fewer pins, some pads on the

    die are not wired to pins on the package.

     

    (back to Eagle's definition of pads and pins...)

    It is a reasonable request to create one device, draw one set of symbols

    for the most extensive package, and on smaller packages either grey out

    the pin on the symbol, or put an "x" at the connect point for those pins

    that have not been connected to a pad.

     

    At this time, Eagle does not permit one to choose a package that has

    fewer pads than the device's symbols have pins.

     

    There is no extra work involved - the relationship between pads on the

    package and pins on the symbol established in the library editor must be

    done regardless of whether are more pins than pads, more pads than pins,

    or an equal number of each.

     

    Jorge,  Is there any chance of refreshing this request?

     

     

     

    You don't want Eagle to just assume that you intentionally used a symbol

    with too many pins and not show you the remaining ones.  That would

    circumvent useful error checking.

     

    I also don't want Eagle to assume that using a package without enough

    pads is prohibited.

     

    An alert box in the library editor can verify the choice.

     

     

      Also, if a different chip has fewer

    pins, you most likely want to draw the symbol differently.  You may want to

    make it a little smaller, change some of the labeling inside the symbol,

    etc.

     

    You actually make a good argument for having the choice available to

    reuse a larger symbol, or design separate symbols.  It would be nice to

    have the ability to use a smaller package.  Whether one chooses to use

    that feature is up to the designer.

     

    There are many cases where one might start out a uC design with a

    smaller package, and promote to a larger package as the design

    develops.  Feature creep can cause this.

     

    On more than one occasion I have designed embedded systems to accept

    multiple packages of the same IC.  This allows the same design to

    survive unavailability of parts.  i.e. If I can get by with a QFP48,

    I'll also overlay the same package with a QFP64, or QFP80.  If the

    optimal 48-pin package is out of stock, production can drop in a 64 and

    keep rolling.

     

    Sure, it takes up a bit more real estate, but it beats having to spin

    another board and qualify it while production is waiting.

     

    A good example is a voltage regulator.  The simple 3-pin variety can be

    drawn more simply and smaller than one with a shutdown input, for example.

    I wouldn't want the simple 3-pin version burdened with a greyed out

    shutdown input.  I also wouldn't want it drawn bigger with inexplicable

    extra space in the 3-pin usage case.

     

    If the symbols are similar except for a few pins, then there isn't really a

    problem here.  Copy and edit works fine.  If the symbols are substantially

    different, then you're going to have to do some work for each case one way

    or the other.

     

    I think you're overestimating the work involved.  The proposed feature

    reduces work - one does not have to create a separate device for each of

    the very similar symbols that also have to be created.  The idea is one

    device, one set of symbols, and variations in package connections.

     

    In my suggestion in December of 2014, I stated that the unused pins (on

    the symbol) should not be shown.  I later refined this to state that

    these pins should either be greyed, or have an "x" at the connection

    point, or both.  As you pointed out, it can introduce errors if the pins

    are simply not shown.

     

    Regards,

        - Chuck

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dukepro
    dukepro over 10 years ago in reply to autodeskguest

    On 09/25/2016 05:32 PM, Olin Lathrop wrote:

    zoltan wrote on Sun, 25 September 2016 01:53

    Hence my request: I'd like to

    draw only one symbol and assign a package, even if the symbol has

    more pins than the package. Then the schematics could grey out or even

    completely hide the pins that are not available on the package.

     

    By the time you specify which pins should be greyed out, you might as well

    have made the minor modifications from the symbol with a little more or

    little less pins.  If you're only changing a few pins, there isn't really a

    problem to solve here.

     

    Olin,

     

    The implication of extra work is not entirely accurate.  This has

    already been discussed in at least one thread that I started titled

    "Allow and Hide Unconnected Pins." in this newsgroup on December 20th of

    2014

     

    In my case, I was dealing with the MSP430 family of microcontrollers.

    Others have run into this problem on Xylinx, Atmel, and others.  This

    addresses instances where everything on the glass is the same.  The

    difference is that on smaller packages with fewer pins, some pads on the

    die are not wired to pins on the package.

     

    (back to Eagle's definition of pads and pins...)

    It is a reasonable request to create one device, draw one set of symbols

    for the most extensive package, and on smaller packages either grey out

    the pin on the symbol, or put an "x" at the connect point for those pins

    that have not been connected to a pad.

     

    At this time, Eagle does not permit one to choose a package that has

    fewer pads than the device's symbols have pins.

     

    There is no extra work involved - the relationship between pads on the

    package and pins on the symbol established in the library editor must be

    done regardless of whether are more pins than pads, more pads than pins,

    or an equal number of each.

     

    Jorge,  Is there any chance of refreshing this request?

     

     

     

    You don't want Eagle to just assume that you intentionally used a symbol

    with too many pins and not show you the remaining ones.  That would

    circumvent useful error checking.

     

    I also don't want Eagle to assume that using a package without enough

    pads is prohibited.

     

    An alert box in the library editor can verify the choice.

     

     

      Also, if a different chip has fewer

    pins, you most likely want to draw the symbol differently.  You may want to

    make it a little smaller, change some of the labeling inside the symbol,

    etc.

     

    You actually make a good argument for having the choice available to

    reuse a larger symbol, or design separate symbols.  It would be nice to

    have the ability to use a smaller package.  Whether one chooses to use

    that feature is up to the designer.

     

    There are many cases where one might start out a uC design with a

    smaller package, and promote to a larger package as the design

    develops.  Feature creep can cause this.

     

    On more than one occasion I have designed embedded systems to accept

    multiple packages of the same IC.  This allows the same design to

    survive unavailability of parts.  i.e. If I can get by with a QFP48,

    I'll also overlay the same package with a QFP64, or QFP80.  If the

    optimal 48-pin package is out of stock, production can drop in a 64 and

    keep rolling.

     

    Sure, it takes up a bit more real estate, but it beats having to spin

    another board and qualify it while production is waiting.

     

    A good example is a voltage regulator.  The simple 3-pin variety can be

    drawn more simply and smaller than one with a shutdown input, for example.

    I wouldn't want the simple 3-pin version burdened with a greyed out

    shutdown input.  I also wouldn't want it drawn bigger with inexplicable

    extra space in the 3-pin usage case.

     

    If the symbols are similar except for a few pins, then there isn't really a

    problem here.  Copy and edit works fine.  If the symbols are substantially

    different, then you're going to have to do some work for each case one way

    or the other.

     

    I think you're overestimating the work involved.  The proposed feature

    reduces work - one does not have to create a separate device for each of

    the very similar symbols that also have to be created.  The idea is one

    device, one set of symbols, and variations in package connections.

     

    In my suggestion in December of 2014, I stated that the unused pins (on

    the symbol) should not be shown.  I later refined this to state that

    these pins should either be greyed, or have an "x" at the connection

    point, or both.  As you pointed out, it can introduce errors if the pins

    are simply not shown.

     

    Regards,

        - Chuck