EAGLE User Support (English) How to Unlock components from the command line (or script).
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
  • Replies 14 replies
  • Subscribers 183 subscribers
  • Views 4175 views
  • Users 0 members are here
Related

How to Unlock components from the command line (or script).

dukepro
dukepro over 8 years ago

 

Eagle 7.7.0

 

It's clear how one can lock the position of components from the command

line:

 

    Lock LED1 LED2 LED3;

 

But what is not clear is to how to unlock it.  Thus far, I have tried:

 

    Lock -LED1      # Unkown element: -

    Lock S LED1     # Unknown element: S

    Lock (S) LED1   # Invalid point: (S) LED1

    Lock (S LED1)   # Invalid point: (S LED1)

 

What I'd like to see is:

 

    Unlock LED1 LED2 LED3;

 

Ideas? Suggestions?

 

Thanks for the help.

 

    - Chuck

 

Attachments:
5140.att1.html.zip
  • Sign in to reply
  • Cancel

Top Replies

  • WarrenBrayshaw
    WarrenBrayshaw over 7 years ago +2
    Hi There is another way. If the following is in the command line LOCK (S@) and then you position the mouse over the locked element and hit enter, the element is unlocked. @ means, 'at the current cursor…
  • rachaelp
    rachaelp over 7 years ago in reply to dukepro +2
    Hi Chuck, I'm not sure why GitLab isn't working for you, it seems to be fine for me. I can send you a copy of the repository, no problem. Do you still have the same email address? If so I can send you…
  • autodeskguest
    autodeskguest over 7 years ago in reply to autodeskguest +1
    On 26.07.2018 13:40, Morten Leikvoll wrote: On 26.07.2018 13:38, Morten Leikvoll wrote: On 04.07.2017 00:13, Chuck Huber wrote: Eagle 7.7.0 It's clear how one can lock the position of components from the…
  • rachaelp
    rachaelp over 8 years ago

    Hi Chuck,

     

    You could use ULP and write an unlock function to retrieve the X and Y coordinates of each refdes passed as a parameter and then exit with LOCK (S X Y) for each one but I don't know of an existing command.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 8 years ago in reply to rachaelp

    Hi Chuck,

     

    I expect you've got this sorted now anyway but I've added another ULP to my library to create an unlock command. The usage is:

     

    RUN unlock LED1 LED2 LED3

     

    You can find the detail here if you would like it: EAGLE ULP Utilities Library

     

    There is a link to the GIT repository containing my library near the top, the usage instructions for all my released library utilities are documented on that page.

     

    Best Regards,


    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 8 years ago in reply to rachaelp

    rachaelp wrote on Tue, 04 July 2017 09:24

    Hi Chuck,

     

    I expect you've got this sorted now anyway but I've added another ULP

    to my library to create an unlock command.

     

    Snip.....

     

     

    Ugggh, the Element14 -> NNTP bridge really mangled that one very badly,

    sorry about that....

     

    You can find the documentation for my EAGLE ULP library here:

     

    https://www.element14.com/community/people/rachaelp/blog/2017/03/03/eagle-ulp-utilities-library

     

    And the GIT repository is here:

     

    https://gitlab.com/rachaelp/eagle-utils

     

    Best Regards,

     

    Rachael

     

    --

    EAGLE support forums at http://www.eaglecentral.ca :: Where the EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shekharkarmarkar
    shekharkarmarkar over 7 years ago

    There is simple way to unlock components. Select component > Right click and go to properties. Uncheck lock. That is all.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 7 years ago in reply to shekharkarmarkar

    shekharkarmarkar  wrote:

     

    There is simple way to unlock components. Select component > Right click and go to properties. Uncheck lock. That is all.

    The question was about unlocking components form the command line or a script, i.e. when you are automating something. Of course you can do it from the context menu, or the properties but that doesn't help with automation.

     

    That is all image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • WarrenBrayshaw
    WarrenBrayshaw over 7 years ago

    Hi

    There is another way.

    If the following is in the command line

    LOCK (S@)

    and then you position the mouse over the locked element and hit enter, the element is unlocked.

    @ means, 'at the current cursor position'.

    That's a command line option but not much different to the mouse right click and selecting 'Unlock'

     

    If you then assign a key combination to cause the  LOCK (S@) , then the action to unlock an element becomes:

    Position mouse over the locked element and then depress the key combination that runs LOCK (S@)

     

    Warren

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 7 years ago

    Hi,

     

    late but ...

     

    Chuck Huber wrote:

    Eagle 7.7.0

     

    It's clear how one can lock the position of components from the command

    line:

     

       Lock LED1 LED2 LED3;

     

    But what is not clear is to how to unlock it.  Thus far, I have tried:

     

       Lock -LED1      # Unkown element: -

       Lock S LED1     # Unknown element: S

       Lock (S) LED1   # Invalid point: (S) LED1

       Lock (S LED1)   # Invalid point: (S LED1)

     

    What I'd like to see is:

     

       Unlock LED1 LED2 LED3;

     

    Ideas? Suggestions?

     

    if you are ok with something like "run unlock LED1 ..." you could

    write an ULP that groups the given parts using the setgroup() function

    and then issues an "lock (>0 0)" on exit.

     

    something like the following would be my first try

    beware: not tested at all!

     

         board(BRD) {

           clrgroup(BRD);

     

         BRD.elements(ELM) {

             if (ELM.name == argv[1]) {

               setgroup(ELM);

               exit("lock (>0 0);");

             }

           }

         }

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 7 years ago

    On 04.07.2017 00:13, Chuck Huber wrote:

     

    Eagle 7.7.0

     

    It's clear how one can lock the position of components from the command

    line:

     

        Lock LED1 LED2 LED3;

     

    But what is not clear is to how to unlock it.  Thus far, I have tried:

    (stuff deleted)

     

    I dont know if it an sw accident, and it is probably just a curiosity

    and of no practical use, but this works on 7.7.0:

     

    Type

         Lock

    then immediately follow up with

         (S@)

     

    ...and it gets unlocked! But the mouse pointer needs to be within the

    window for it to work.. Maybe there are other side effects that can be

    explored..

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 7 years ago in reply to autodeskguest

    On 26.07.2018 13:38, Morten Leikvoll wrote:

    On 04.07.2017 00:13, Chuck Huber wrote:

     

    Eagle 7.7.0

     

    It's clear how one can lock the position of components from the

    command line:

     

        Lock LED1 LED2 LED3;

     

    But what is not clear is to how to unlock it.  Thus far, I have tried:

    (stuff deleted)

     

    I dont know if it an sw accident, and it is probably just a curiosity

    and of no practical use, but this works on 7.7.0:

     

    Type

        Lock <refdes>

    then immediately follow up with

        (S@)

     

    ...and it gets unlocked! But the mouse pointer needs to be within the

    window for it to work.. Maybe there are other side effects that can be

    explored..

     

     

    Having just said that, here seems to be the solution to unlock!:

    "lock  (S@);"

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 7 years ago in reply to autodeskguest

    On 26.07.2018 13:40, Morten Leikvoll wrote:

    On 26.07.2018 13:38, Morten Leikvoll wrote:

    On 04.07.2017 00:13, Chuck Huber wrote:

     

    Eagle 7.7.0

     

    It's clear how one can lock the position of components from the

    command line:

     

        Lock LED1 LED2 LED3;

     

    But what is not clear is to how to unlock it.  Thus far, I have tried:

    (stuff deleted)

     

    I dont know if it an sw accident, and it is probably just a curiosity

    and of no practical use, but this works on 7.7.0:

     

    Type

         Lock <refdes>

    then immediately follow up with

         (S@)

     

    ...and it gets unlocked! But the mouse pointer needs to be within the

    window for it to work.. Maybe there are other side effects that can be

    explored..

     

    Having just said that, here seems to be the solution to unlock!:

    "lock <refdes> (S@);"

     

    Damn, I was too quick.. My mouse pointer was too close to the device I

    was playing with. Both my suggestions fail if the pointer is closer to a

    different device.. Sorry for the alarm image

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
>