Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Error using Mirror tool.. ...
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 189 subscribers
  • Views 1327 views
  • Users 0 members are here
Related

Error using Mirror tool.. ...

e14 Contributor
e14 Contributor over 9 years ago

Hi All,

 

I'm using Eagle v6.6.0 standard edition, and I'm encountering an error when

I try to move a component to the backside of the board using the mirror

tool. The error is "The Standard Edition of Eagle cannot perform the

Requested operation", and "Some objects extend outside the allowed board

area".

 

My board size is 5" x 3.5", and the component easily fits on the frontside

of the board and Eagle is happy about it. The component outline itself is

3.7" x 2.8", so it seems like in the act of mirroring that Eagle perceives

the component to be outside the allowable area?

 

The component in question is for a GLCD module, and simply consists of a 20

pin header, 4 mounting holes, and the part outline.

 

Thanks,

 

John  

--

EAGLE support forums at http://www.eaglecentral.ca :: Where the EAGLE community meets.

 

  • Sign in to reply
  • Cancel
Parents
  • rachaelp
    rachaelp over 9 years ago

    Hi John,

     

    Is the package centred on it's origin or has the package been created with the origin on one corner? If it's been placed on a corner then mirroring it will mirror it on that corner such that part of the part would end up partially outside the board. If this is the case then you'll need to edit the part to centre it so that when it's mirrored it mirrors about its centre and sits directly below where it was on the bottom side.

     

    Best Regards,


    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rachaelp
    rachaelp over 9 years ago

    Hi John,

     

    Is the package centred on it's origin or has the package been created with the origin on one corner? If it's been placed on a corner then mirroring it will mirror it on that corner such that part of the part would end up partially outside the board. If this is the case then you'll need to edit the part to centre it so that when it's mirrored it mirrors about its centre and sits directly below where it was on the bottom side.

     

    Best Regards,


    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 9 years ago in reply to rachaelp

    Hi Rachel,

     

    OK, many thanks! Yes, the part has its origin at one corner, so I'm sure

    that is what is going on! This origin location is desirable for placement

    purposes, but I can work around that issue as long as I can get the part on

    the backside!

     

    Thanks,

     

    John

    --

    EAGLE support forums at http://www.eaglecentral.ca :: Where the EAGLE community meets.