Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Version 10MM
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 188 subscribers
  • Views 1122 views
  • Users 0 members are here
Related

Version 10MM

abvadax
abvadax over 7 years ago

JUst completed PCB using eagle. All CAM files completed and zipped to ship for quote.

I need 20 boards. Files attached.

How do I begin?

Attachments:
version 10MM board_2019-02-16.zip
  • Sign in to reply
  • Cancel
Parents
  • shabaz
    shabaz over 7 years ago

    Hi Anthony,

     

    Please see here, and contact them directly:

    Cheapest PCB makers, low volume

     

    However, you should double-check if you need to do anything with the RST pin or not, for the module you're using - it seems you've left it disconnected.

    I've not used this module, so this is just a suggestion - maybe you've already confirmed.

    image

    Also, it's bad practice to have all traces at 6mil, usually at least the power traces are thickened, and all traces look autorouted and component placement could also be better.

    For an initial prototype it may work enough to get by.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to shabaz

    Maybe turn C1, C10, C12 and C18 180°? And give T1 a quarter inch turn to the right?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to shabaz

    Maybe turn C1, C10, C12 and C18 180°? And give T1 a quarter inch turn to the right?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to abvadax

    abvadax  wrote:

     

    Thank you for those suggestions. I will  manually make the changes.

    Regards

    ABvadax

    They are suggestions - a few things I would change if it was me doing the layout.

    I'm not opposed to auto routing by the way. For commercial designs, if auto mode delivers a board that is within specs, regulations and costs, there is nothing that can beat it.

    Many people will criticise the layout then, but economically and business wise, any minute spent to improve by a designer may not return its value.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • abvadax
    abvadax over 7 years ago in reply to Jan Cumps

    Thank you for those suggestions. I will  manually make the changes.

    Regards

    ABvadax

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 7 years ago in reply to Jan Cumps

    On 17/02/2019 09:31, Jan Cumps wrote:

    Maybe turn C1, C10 and C18 180°?

     

    And C4, C13, C21

     

    And give T1 a quarter inch turn to the right?

     

    C15 and D6 would benefit from a quarter turn right, maybe C14 too.

     

    C19 should be rotated right and moved to the end of IC3, where it can do

    its job of being a LOCAL decoupling capacitor, although what it's

    decoupling is unclear.

     

    Without the schematic it's very hard to say how many other mistakes

    there are. I suspect this board has not had sufficient care or attention

    paid in any aspect, given the sloppy approach to part placement and routing.