Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum CadSoft EAGLE development team developing XML format for schematic, layout and parts libraries!
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 30 replies
  • Subscribers 191 subscribers
  • Views 8035 views
  • Users 0 members are here
  • farnell
  • pcb_layout
  • pcb
  • open
  • Design
  • source
  • open_source_hardware
  • eagle_pcb
  • cadsoft
Related

CadSoft EAGLE development team developing XML format for schematic, layout and parts libraries!

e14 Contributor
e14 Contributor over 16 years ago

hello makers -

 

this is my first post here, i'm the senior editor at MAKE magazine and also the creative director at adafruit. i've been part of a growing movement called "open-source hardware" for the last 5 years or so. today we just got some great news from the CadSoft EAGLE development team about the their long term commitment to text based file formats in the world of electronics development. with their permission i am posting this here and on MAKE (as well as adafruit). it's extremely exciting for those of us who wanted an XML format for files and we're thrilled CadSoft EAGLE has said they're committed to it!

 

here's the overview of what we learned:

 

  • CadSoft EAGLE (our preferred schematic/layout software) has told us they are committed to a text based format in the long term.
  • The CadSoft EAGLE development team is developing a new format for schematic, layout and parts libraries that is XML, this means every object and line will be written out in text description.
  • You won't have to worry about binary file corruption, you will be able to hand-edit or generate schematics and layouts and of course the magic of version-control (such as github) will be easier than ever with real text 'diff's!
  • This will be a fully documented format and also of course a converter for old CadSoft EAGLE binary-type formats.

 

 

this is a great direction and i encourage you to support EAGLE as you decide which tools to use now and in the future. but that's not all, i've chatted with the element-14 folks and they're all set up for your feedback, if they're very interested in Maker voices their product development. so here's your chance folks!

 

cheers,

pt

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    I'm all for openness and transparency in data files. If the data in your text file is large, though, then it can get pretty nasty for a human to parse and edit. I consitently deal with verilog netlists that are on the order of 100Mb in size for our ASICs at work. In fact, lots of files for my job are text (SPEF, netlist, DEF, LEF, LIB). We don't edit netlists by had because they are too large and complicated. We use EDA tools to manually manipulate netlists with languages like TCL (edit netlist disconnect, edit netlist connect, edit netlist create and_gate). I would recommend supporting the reading and writing of compressed XML files out of the gate. Why waste 100MB of disk space when gzip will compress it down to 2MB? Most linux distros command line utils/editors support auto decompress of gzipped files. But I guess that doesn't apply to windows very well. Since all my EDA work is on linux (none of the asic tools support windows), I tend to foget it exists for other eda industries like PCB.

     

    I don't think you can claim checking them into a revision control system as a feature/positive. The text in a file can look completely different to "diff", but still represent the exact same design data. The same net coordinates can live on line 5 or line 5,000,000 and still represent the same thing. We check in our text verilog netlists to RCS at work, but the diffs usually end up being 95% different despite only having 3 new logic gates added. Might as well been a binary file at those diff rates. Now if you can guarentee exact text formatting and order from output to output, then this diff issue obviously goes away.

     

    That being said, it is great when I run across an EDA vendor using a straight forward text file for a input or output file. Did you board dimentions change, but you want to keep all the x,y coordinates of your components? Start up a new board and draw the dimenstions, then save to a text file. Rip out the old componet coordinate section from the old text file and and place it in the new one and vola! Instant component placements! ( this is a somewhat bad example since you can just take your board file and edit the dimensions with components in place - but I think you get my point).

     

    BTW - I love eagle cad. Any chance you guys could get a graphics designer to re-work your icons? Nothing says polished tool like professional and modern icons. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    XML diff works best if you enforce lang-based sorting of the hierarchy.  For example, if you have a lib-cells-views-insts structure, the cells will always appear in the same cell-name alphanum order, the views will always appear in the same view-name alphanum order, and most importantly all the instances will appear in the inst-name alphanum sorted order.  For coordinates-based diffs, graphical structures could stick to a numerically-sorted order, like X-coord then Y-coord, or worst case a brute-force XOR/intersection operation using something like Java's built-in Area class boolean ops.

     

    Worst-case, build the enforced sorting mechanism into the revision control front-end.  There's always a way! image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    i'm excited and the goal of this post was to get people talking about this - success!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    i'm excited and the goal of this post was to get people talking about this - success!