Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum help for the create script
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 188 subscribers
  • Views 561 views
  • Users 0 members are here
Related

help for the create script

e14 Contributor
e14 Contributor over 15 years ago
Hello friends
I need your help for the create script for the EAGLE
I use this command (Bill Of Material : RUN BOM-AM-17.ulp; | \) from scripr to run a ULP file and it works properly
The problem is that I want to execute ULP that is found in my own folder in located in C: \ Program Files \ EAGLE-5.11.0 \ eagle3d \
How to write the RUN command to include the path that I
Please help me thanks
 
my script eagle.scr
----------------------------------------------------------------------
# Board Command Menu Setup
# Also includes widths and diameters
#
# Created 09/01/2011
SCH:
Grid Default;
Change Width 0.006;
Grid  On
MENU  ' Grid {\
  (1) = 0.05 : Grid inch 0.05;|\
  (2) = 0.01 : Grid inch 0.01;|\
  (3) = 0.001 : Grid inch 0.001;|\
  (4) = Default : Grid inch 0.1;|\
  --- |\
  Grid  On : GRID LINES On; | \
  Grid  Off : GRID LINES Off;\
  }' \
  'Tools {\
              Create Frame : RUN create-frame_v1.0.2.ulp; | \
  Re Annotate : RUN 00-Reannotate-sch.ulp; | \
              Bill Of Material : RUN BOM-AM-17.ulp; | \
  Auto place sheet : RUN APS.ulp;  \
           }'\
  • Sign in to reply
  • Cancel
Parents
  • Richard_H
    Richard_H over 15 years ago

    Hi,

     

    you have to include the path into quotes, if there are spaces in it, for example:

    RUN "C:\Program Files\EAGLE-5.11.0\eagle3d\test.ulp" ;

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to Richard_H
    Hi Richard_H
    Thank you very much for your reply
    I tried the command (RUN "C:\Program Files\EAGLE-5.11.0\eagle3d\3d41.ulp"  but it turns out error
     
    image
     
    He has a problem with Program Files folder It cannot occupy him
    I tried the command (run C:\Program_Files\EAGLE-5.11.0\eagle3d\3d41.ulp)
    again gave an error message for non-existent file
     
    image
     
    but the file exists, I can not understand why
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 15 years ago in reply to e14 Contributor

    Hi again,

     

    the problem here is that the path contains a space  character between Program and Files. So you have to start the ULP with  the RUN command and put the whole path into single quotes (I used double  quotes in my first post, sorry...).

    RUN 'C:\Program Files\EAGLE-5.11.0\eagle3d\test.ulp' ;

     

    There  could be also a second problem. I don't know the ULP you are working  with, but i could also be the case that you have to verify the ULP   itself. If there are some statements that are referring to files the   paths there have to be set into single quotes as well. So please check   the ULP for this.

     

    Best regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Richard_H
    Richard_H over 15 years ago in reply to e14 Contributor

    Hi again,

     

    the problem here is that the path contains a space  character between Program and Files. So you have to start the ULP with  the RUN command and put the whole path into single quotes (I used double  quotes in my first post, sorry...).

    RUN 'C:\Program Files\EAGLE-5.11.0\eagle3d\test.ulp' ;

     

    There  could be also a second problem. I don't know the ULP you are working  with, but i could also be the case that you have to verify the ULP   itself. If there are some statements that are referring to files the   paths there have to be set into single quotes as well. So please check   the ULP for this.

     

    Best regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to Richard_H
    Hi again friend Richard_H
    Thank you for your help
    I understood that what I ask is above the possibilities that it offers the EAGLE
    I will send e-mail with the problem that I face in cadsoft
    I do not wait solution in my problem from cadsoft  I will try
     
    (If I find the solution I will put here him to see whoever is interested)
     
    Thank you again friend Richard_H
    toths