Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum EagleCad external wire
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 189 subscribers
  • Views 1275 views
  • Users 0 members are here
  • eaglecad
Related

EagleCad external wire

e14 Contributor
e14 Contributor over 12 years ago

Hi! I'm new to EagleCad. I'm getting my first board ready to print. I have a separate circuit that I am going to need to connect to this pcb by a wire. It would be nice if I could have it wired to a hole in the board I could then solder my wire through.  How do you designate this in the software or is there a better way to do it?

  • Sign in to reply
  • Cancel
  • Fred27
    Fred27 over 12 years ago

    I tend to use a pin header (from the pinhead library if I remember correctly) as you can include this is your schematic. Whilst they're intended for placing a 0.1" pitch header row I find they're also ideal if you want a wire - or more likely wires. The solder pads and holes are a nice size.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to RayA

    Thanks Ray! I haven't worked with any electronics in 3 or 4 years so I'm trying to get back into it. It's a slow process so every bit helps.

     

    Your advice is exactly what I was looking for, thank you!

     

    Best,

    Tom

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • RayA
    RayA over 12 years ago

    Hi Tom,

    I'll chime in here, just in case you haven't already found the answer.

     

    The best way to place a hole to solder a wire into is just the same as placing any other component. Take a look in the "Wirepad" library, and you'll find a selection of different sized holes with copper pads around them. Place one on the schematic, and it will also show up in the board layout with a connected airwire for you to route.

     

    A second way that also works, is to do it all in the layout editor. Just place a "Via" wherever you want to solder in your wire, then either use the "Wire" tool or the "Route" and "Split" tools to connect that via to the correct a trace on your layout. You can use the "Info" tool to adjust the size and shape of the via. Doing it this way, it will not show up on your schematic.

     

    Ray