Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
Forum Reticon SAD1024 Delay Chip
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 39 replies
  • Answers 14 answers
  • Subscribers 203 subscribers
  • Views 13639 views
  • Users 0 members are here
Related

Reticon SAD1024 Delay Chip

Andy Betts
Andy Betts over 9 years ago

Reaching out to the people on this web site.......

 

I'm after a SAD1024 delay chip, they were manufactured by Reticon and are now discontinued, and have been for around 30 years. I'm hoping someone here may have one lying around....... if so can you get back to me and I'll make you an offer to buy it off you.

 

As a heads up this is required for a planned pedal build, for the near future, but it all rests on being able to obtain this IC chip.

 

The data sheet is available to read here

 

http://www.pmerecords.com/Docs/Archer_SAD-1024_Tech_Data.pdf

  • Sign in to reply
  • Cancel
Parents
  • jw0752
    0 jw0752 over 9 years ago

    Hi Andy,

    I checked and I do not have this chip. Apparently it was sold for a while by Radio Shack under stock number 276-1761. There was some talk on the following link about using a MN3007 as a possible substitute.

     

    http://music-electronics-forum.com/t23353/

     

    I see that there are two or three listed on ebay but the sellers know they have little pieces of gold judging by the price tags.

     

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 9 years ago in reply to jw0752

    Andy,

    You may know these people:

     

    Small Bear Electronics

     

    They have clones of the MN3207 chip.

     

    Why must you have the SAD1024, can you post the circuit of the thing you want to build. It is possible to make a replacement for the SAD1024 using an ADC, tiny FPGA and DAC - it won't be the same size (on a hobby budget) but would work fine, and offer all sorts of other possibilities.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andy Betts
    0 Andy Betts over 9 years ago in reply to michaelkellett

    Hi Michael

     

    Yeah, I know small bear... US supplier, and expensive to get shipped over to the UK.

     

    The circuit is attached

     

    image

     

    From what I understand, the SAD1024 is pretty peculiar to this circuit, however if there's a good substitute I'm willing to look into that.

     

    Original SAD chips are expensive, for that very reason....... They are gold

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 9 years ago in reply to michaelkellett

    Oh I see.. I hadn't realized that is what a flanger did : (

    I guess at some stage it just makes sense to do all this in software on a PC or DSP. I have a friend who works in the sound industry, he uses some fancy gear to generate virtually any sound programmatically, essentially a DSP connected to a PC, and he downloads either instructions or scripts to it. But, at the same time he also uses low-tech too, he will use a mic and record anything interesting and then play with it to make the effect he is seeking.

    Motorola/Freescale had a nice dev-board (probably still available on ebay) which had a DSP (56k series, so quite old : (, enough RAM for echo-style effects, and codec, and I think a serial port for downloading the program to it. It could make a nice universal effects pedal!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 9 years ago in reply to michaelkellett

    Oh I see.. I hadn't realized that is what a flanger did : (

    I guess at some stage it just makes sense to do all this in software on a PC or DSP. I have a friend who works in the sound industry, he uses some fancy gear to generate virtually any sound programmatically, essentially a DSP connected to a PC, and he downloads either instructions or scripts to it. But, at the same time he also uses low-tech too, he will use a mic and record anything interesting and then play with it to make the effect he is seeking.

    Motorola/Freescale had a nice dev-board (probably still available on ebay) which had a DSP (56k series, so quite old : (, enough RAM for echo-style effects, and codec, and I think a serial port for downloading the program to it. It could make a nice universal effects pedal!