Forum needing help to connect a 2-pin rc-car steering motor to an adafruit pwm i2c controller
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
  • Replies 15 replies
  • Subscribers 183 subscribers
  • Views 3162 views
  • Users 0 members are here
  • raspberry pi i2c
  • servo motor
  • i2c
  • how to i2c
  • pwm
  • raspberry pi io
  • servo
  • pwm controller
Related

needing help to connect a 2-pin rc-car steering motor to an adafruit pwm i2c controller

tlucas756
tlucas756 over 8 years ago

So I saw a neat project on a magazine about controlling an rc-car wirelessly through a raspberry pi, using pwm.

I ordered everything I needed, mainly an i2c controller, and I started working on it. i am using a clone of the adafruit controller instead of a real one, because it was a lot cheaper, though the functionality remains the same.

Now, I have a problem. The article says that I need to connect the steering motor to the 3 pins on the adafruit controller, which are labeled power, ground, and PWM, but my motor only has two wires, so I have no idea what they do, or what to do next.

I do not have another rc-car to do this on. How do I connect the motor to the controller? do I need to get a different motor?

Thank you for your help!

image

imageimageimage

  • Sign in to reply
  • Cancel

Top Replies

  • beacon_dave
    beacon_dave over 8 years ago +3
    Not sure from the photo if your steering is actually a DC motor or a spring loaded solenoid. Does the steering spring back to centre if the wheels are pushed and let go ? You will also likely have problems…
  • dougw
    dougw over 8 years ago +3
    As Dave indicates a DC motor would need an H-Bridge to reverse polarity. The micro servo might work as a demo but may have problems in actual use. You need to check if the torque is enough, the speed is…
  • ninjatrent
    ninjatrent over 8 years ago +3
    The L293D h bridge will drive this type of motor. It is a very low cost part (US $2). The PCA9685 is for use with servos although as mentioned a circuit can be created. The cheapest and easiest option…
  • 14rhb
    14rhb over 8 years ago

    Tiago,

     

    You need a few extra electronic components in between the Adafruit board and your motor. Something like this:

    arduino - Control of a coreless DC motor using a PWM and a ...

    (from https://electronics.stackexchange.com/questions/176601/control-of-a-coreless-dc-motor-using-a-pwm-and-a-mosfet  )

     

    Happy building image

     

    Rod

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • 14rhb
    14rhb over 8 years ago in reply to 14rhb

    Actually I might have misled you there - I didn't notice it was the steering motor you were having trouble with (sorry).

     

    That motor might change polarity to make it turn either direction. It could be that PWM isn't the right solution for that. I think for that you need to put something else between the Adafruit PWM and your motor called an H-bridge circuit. That would allow you to control the direction that the simple DC motor can turn.

     

    Perhaps another E14 member with more knowledge of how RC cars work can comment ?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 8 years ago

    Not sure from the photo if your steering is actually a DC motor or a spring loaded solenoid. Does the steering spring back to centre if the wheels are pushed and let go ?

     

    You will also likely have problems with your speed motor as the way you have shown it connected it will result in 'max speed' in one direction.

     

    It looks like you may need a different controller or add a dual H-bridge motor driver to your PWM controller.

     

    The existing Adafruit controller is designed for controlling servo motors or dimming LED's using a PWM signal.

     

     

    You can use the PWM output however to drive the enable pin on an H-bridge driver like the L293D which will give you motor speed control and then use four GPIO pins to control the direction of each motor independently for forward/reverse and left/right

     

    https://learn.adafruit.com/adafruit-raspberry-pi-lesson-9-controlling-a-dc-motor/lm293d

    https://learn.adafruit.com/adafruit-arduino-lesson-15-dc-motor-reversing/an-experiment

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • tlucas756
    tlucas756 over 8 years ago in reply to beacon_dave

    Thank ypu for responding!

     

    the motor might be a DC motor, because it does not spring back when I push the wheels.

     

    Also, I have to find a quick solution to this, as I have to show this to my electronics teacher next week, and I can't get any new components in time.

     

     

    Also, I still have the original controller chip that came with the car when it was new - It's a Realtek RX2C A5081 35T, but in order to make my project work, I can't add that chip in.

    What I was thinking was to get one of those cheap arduino servos (that have 3 pins) and replace the one in my rc-car, though I'm not sure if that would work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • tlucas756
    tlucas756 over 8 years ago in reply to tlucas756

    one of these:    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 8 years ago in reply to tlucas756

    Yes, that should work with the Adafruit PWM servo controller.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 8 years ago

    As Dave indicates a DC motor would need an H-Bridge to reverse polarity.

    The micro servo might work as a demo but may have problems in actual use. You need to check if the torque is enough, the speed is adequate, and the angle of rotation is sufficient.

    If all of that is okay, the wheels can typically transmit a high spike load to the motor when one wheel hits a bump or a wall. This will often strip the plastic gears in a servo motor. Servo-savers can reduce the spike load, but it may still need metal gears.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 8 years ago in reply to dougw

    There appears to be a metal gear version of the micro servo:

    https://www.adafruit.com/product/1143

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • tlucas756
    tlucas756 over 8 years ago in reply to dougw

    would this one work? it does have metal gears.

     

    YOURobot - Servo Motor Tower Pro MG995

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 8 years ago in reply to tlucas756

    Adafruit appear to approve of them:

    https://www.adafruit.com/product/1142

    "We now carry the Tower-Pro MG-995, they are very nice, high quality servos, excellent for use in robotics."

    The question is probably more a case of can you fit it into the car in place of the existing steer motor ?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
>