Forum needing help to connect a 2-pin rc-car steering motor to an adafruit pwm i2c controller
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
  • Replies 15 replies
  • Subscribers 183 subscribers
  • Views 3159 views
  • Users 0 members are here
  • raspberry pi i2c
  • servo motor
  • i2c
  • how to i2c
  • pwm
  • raspberry pi io
  • servo
  • pwm controller
Related

needing help to connect a 2-pin rc-car steering motor to an adafruit pwm i2c controller

tlucas756
tlucas756 over 8 years ago

So I saw a neat project on a magazine about controlling an rc-car wirelessly through a raspberry pi, using pwm.

I ordered everything I needed, mainly an i2c controller, and I started working on it. i am using a clone of the adafruit controller instead of a real one, because it was a lot cheaper, though the functionality remains the same.

Now, I have a problem. The article says that I need to connect the steering motor to the 3 pins on the adafruit controller, which are labeled power, ground, and PWM, but my motor only has two wires, so I have no idea what they do, or what to do next.

I do not have another rc-car to do this on. How do I connect the motor to the controller? do I need to get a different motor?

Thank you for your help!

image

imageimageimage

  • Sign in to reply
  • Cancel

Top Replies

  • beacon_dave
    beacon_dave over 8 years ago +3
    Not sure from the photo if your steering is actually a DC motor or a spring loaded solenoid. Does the steering spring back to centre if the wheels are pushed and let go ? You will also likely have problems…
  • dougw
    dougw over 8 years ago +3
    As Dave indicates a DC motor would need an H-Bridge to reverse polarity. The micro servo might work as a demo but may have problems in actual use. You need to check if the torque is enough, the speed is…
  • ninjatrent
    ninjatrent over 8 years ago +3
    The L293D h bridge will drive this type of motor. It is a very low cost part (US $2). The PCA9685 is for use with servos although as mentioned a circuit can be created. The cheapest and easiest option…
  • tlucas756
    tlucas756 over 8 years ago in reply to beacon_dave

    I was planning on tearing the motor apart and only salvage the motor itself, because the assembly of the motor in the car already has the gears inside.

     

    Though, if I'm gonna do that, I'll just get the cheaper one, since I won't be using the metal gears

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • ninjatrent
    ninjatrent over 8 years ago

    The L293D h bridge will drive this type of motor. It is a very low cost part (US $2). The PCA9685 is for use with servos although as mentioned a circuit can be created. The cheapest and easiest option would be to purchase an L293D h bridge.

    https://www.adafruit.com/product/807

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 8 years ago in reply to tlucas756

    Ok - are you familiar with what's inside a servo motor though ?

     

    If not then you may want to take a quick look at this video:

    https://www.youtube.com/watch?v=9cvCRnVFpnA

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 8 years ago in reply to tlucas756

    The servo needs the rest of the internal circuitry to work like a servo. If you just use the motor, you will need the H-bridge just like any other DC motor.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • ninjatrent
    ninjatrent over 8 years ago

    Hi Tiago,

     

    I have the Adafruit version of this part.

     

    I have also experienced taking a rc car apart to find this type of 6V motor for steering control. It is not as precise as a servo. If this is the only option for your project then I would recommend a L293D or L298N Dual H Bridge Motor driver. This will handle the 6V steering and drive motors on this car.

     

    This will be easier than replacing the steering motor with a servo.

     

    The 16 channel pwm/servo driver that you have purchased is a good part for a hexapod type robot or robotic arm. With this part you could include a servo controlled arm or a camera gimbal into your project. This pwm/servo driver might also be used to control RGB LEDs.It might also be possible to use this driver to control the esc on a quadcopter drone. Even if you can't use it with your current project, it might come in handy for a future project.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
<