Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum pick and place in circuit studio
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Locked Locked
  • Replies 4 replies
  • Subscribers 89 subscribers
  • Views 1001 views
  • Users 0 members are here
  • pick and place
  • frontpage
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

pick and place in circuit studio

garonix
garonix over 7 years ago

Hello,

Is it possible to add the schematic's "value" to one more column in "pick and place" file?

I need it for my pick and place machine.

It serves to assemble sames components together.

For example all resistor of footprint 0805 and 1K value together in same place in pick and place machine.

The other solution is to concatenate the "pick and place" file and Bill Of Materials manually, but lot of mistake.

Thanks.

  • Cancel
Parents
  • e14softwareuk
    0 e14softwareuk over 7 years ago

    I don't believe there any any options to add additional data to the pick and place file. However the comment field is included in the file so it may be possible to use the comment field.

    image

    Pick and Place Data Format

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • garonix
    0 garonix over 7 years ago in reply to e14softwareuk

    It's a good idea.

    I have test it, I have change all comment in schematic to =Value.

    In PCB, I have clicked to component link and update, it says link update.

    But, if I click to a component in PCB, the comment has not changed.

    I have test the pick and place file generation, but effectively, the comment have not changed.

    It is a bug in the component Links command ?

    Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • garonix
    0 garonix over 7 years ago in reply to garonix

    I have solution for last problem: in schematic: home-> project->update PCB

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14softwareuk
    0 e14softwareuk over 7 years ago in reply to garonix

    Thanks for posting your progress. The component link command is designed to ensure that CircuitStudio can match up the components on the schematic and PCB. This is different to the Update PCB command which actually passes across any changes. Running the component link command first means means that the Update PCB command has the best change of updating everything without error.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • e14softwareuk
    0 e14softwareuk over 7 years ago in reply to garonix

    Thanks for posting your progress. The component link command is designed to ensure that CircuitStudio can match up the components on the schematic and PCB. This is different to the Update PCB command which actually passes across any changes. Running the component link command first means means that the Update PCB command has the best change of updating everything without error.