Cypress
  • Products & Partners
  • Manufacturers
  • Cypress
  • More
  • Cancel
Cypress
Forum Query
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 31 replies
  • Subscribers 10 subscribers
  • Views 5048 views
  • Users 0 members are here
Related

Query

e14 Contributor
e14 Contributor over 16 years ago
I would like to know whether the ADC in Analog modules of the PSoC features "Simultaneous Sampling". Someone please provide some information on this ...
  • Sign in to reply
  • Cancel
Parents
  • Sunnyzhuo
    0 Sunnyzhuo over 16 years ago

    the following link is base knowledge of the simultaneous samping:

     

    http://zone.ni.com/devzone/cda/tut/p/id/4105

     

    and the the following link is the simultaneous samping feature of the adc module in the cypress'psoc:

     

    DualADC_UM13555.pdf

     

    I hope they are useful to you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to Sunnyzhuo
    Thanks for the information. But we require 14 bit ADC for our application. Please suggest a correct part of PSoC and the development kit associated with it.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Oliver
    0 Oliver over 16 years ago in reply to e14 Contributor
    There is no any CY8C28xxx Serial PSoC stocked both in Farnell and Newark.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to Oliver
    Thank you very much Is part  CY8CKIT-002CY8CKIT-002 PSoC MiniProg3 available
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to Oliver
    Thank you Is part no  CY8CKIT-002CY8CKIT-002 PSoC MiniProg3 available If available then whats the price of it(in Indian rupees including taxes shipping and handling charges(if applicable And also whats the time it will take to ship the same itemt
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Oliver
    0 Oliver over 16 years ago in reply to e14 Contributor

    Yes, the Kit CY8CKIT-002 is available in Farnell and Newark, it is about 90.00USD, the order code is 26R2364 and 1753960 .

     

    I will transfer you to sale team in India, the sales engineer and custome service will contact you soon.

     

    best regards;

     

    oliver zhang

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Oliver
    0 Oliver over 16 years ago in reply to e14 Contributor

    Could you tell me your contact details (phone No. or email addr) so that the sale engineer can contact you?

     

    You can also send  an email to me (yzhang@premierfarnell.com)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to Oliver
    Thanks for the useful information. I have mailed the contact details to your official e mail id. Please find the details.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Oliver
    0 Oliver over 16 years ago in reply to e14 Contributor

    got it.

     

    Sale engineer in India will contact you soon.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to Oliver

    Hello,

     

        I have received samples of part CY8C28645 from Cypress. Its smd quad pack. how do i program the device. Is there programmer board design for the same. Please help.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to e14 Contributor
    Please someone do reply...!!
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Oliver
    0 Oliver over 16 years ago in reply to e14 Contributor

    There are two methods to program the device:

     

    1.On board program and debug: assemble the device on your PCB and you can program or debug it through ICE debugger.

     

    2. You need an adapter which can change package from QFN to DIP

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Oliver
    0 Oliver over 16 years ago in reply to e14 Contributor

    There are two methods to program the device:

     

    1.On board program and debug: assemble the device on your PCB and you can program or debug it through ICE debugger.

     

    2. You need an adapter which can change package from QFN to DIP

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to Oliver
    I am going for the second method. i.e. using an adapter to convert QFN to DIP. What are the points to be taken care while doing this ? I am using PSoC part no. CY8C28645-24LTXI in my design. Its a 48 pin QFN package. I have planned to get design a PCB with footprint of QFN package and taking the leads through the connectors for programming and other interface. Is any current limiting resistors or capacitors required while connecting the programmer to the respective pins. I am using Miniprog3 as my device programmer. please help.??!! 
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Oliver
    0 Oliver over 16 years ago in reply to e14 Contributor

    The soulution that you plan to design is the first method. I will attach a PDF file to help you design a PSoC system.

     

    By the way, I can not confirm how the Miniprog 3 connect your target board because i can not get any detailed information of it, and which conntetor used .

     

    Maybe, you want to have a look on Cypress website at:

    CY3250-286XXQFN-POD Replacement In-Circuit Emulation (ICE) Pods (2) for Debugging QFN CY8C28xxx PSoCRegistered Devices

     

    CY3250-286XXQFN: In-Circuit Emulation (ICE) Pod Kit for Debugging QFN CY8C28xxx PSoCRegistered Devices

    Attachments:
    imageICE_Pod_Schematic4[1].pdf
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to Oliver
    Thanks for the information. I have designed a board (Target board) which includes PSoC (CY8C28645-24LTXI) IC with a programming header, I/O interface header and power unit. I am using Miniprog3 for programming my device. I am programming my device in Power ON mode. After programming i am going to use my device for my application. I will be giving power to my board externally. My question is do i have to provide an external clock source also?? Or does part no. CY8C28645-24LTXI has internal clocking unit in it??
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Oliver
    0 Oliver over 16 years ago in reply to e14 Contributor

    There are some description on page 1 of Cy2C8xxx datasheet,it describes as below:

     

    • Precision, Programmable Clocking
      Internal ±2.5% 24/48 MHz Main Oscillator
      Optional 32.768 kHz Crystal for Precise On-Chip Clocks
      Optional External Oscillator, up to 24 MHz
      Internal Low Speed, Low Power Oscillator for Watchdog and
      Sleep Functionality

     

    It shows us that PSoC has internal clock, there is no need to provide the external clock source for PSoC.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to Oliver

    Hello,

     

    Thanks for the information.