TDK
  • Products & Partners
  • Manufacturers
  • TDK
  • More
  • Cancel
TDK

TDK Blog

  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join TDK to participate - click to join for free!

TDK Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • In AI Infrastructure: Compute Is Only as Powerful as What Supports it.

    Catinca - TDK
    Catinca - TDK
     Making AI servers more powerful isn't just about more powerful processors; it's about more efficient power electronics, more powerful cooling, and more data moving at ever-higher speeds. At electronicaFair 2026, discover how TDK technol...
    • 28 Oct 2026
  • A Supercomputer on Wheels. Even Gravity Can Keep it Down.

    Catinca - TDK
    Catinca - TDK
    Trillions of operations per second. In a car.But more computing power also means tougher engineering challenges: stable powerclean signals reliable control.That’s where TDK comes in.From in-vehicle networking and power for high-performance...
    • 23 Oct 2026
  • Less CO2. Same Mission: Protecting Electronics.

    Catinca - TDK
    Catinca - TDK
    ️ Less CO2. Same Mission: Protecting Electronics. Guarding sensitive electronics against overvoltages is one thing. Doing it with up to 30% lower CO₂ footprint adds another dimension to component design.Our new X series of multilayer chip varist...
    • 16 Oct 2026
  • What If You Could Find the Problem Before You Build the Drive?

    Catinca - TDK
    Catinca - TDK
     A drive is more than the sum of its components.Electrical behavior, thermal conditions, and component interactions can all influence how the final system performs. And discovering an issue after the test hardware is built can be expensive.Simul...
    • 23 Sep 2026
  • TDK expands ultra-compact snap-in capacitor series for AI servers

    Catinca - TDK
    Catinca - TDK
    ️  AI Needs More Power. Not More Space. As AI server power supplies move toward ever-higher power densities, the DC link has to keep up without taking up more valuable board space.That is where capacitor design becomes a system-level considerati...
    • 17 Sep 2026
  • TDK: System-Oriented Component Design for Industrial Drives (2)

    Catinca - TDK
    Catinca - TDK
     Good Control Starts With Knowing What's Actually Happening In a variable frequency drive, control algorithms are only as good as the signals they receive. Accurate current and temperature sensing provides the feedback needed to keep operati...
    • 31 Aug 2026
  • NEW RELEASE: TDK adds vibration-resistant axial and soldering-star capacitors for 125 V and upgrades 63 V series

    Catinca - TDK
    Catinca - TDK
    Because Every Component You Remove Makes the System Better. Designing compact 96 V battery systems isn't only about fitting more power into less space. It's about reducing complexity, improving reliability, and making every cubic centimeter count.Our...
    • 5 Aug 2026
  • DC-link capacitors with ultra-low inductance for SiC-based power electronics

    Catinca - TDK
    Catinca - TDK
    Taming SiC Starts with What You Can't See As switching frequencies increase, parasitic inductance becomes a critical design challenge. Even small amounts of ESL can contribute to voltage overshoots, additional stress on power semiconductors, and redu...
    • 29 Jul 2026
  • TDK: System-Oriented Component Design for Industrial Drives

    Catinca - TDK
    Catinca - TDK
    Variable-Speed Drives All Follow The Same Principle. Until Physics In.  At their core, variable-speed drives all do the same thing: they regulate voltage and frequency to operate electric motors efficiently.The principle is straightforward.Desig...
    • 21 Jul 2026
  • TDK introduces compact ThermoFuse varistors for surge protection of up to 50 kA

    Catinca - TDK
    Catinca - TDK
    Downtime Is Expensive. Smart Protection Isn't. With our new MT40 ThermoFuse varistors, we introduce a compact surge protection solution engineered for extreme electrical environments - delivering up to 50 kA peak surge capability in a minimized footp...
    • 9 Jun 2026
  • TDK announces two new DC link capacitor series optimized for on-board chargers in electric vehicles

    Catinca - TDK
    Catinca - TDK
       When 800V Pushes Harder, Stability Becomes a Design Decision. As EV on-board chargers move toward higher voltages and currents, DC link capacitors must deliver uncompromising performance - without increasing system size or complexity.Wit...
    • 26 May 2026
  • TDK announces the new series of DC-Link film capacitors with high thermal robustness for demanding automotive and industrial power electronics

    Catinca - TDK
    Catinca - TDK
     Power Density Without Oversizing. Built for +125°C. Next-generation power electronics, whether in xEV traction inverters, onboard chargers, or industrial converters, are pushing DC link designs to their thermal limits. That’s exactly ...
    • 14 May 2026
  • Silver price hikes! Don’t worry, TDK has the answer

    Catinca - TDK
    Catinca - TDK
    When Material Costs Spike, Engineering Decisions Matter.  Silver prices have surged and with them, the cost and risk profile of conventional piezo designs. But what if the solution isn’t about managing volatility… but eliminating de...
    • 7 May 2026
  • TDK - Redefining DC Links for Next‑Gen Power Electronics

    Catinca - TDK
    Catinca - TDK
    85 °C is not enough for next-generation DC Link Design! Power electronics are evolving faster than ever and conventional DC link capacitors are starting to hold engineers back. At the heart of this shift: wide-bandgap semiconductors (like Si...
    • 30 Apr 2026