Würth Elektronik
  • Products & Partners
  • Manufacturers
  • Würth Elektronik
  • More
  • Cancel
Würth Elektronik
Blog ANP031: Determination of the Ideal Power Inductor for Energy-Efficient Applications
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Würth Elektronik to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: sleuz
  • Date Created: 25 Jan 2016 2:18 PM Date Created
  • Views 1228 views
  • Likes 2 likes
  • Comments 0 comments
  • energy-efficient
  • power_inductor
  • power_inductor_losses
  • energy_efficiency
  • power_supply
  • switching_loss
  • low_internal_losses
Related
Recommended

ANP031: Determination of the Ideal Power Inductor for Energy-Efficient Applications

sleuz
sleuz
25 Jan 2016

Determination of the Ideal Power Inductor for Energy-Efficient Applicationsimage

 

 

 

 

ANP031 BY ALEXANDER GERFER, RANJITH BRAMANPALLI, JOCHEN BAIER

 

 

 

1. Introduction

Energy-efficient devices are important components for saving resources and protecting the environment. The more efficient the electronics, the longer the battery service life for mobile devices - and in large-scale industrial and server installations with thousands of loads, the energy requirement is markedly reduced. The basis for energy-efficient devices is essentially influenced by the power supply unit. While linear regulators still most widely used in the past were voltage regulators, mainly switch mode power supplies are found in modern power electronics. The continuous reduction in processor voltages has played its part in this. A few years ago, switching frequencies up to 300 kHz were widespread, whereas modern switching controllers usually clock with frequencies of 800 kHz and more. The switching losses, on the one hand, but also the power inductor losses, on the other, are important aspects in the design of switching power supply units.

New iron alloy group material compositions have further reduced core material losses for high current power inductors. WE-MAPI is a component series whose adept material selection and manufacturing technology combines the optimal use of inductance and current carrying capacity with low internal losses. A new tool – REDEXPERT – based on a metrological procedure, helps the developer determine the hitherto most accurate data for DC and AC current losses in power inductors in the application environment. Core loss calculations based on Steinmetz equations very soon reach their limits here.

 

2. WE-MAPI structure and properties

WE-MAPI is the latest and most innovative series of coils from Würth Elektronik. Conventional coils mostly use enameled copper wire wound around the core and soldered or welded to the terminal with a clip. The outer shielding ring is then mounted and bonded with the inner core and the winding.

 

imageimage

Figure 1: View of the WE-MAPI and the direct contacting of the wire with the connection pads

 

WE-MAPI breaks new ground and the winding is contacted directly with the component's connection pad without soldering and welding. Saving the clip allowed the effective diameter to be increased, which means fewer windings are needed for the same inductance values. This is directly expressed in a considerably reduced DC resistance (RDC) of the winding.

 

In the application, the start of the winding of the coil is usually connected with the switching node of the switching controller – a marking on the component indicates this. Consequently, the spatial expansion of the "hot" switching node is minimized and coupling effects through the outer part of the winding at a "stable" potential are also shielded.

 

imageimage

Figure 2: Self-shielding winding and core design for improved EMI behavior of the WE-MAPI series

 

The core consists of an innovative metal alloy pressed around the winding. This confers the WE-MAPI series high inductance values with a small package size. At the same time, the special construction of the core has a self-shielding effect. The core material itself is temperature stable with only a slight drift and "soft" saturation behavior. A protective layer is also applied around the core rendering the surface resistant against environmental influences. The WE-MAPI series components are available in many different package sizes from 1.6² x 1.0 mm, up to 4.0² x 2.0 mm.

 

image

Figure 3: Overview of the available package sizes for WE-MAPI

 

3. Losses in power inductors

The losses of a power inductor arise from core material losses and winding losses. The winding losses themselves can be divided into DC current losses, essentially influenced by the DC resistance of the winding

image

and the AC losses (RAC) of the winding that arise from skin and proximity effects. Several methods are available to determine AC losses of the winding, e.g. the Dowell, Ferreira or Nan/Sullivan methods.

The importance of AC losses in modern switching controllers can be ascertained with a simple set-up and measurement of the relevant losses. As an example, we take a buck converter with an input voltage of 24 V. At the output there is 12 V with 2 A. The clock frequency is 500 kHz. In Figure 4, a WE-MAPI 4020 series power inductor with 2.2 μH is compared with power inductors of the same package size. It is clearly apparent that with all the coils measured, the AC losses outweigh the DC losses.

 

image

Figure 4: AC and DC losses of a 2.2 μH coil, buck converter with 24 V to 12 V, 2 A, 500 kHz

 

The coil is one of the most important components in switching controllers. Accurate determination of the losses and heating is therefore a critical step in the selection of the right component. In order to be in a position to predict heating, the AC losses firstly have to be accurately determined.

 

3.1. The Steinmetz models

Viewed historically, core losses were determined with the Steinmetz Model (1), and later with the Modified Steinmetz Model (2) or the Generalized Steinmetz Model (3):

 

image

 

Whereby     are the core losses per unit volume,    the switching frequency, and        the magnetic sinusoidal modulation.        is the equivalent frequency that results in non-sinusoidal modulation for a deviating duty cycle.   ,    &    are the constants of the core material determined by extensive measurements with a ring core. The essential drawback of the Steinmetz equation is that it mainly applies for sinusoidal excitations and determination of the coefficients is usually only measured with small signals.

However, in most applications in power electronics, the coil current is not sinusoidal. And the currents are large signals of several mA up to several hundred Amperes. There are also other models that attempt to resolve the problem of non-sinusoidal waveforms by separating hysteresis and eddy current losses. Here the empirical Steinmetz equation has proven to be a useful variant, but it only offers high accuracy for sinusoidal currents. However, the various Steinmetz models only work

 

WE-MAPI Other C Other V

Power Loss [mW]

Power Loss Comparison

 

optimally with a duty cycle of 50% and within a restricted frequency range. In addition, on account of the high complexity in finding the magnetic path length, the determination of core losses with the help of existing models for iron powder and metal alloys is not only demanding, but the accuracy is also subject to serious fluctuations. And for inductors that consist of several different core materials, estimation of the losses is only possible with great effort, if at all.

 

3.2. The Würth Elektronik Model

Würth Elektronik eiSos has developed a highly modern model capable of accurately determining the complete AC losses in inductors. This model is based on empirical data obtained with a real-time application set-up. Here the total losses of the inductor are divided into AC and DC losses. Empirical data are measured with a DC/DC converter, as presented in Figure 5. A pulsed voltage is applied to the inductor, whereby the input power        and the output power          are measured.           =        −          is determined on this basis and the AC losses of the coil       are separated. This procedure is used to measure the different parameter settings – such as fluctuations in the magnetic modulation, switching frequency, ripple current, etc. – and this empirical data is recorded. With the help of this empirical data, the model is created for calculation of the AC losses:

 

image

Figure 5: Set-up of the DC/DC converter for determining loss and the associated oscilloscope recordings

 

 

Advantages of the Würth Elektronik AC loss model:

 

  • The empirical data is based on a DC/DC converter
  • Accurate determination of losses for every given duty cycle
  • Accurate across a wide frequency range (10 kHz to 10 MHz)
  • Also considers the smallest changes in the core material and the winding structure
  • Applicable for components with more than one material used
  • Accurate determination of losses in components with iron powder and metal alloys
  • Applicable for every possible core design and winding structure
  • Also includes AC winding losses

 

3.3. Performance of the Würth Elektronik Model

The model from Würth Elektronik has been extensively validated and compared with existing models and measured data. AC losses for different materials, such as WE-Superflux, iron powder, NiZn, MnZn, etc. have been measured over wide duty cycle and frequency ranges and compared with theoretical models (Figure 6). The following graphs show the core losses determined with the Steinmetz power equation (Pst), Modified Steinmetz equation (Pmse) and the Generalized Steinmetz equation (Pgse). REDEXPERT shows the AC loss following calculation with the AC loss model from Würth Elektronik. The measured AC loss is “Real”.

 

image

Figure 6: Inductor made of MnZn and iron powder at 33% DC

 

4. Determining losses with REDEXPERT

 

REDEXPERT is the new online design tool from Würth Elektronik eiSos used to select a suitable power inductor for the respective application. REDEXPERT is an easy-to-operate and effective tool, enabling components to be compared and selected within the shortest time. Firstly the user enters the input and output parameters for the required topology. REDEXPERT then calculates the necessary inductance value and displays the suitable inductances. Figure 7 shows the REDEXPERT

screenshot.

 

image

Figure 7: Simulation of a buck converter in REDEXPERT with WE-MAPI components

 

The calculation of AC losses in a magnetic component is just as critical as it is complex, but not with REDEXPERT, as the new AC loss model from Würth Elektronik is integrated. Based upon accurate calculation of the complete AC losses, the application is also suitable for temperature estimation. Currently REDEXPERT supports three topologies in which the component can be selected for the application: buck, boost and SEPIC converters. The losses are displayed graphically over the complete input voltage range in order to also take extreme scenarios into consideration. This way the most energy-efficient power inductor for the respective application can be selected in next-to-no time.

In order to determine the right inductor for a buck converter, enter the existing input voltage range and the output voltage and current in the input screen (Figure 8), as well as the switching frequency, the diode flow voltage and the targeted ripple current of the inductor. By clicking on "Display details", the suitable power inductor is obtained, including its anticipated ripple currents and the losses in the application.

 

image

Figure 8: Defining the buck converter and the losses of the selected inductor

 

There is also a manual loss calculator, which calculates the losses for power inductors independent of the topology. Only the frequency, the duty cycle and the ripple current, or the voltage drop, have to be entered, and REDEXPERT takes care of the rest. One practical aspect is that the entries are immediately displayed in graphic form below the entry screen.

REDEXPERT is a web-based tool, i.e. the user neither has to download REDEXPERT nor worry about updating. Registered customers benefit from further advantages, e.g. determination of inductance value or temperature increase of the inductor for every possible current value.

 

5. Summary

The WE-MAPI power inductors offer maximum power in the smallest of spaces. With the innovative core material and the sophisticated design, new standards have been set. For energy-efficient switching controllers, the WE-MAPI is best selected with REDEXPERT, the new online design tool from Würth Elektronik. This integrates the world's most accurate AC loss model, which renders the parameters of frequency, ripple current and duty cycle with high accuracy over a wide range of values.

 

IMPORTANT NOTE

The application information, based on our current state of knowledge and experience, serves as general information and cannot be taken as an assurance from Würth Elektronik eiSos GmbH & Co. KG as to the suitability of the product for

customer applications. The application information may be changed without prior notice. This document and parts thereof may not be reproduced or copied without written consent. Würth Elektronik eiSos GmbH & Co. KG and its partners and

subsidiaries (together hereinafter referred to as "WE") are not liable for any kind of application-related support. Customers are entitled to use WE's support and product recommendations for their own applications and designs. Customers bear

sole responsibility for the applicability and use of WE products in a particular design in every case. Based on this fact, it is the customers' responsibility to initiate any investigations necessary and to decide whether or not the device with the

specific product features described in the product specification is approved and suitable for the respective customer application.

The technical data are specified in the current data sheet for the product. For this reason, customers have to use the data sheets and attention is expressly drawn to the fact that they have to ensure the data sheets are up to date. The current

data sheets can be downloaded from www.we-online.com. Customers must strictly observe product-specific remarks and warnings. WE reserves the right to undertake corrections, modifications, additions, improvements and other amendments

to its products.

Licenses and other rights of any kind, especially to patents, utility models, marks, copyrights or other commercial protection rights, are hereby neither granted nor shall any duty be implied to grant such rights. By publishing information on thirdparty

products or services, WE neither grants a license to use such products or services nor offers a guarantee or endorsement for them.

The use of WE products in safety-critical applications or those in which severe personal injury or death can arise due to product failure is not permissible. Furthermore, WE products are neither designed for nor intended for use in fields such

as military technology, aerospace, nuclear control, navy, transportation (control of motor vehicles, trains or ships), traffic control installations, civil protection, medical technology, public information networks etc. Customers must inform WE of

the intention of such use prior to the start of the planning phase (design-in phase). For customer applications with stringent safety requirements in which the malfunction or failure of an electronic component could endanger life and limb, customers

must ensure that they have the required expert knowledge of the safety and legal implications of their applications.

Customers acknowledge and agree that, notwithstanding all application-related information and support provided by WE, they bear full responsibility for all legal, statutory and safety related requirements in conjunction with their products and the

use of WE products in such safety-critical applications. Customers shall indemnify and hold WE harmless with respect to all claims arising from such safety-critical customer applications.

 

USEFUL LINKS

Application Notes: http://www.we-online.de/app-notes

REDEXPERT Design Tool: http://www.we-online.de/redexpert

Toolbox: http://www.we-online.de/toolbox

Product catalog: http://katalog.we-online.de/

 

CONTACT INFORMATION

Würth Elektronik eiSos GmbH & Co. KG

Max-Eyth-Str. 1, 74638 Waldenburg, Germany

Phone: +49 (0) 7942 / 945 – 0

e-mail: appnotes@we-online.de

Web: http://www.we-online.de