PCB Design, Prototyping and Production
  • Products & Partners
  • More
PCB Design, Prototyping and Production
PCB Forum PCB Holders
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PCB Design, Prototyping and Production to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 40 replies
  • Subscribers 157 subscribers
  • Views 8507 views
  • Users 0 members are here
  • dougw
  • PCB holders
  • PCB vises
Related

PCB Holders

dougw
dougw over 2 years ago

I've been doing some reorganizing and noticed I have a collection of PCB holders. I decided to do a quick post on them to spark some discussion around what constitutes a good PCB holder.

This video is a brief overview of the holders I have and how I use them.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Here are some other PCB holders I built..

What do you use to hold PCBs and what do you think is a good holder system?

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 2 years ago in reply to colporteur +3
    It is a genius material, so many uses. It comes in a sheet form, between waxed paper. The first time it is used, it just needs to be stretched a bit, and it becomes sticky (without leaving any residue…
  • michaelkellett
    michaelkellett over 2 years ago +3
    My favourites are steel toolmakers vices. I bought three at a very good price from MSV a couple of years ago - never seen good ones so cheap again They do for all sorts of things apart from holding…
  • Andrew J
    Andrew J over 2 years ago in reply to colporteur +2
    Seriously, blu-tack is the way to go here as they don't move at all once stuck down - the only thing to be aware of is avoiding getting blu-tack stuck in any empty holes! I picked that tip up from Shabaz…
Parents
  • colporteur
    colporteur over 2 years ago

    Your post was very timely for me.

    I use the through hole device you presented. I have a few of the others you mentioned also.

    You answered the question I was going to ask and that was "How do you hold components to solder once you flip them.?" I will find a piece of foam and give it a try.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 2 years ago in reply to colporteur

    Seriously, blu-tack is the way to go here as they don't move at all once stuck down - the only thing to be aware of is avoiding getting blu-tack stuck in any empty holes!  I picked that tip up from Shabaz.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • anniel747
    anniel747 over 2 years ago in reply to Andrew J

    Contacts contamination risk.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 2 years ago in reply to anniel747

    Never, ever, ever been a problem.  Do as normal: clean the PCB with IPA after soldering.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • anniel747
    anniel747 over 2 years ago in reply to Andrew J

    I have seen it a few time from pros to DIY jobs. Some connectors needed replacement. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • anniel747
    anniel747 over 2 years ago in reply to Andrew J

    I have seen it a few time from pros to DIY jobs. Some connectors needed replacement. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • shabaz
    shabaz over 2 years ago in reply to anniel747

    Blu-Tack is about as harmless as anything, perhaps there is a chance of finger oils on the board/components or handling the solder causing more contamination. 

    Blu-Tack is also useful to raise some components slightly off the board (this can be done without the blu-tack touching the wires if desired, but it's hard to see that being an issue for anything apart from space-lasers or other critical stuff. There's no need to wedge Blu-Tack into connector pins, just a couple of blobs can support each end.

    Besides, the Weller clamp has plastic pieces and foam, there's a chance of contamination from that if the soldering iron accidentally touches and melts it.

    I use a similar tool vice as Doug, but a lightweight aluminium version. Main downside is that it can't handle boards much bigger than 60mm, but that covers 80% of the stuff I work on.

    image

    It has a V-notch that's handy for circular connectors, but recently I've been thinking of making some 3D-printed clamp for one or two circular connectors that can get particularly awkward. No time to work on it : (

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 2 years ago in reply to shabaz

    I have a couple of cheap plastic vises with this form factor, but find they are too light (they slide around too easily) and they can't hold even a moderate sized card. That one looks pretty stable though. They were omitted from the video because I use them so little for holding PCBs, I probably looked right at them without remembering they could be used to hold PCBs...Relaxed

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to dougw

    Yes it's great. It's lighter than iron or steel but not super-light. I think it's a clone of this, which is 500 grams:

    image

    I use it on this ESD mat (really excellent mat too, and surprisingly low-cost for the size!), and it doesn't slide around:

    image

    The jaws have a large flat top surface, and I end up using that as a "staging area" when soldering same-value SMD resistors etc! 

    There's also often blobs of blu-tack tacked on the top of the jaws, so that I can quickly hold a board down if it's too awkward for the jaws (e.g. if there are parts right to the edge, such as side-mounting right-angle SMA connectors etc!). 

    This one on Amazon looks so promising, and can handle boards up to 130mm wide! It is alu, 1kg:

    However, it's pricey : ( plus, the depth is 13mm, and there could be components taller than that off the surface of the PCB.

    Also, the recess for the PCB is just a bit too much (4mm).  It's a shame, it is so close! But good from far, far from good : (