PCB Design, Prototyping and Production
  • Products & Partners
  • More
PCB Design, Prototyping and Production
PCB Forum PCB Holders
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PCB Design, Prototyping and Production to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 40 replies
  • Subscribers 157 subscribers
  • Views 8493 views
  • Users 0 members are here
  • dougw
  • PCB holders
  • PCB vises
Related

PCB Holders

dougw
dougw over 2 years ago

I've been doing some reorganizing and noticed I have a collection of PCB holders. I decided to do a quick post on them to spark some discussion around what constitutes a good PCB holder.

This video is a brief overview of the holders I have and how I use them.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Here are some other PCB holders I built..

What do you use to hold PCBs and what do you think is a good holder system?

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 2 years ago in reply to colporteur +3
    It is a genius material, so many uses. It comes in a sheet form, between waxed paper. The first time it is used, it just needs to be stretched a bit, and it becomes sticky (without leaving any residue…
  • michaelkellett
    michaelkellett over 2 years ago +3
    My favourites are steel toolmakers vices. I bought three at a very good price from MSV a couple of years ago - never seen good ones so cheap again They do for all sorts of things apart from holding…
  • Andrew J
    Andrew J over 2 years ago in reply to colporteur +2
    Seriously, blu-tack is the way to go here as they don't move at all once stuck down - the only thing to be aware of is avoiding getting blu-tack stuck in any empty holes! I picked that tip up from Shabaz…
Parents
  • colporteur
    colporteur over 2 years ago

    Your post was very timely for me.

    I use the through hole device you presented. I have a few of the others you mentioned also.

    You answered the question I was going to ask and that was "How do you hold components to solder once you flip them.?" I will find a piece of foam and give it a try.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 2 years ago in reply to colporteur

    Seriously, blu-tack is the way to go here as they don't move at all once stuck down - the only thing to be aware of is avoiding getting blu-tack stuck in any empty holes!  I picked that tip up from Shabaz.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 2 years ago in reply to Andrew J

    blu-tack is new to me. I have used Frog painters tape in the past. It is a real pain in the *** to use but I haven't discovered an alternative. Shabaz recommendations are top shelf. I'm curious to know more.

    Can you use it like a foam bed to hold multiple components in place while you flip the PCB to the soldering side?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to colporteur

    It is a genius material, so many uses. It comes in a sheet form, between waxed paper. The first time it is used, it just needs to be stretched a bit, and it becomes sticky (without leaving any residue). The properties of blu-tack remain approx. forever, i.e. the material is always reusable and never dries up.

    image

    It can hold multiple parts at once, the photo below shows a couple of parts being held down. It's strong enough that the parts don't move when soldering, and afterwards, it comes off in one piece, with no residue left. If it is in an awkward place, then dabbing it with a larger piece of it will lift it all off.

    I suppose it may leave a micro-film of oil, but probably no more than finger oil. When Blu-Tack is removed, the surface is dry and zero visible residue. Even if it gets hot, nothing seems to happen to it. It's as benign/inert as one could hope for I guess.

    image

    An example of holding a larger module; here the module was deliberately raised off the board slightly, just to demonstrate that Blu-Tack holds the item in a controlled fashion, and doesn't sag/slip in normal use:

    image

    It's super-useful for pin headers, LEDs, large capacitors, etc., it holds them all in vertical alignment!:

    image

    I also use it for holding down ICs too, connectors, pretty much anything. 

    The photos above show the board in an aluminium tool vice, and the top flat surfaces are ideal for Blu-Tack too,  e.g. if there is a large PCB to be held down, or to temporarily hold wires in position, etc.

    The genuine stuff is "Bostik Blu-Tack", and costs just over £1 here for a pack. Interesting seeing the scores in the Amazon results below... Surprising that any reviewer could possibly give it less than 5 full stars! 

    image

    Wikipedia entry of uses for it:

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 2 years ago in reply to shabaz

    There are variations on a theme as well.  My (now) wife brought a pack of white tack with her when she moved in 13 years ago.  No idea how old it actually is but it has never gone off and inevitably it’s always the same bits that get reused and reused and reused….  One could think the stuff is an environmental disaster.  Or maybe along with cockroaches the only thing that would survive a nuclear holocaust!  

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to Andrew J

    Hehe definitely indestructible material : ) 

    I just saw this vice, wide enough for 100mm boards:

    image

    Still not fit-for-purpose since there's little depth, but the alu could easily be tapped and alu blocks screwed onto it to raise the clamping position.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 2 years ago in reply to shabaz

    I sort of feel that once you have to start finagling a tool to make it work better, you're better off buying a better tool in the first place!  The Duratool holder that Doug mentioned is fine for most hobbyist size boards - I've used it up to 15cm and it still has plenty of leeway.  Clamp the board in, place the parts, blu-tack them down, spin the board and solder away.  The height the board is held above the bench works well for me and I can rest a forearm on the bench whilst soldering.  It just requires the board to be positioned in such a way as to avoid spinning it when soldering; not that it freewheels but sometimes you want the board at an angle (rather than parallel to the bench) and you can inadvertently push it with the iron. It's dirt cheap to start with as well.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to Andrew J

    I'm the same, I'd generally rather buy a purpose-built tool, although I get the feeling these vices could be particularly nice to use for when a board is desired to be worked on flat. I have a bunch of optical alu blocks so I might modify a couple of them with grooves (for PCB and a notch if possible for round connectors; don't think I have any milling bit for that : (

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 2 years ago in reply to shabaz

    Are they heavy enough to not shift around?  I know you don't apply a lot of pressure on the tip of the iron but if it's too light it may still move.

    You could 3d print small pieces with grooves and stick them the the clamp blocks with blu-tack!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to Andrew J

    I've ordered one to give it a shot. I think it may be about a kilogram in weight (the two rails and thread are steel even though the rest is alu). I use an ESD mat, which will add a bit of grip. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 2 years ago in reply to shabaz

    That vise looks like a pretty useful size and a decent price.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 2 years ago in reply to Andrew J

    Buying the right tool is definitely preferred, but if you bought a tool that isn't quite optimal and it can be modified to work better, it can be worthwhile. I just modified a battery operated electric screwdriver to have a power connector so I can run it from a power supply. Running it from primary batteries made it useless to me, so I am much happier with the power supply solution. It can still run from batteries, but I don't ever expect to put batteries in it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 2 years ago in reply to Andrew J

    Buying the right tool is definitely preferred, but if you bought a tool that isn't quite optimal and it can be modified to work better, it can be worthwhile. I just modified a battery operated electric screwdriver to have a power connector so I can run it from a power supply. Running it from primary batteries made it useless to me, so I am much happier with the power supply solution. It can still run from batteries, but I don't ever expect to put batteries in it.