Raspberry Pi
  • Products
  • More
Raspberry Pi
Blog 3D Printed Raspberry Pi 4 Enclosure with Fan
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fmilburn
  • Date Created: 14 Aug 2019 4:14 AM Date Created
  • Views 4526 views
  • Likes 12 likes
  • Comments 19 comments
Related
Recommended
  • fan
  • raspberry pi 4
  • enclosure
  • raspberry pi 3
  • case
  • 3d print

3D Printed Raspberry Pi 4 Enclosure with Fan

fmilburn
fmilburn
14 Aug 2019

The new Raspberry Pi 4 will not fit in any of the enclosures I have at hand and while doing preparation for a RoadTest I found that my Pi was overheating and throttling back.  A quick web search did not find what was desired and besides designing one seemed like a good learning opportunity.  The resulting design, done in Fusion 360, has the following features:

  • Pi 3 also fits the enclosure
  • Snap fit with no screws
  • Base enclosure has a plain, solid top
  • Camera slot can  be added to the print
  • Display slot can be added to the print
  • 30 mm fan can be added to the print

 

The additional features are added by altering their individual parameters which are kept in an easily accessible table.  Changes to clearances and key dimensions can also be changed if needed by modifying their parameters.  This might prove useful in printers with different resolution or if for example the case height needs to be extended to fit a hat.

 

The basic design is similar to one that was posted right after the Pi 4 came out.  This enclosure was designed separately from the ground up however and is not compatible.  To accommodate the difference in USB, multiple HDMI, etc. between the Pi 3 and the Pi 4  the case slots in these areas is open without dividers.  A camera slot, display slot, 30 mm fan opening, or any combination thereof can be added in seconds.

{gallery} Raspberry Pi Enclosure Print Options

image

Plain Enclosure

image

Enclosure with Openings for Camera and Display

image

Enclosure with Openings for Fan, Camera, and Display

 

Printing was done on an ANYCUBIC I3 MEGA with the following settings:

  • Layer Height = 0.2 mm
  • Wall Thickness = 1.2 mm (Wall Line Count = 3)
  • Filament = 1.75 mm PLA
  • Print Temperature = 200 C
  • Bed Temperature = 60 C

 

Total print time for the top and bottom is around 5 hours depending on the wall thickness chosen and the slots.  The photo below shows the Pi 4 mounted in an enclosure with a fan on top.  At this point a heat sink has not been added - just the fan.

image

As noted above, there was throttling prior adding the fan.  Raspberry Pi states that a warning is normally issued when 80 C is reached and throttling occurs at 85 C.  With the fan, temperatures did not exceed 72 C during the stress testing with the CPU at 100% for approximately 10 minutes.

 

Fusion 360 has amazing capabilities although I am still finding my way around it.  I am using the free one year trial for hobbyists.  I am very happy with the outcome and there are only a couple of small things I may change with the design:

  • Some of the openings are a bit large and could be reduced in size for aesthetics
  • The case width could be enlarged 1-2 mm as there is a tight fit on one side which makes removal of the top a bit hard

 

The fan also whines and I will probably cut some foam to fit between it and the case to dampen it.

 

Thanks for reading, comments and suggestions are always welcome.

  • Sign in to reply

Top Comments

  • dougw
    dougw over 6 years ago +6
    Nice design. The "ports on multiple sides" design of the Pi is a great application for 3D printed solutions, but I have shied away from doing them because of the temperature. I had one box (not for a Pi…
  • fmilburn
    fmilburn over 6 years ago in reply to balearicdynamics +6
    Hi Enrico, I don't plan to post it widely because I am using the free license and I do not understand what that allows and I don't want to lose my license. However, I would be happy to send you or any…
  • e14phil
    e14phil over 6 years ago +5
    I (genuinely) love the feel of using $500+ kit and years of know how to fix a problem as small as a $12 case. Fills me with genuine happiness. Phil
Parents
  • dougw
    dougw over 6 years ago

    Nice design. The "ports on multiple sides" design of the Pi is a great application for 3D printed solutions, but I have shied away from doing them because of the temperature. I had one box (not for a Pi) that sagged over the course of a year or so due to elevated temperatures. It wasn't approaching PLA melting temperature - it was something like the temperature in a car cab. The black items in a car can get too hot to touch comfortably if they are in the sun - about 60 C, but these boxes weren't in direct sunlight. I know the internal temperature of a Pi processor is in this range, I'm just not sure how hot the plastic case could get. I would be interested to know how your case fares over time (and temperature).

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dougw
    dougw over 6 years ago

    Nice design. The "ports on multiple sides" design of the Pi is a great application for 3D printed solutions, but I have shied away from doing them because of the temperature. I had one box (not for a Pi) that sagged over the course of a year or so due to elevated temperatures. It wasn't approaching PLA melting temperature - it was something like the temperature in a car cab. The black items in a car can get too hot to touch comfortably if they are in the sun - about 60 C, but these boxes weren't in direct sunlight. I know the internal temperature of a Pi processor is in this range, I'm just not sure how hot the plastic case could get. I would be interested to know how your case fares over time (and temperature).

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • fmilburn
    fmilburn over 6 years ago in reply to dougw

    Thanks Doug for that warning.  I will keep an eye out for sagging (and try to remember to report back).  During my upcoming RoadTest I could also place a thermocouple in the case just to see what the temperature of the air in the case is doing as well as maybe one on the case ceiling.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 6 years ago in reply to dougw

    Hi Doug,

     

    I have had the version with the fan working for about 6 weeks now, using it daily, and the case is fine.  The fan is on constantly and the air coming out of the case is only slightly above ambient.  The case itself does not feel particularly warm so it is not surprising that there is no problem. 

     

    I suppose I should try the version with no fan and see what happens but then it will be subject to throttling which is undesirable for my experiments with Tensorflow.

    • Cancel
    • Vote Up +2 Vote Down