Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Blog An Industrial Enclosure for Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 26 Apr 2019 1:15 PM Date Created
  • Views 13275 views
  • Likes 20 likes
  • Comments 36 comments
Related
Recommended
  • rpi 4
  • raspberry pi 4b
  • rpi bc din rail housing for raspberry pi computers
  • pi 3 model b+
  • rpi-bc 107
  • raspberry pi 4 b
  • pi 3 b+
  • rpi-bc

An Industrial Enclosure for Raspberry Pi

shabaz
shabaz
26 Apr 2019

Note: The video shows a Pi 3 being used with this enclosure, but has also been tested with Pi 4, and it works fine. See photo further below for a Pi 4 inside the enclosure.

 

  • Introduction
  • What is it?
  • Is there a need for the Pi in industry?
  • Installing the Pi
  • Designing your own Circuits
  • Un-clipping the case
  • Using a Ribbon Cable
  • Using the Front Panel
  • Putting it Together: Raspberry Pi 4 and Custom Board
  • Summary

 

Introduction

Fed up of leaving my Pi’s exposed, I was on the lookout for a Pi enclosure that would have space for additional circuitry. I frequently need a decent enclosure that doesn’t look out of place in a factory, not only suitable for deployments in industrial control panels, but also for home use and general experimentation too.

 

I recently purchased a new Pi 3 Model B+, and it was a good opportunity to look for a suitable enclosure. The Phoenix Contact RPI-BCPhoenix Contact RPI-BC seemed attractive, because it was large enough to add custom circuitry inside it too! Also, it was surprisingly low-cost which always helps. There were some reviews of the RPI-BC a couple of years ago but I was not sure if the newer Pi 3B+ would fit it or not, and happily it is a perfect fit. The RPI-BC enclosure could be of great interest to engineers, since there is high demand for industrial edge computing. This short blog post shows some ideas on how to work with the case and Pi 3B+.

 

The case is intended for DIN rail fitting in industrial control panels. However, it could be used as-is too. It looks attractive enough to use elsewhere too, and the front panel could have a sticker with graphics attached, or it could be drilled out for custom controls.

 

For a three-minute video tour, see here:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

What is it?

The RPI-BCRPI-BC is a plastic enclosure by Phoenix Contact, known for industrial automation components and solutions. The enclosure will allow you to design Pi software and add-ons that can clip together onto a DIN rail.

image

 

The case is not ruggedized (nor is it intended for dusty environments since connections are exposed) so those are some constraints that define where the enclosure could be deployed, i.e. it’s intended use is inside control panels or a cabinet/closet.

 

Phoenix Contact has built an ecosystem of individual components that make up the enclosure, front panels, and prototyping circuit boards, but the main parts are all available with a single order code, and that’s what is discussed here.

 

The shell has three main parts – two main halves, and a removable cover that could be drilled to accommodate LEDs or displays for instance, or even a camera. Inside, there is room for a couple of circuit boards, and an 18-way expansion connector if desired, to allow sideways linking with other enclosure modules on the same DIN rail. It’s a neat, attractive solution.

(Image source: adapted from several photos from the Phoenix Contact website)image

 

Is there a need for the Pi in industry?

I believe the answer is yes! The amount of compute power allows for many interesting things to be done in edge computing scenarios in an office or factory. I’ll touch on this more in a later article. However, it is plain to see there is growing interest in using low-cost hardware to do more intensive processing locally. There are many variants and custom builds of the Pi from sources such as Avnet and Hilscher. I’ve had first-hand experience in seeing a healthcare-related custom build of the BeagleBone Black (an ARM based computer similar to the Pi) as another example. The Linux operating system is highly attractive for creating a lot of functionality quickly into products, and manufacturers have taken steps at hardening the platforms and adding security to suit industrial use-cases.

 

Installing the Pi

The RPI-BC uses a nice way of positioning and securing the Pi. There are a couple of black plastic rails that clip on to the Pi to act a carrier. There are lips that fit the shell of the case, and then the Pi is secured when the other half of the shell is attached. 

image

 

Once installed, the power supply micro USB connector and HDMI and audio connectors are accessible inside the enclosure which is great – they are unlikely to all need exposing outside, but cables can be routed in the empty space if needed.

image

 

The carrier rails ensure that the Pi is very accurately positioned inside the case. That’s needed, so that the micro SD slot and LED holes are also positioned accurately. Incidentally since the Pi’s micro SD card is not ‘push to eject’ but is ‘pull to eject’, if the end user will need to remove the card with the enclosure closed, some tape on it helps.

image

 

Designing your own Circuits

Some Phoenix Contact prototyping boards for the RPI-BC are available; one prototyping board plugs onto the Piprototyping board plugs onto the Pi, and another prototyping board fits the space to the sideprototyping board fits the space to the side. To make custom PCBs easier, so I took the dimensions, and made up an EAGLE CAD part (attached to the bottom of this blog post).

image

 

The parts required to assemble such a custom PCB are a 40-way connector strip40-way connector strip and optionally up to four 4-way connectors4-way connectors.

 

Un-clipping the case

The two main halves of the enclosure clip together. They are easy to disassemble using thin plastic such as a guitar pick.

image

 

Using a Ribbon Cable

If you’re unsure what circuitry to attach, that decision can be left until later : ) by using a ribbon cable plugged onto the Pi instead of the previously-mentioned PCB. I used a 40-way insulation displacement connector40-way insulation displacement connector (IDC) and a 26 way connector26 way connector and 40 way ribbon cable40 way ribbon cable and the cable assembly can be left inside the case, or it can be brought out through the holes on either side of the enclosure. There’s enough space to make a small PCB in future that the 26-way connector can plug onto. To make the cable assembly, a 40-way cable was used and it was slit and cut. A vice can be used to close the IDC connectors.

image

 

Using the Front Panel

The front panel can have holes drilled for buttons and LEDs and so on, and it permanently clips onto the front of the enclosure, however it could be turned into a hinged flap if desired, by cutting out plastic in three areas before attaching it on (there is an optional front panel order code that doesn't need this manual modification).

image

 

Putting it Together: Raspberry Pi 4 and Custom Board

The photo here shows an example board designed with EAGLE CAD, installed along with the Pi 4, into the enclosure. The flap covers the display/controls and hinges open to reveal the user instruction sheet. The flap could be replaced with a 3D printed version with holes for the display and buttons if desired.

image

 

Summary

The RPI-BC enclosureRPI-BC enclosure is a perfect fit for the Pi 3B+ (and it also works with other Pi variants, such as the A+ models with an optional A+ adaptoroptional A+ adaptor). I really liked that it was easy to attach additional circuitry if required, and I’m looking forward to using it in multiple projects, using custom PCBs.

 

It’s low-cost, and very functional. Surprisingly, it is also excellent for brainstorming - having such a case and the ease to build things with it, opens up many possibilities for exciting new solutions with the Pi. if you develop any, or have ideas, it would be great to hear about them.

Thanks for reading!

Attachments:
RPI-BC EAGLE CAD library v1.1.zip
  • Sign in to reply

Top Comments

  • beacon_dave
    beacon_dave over 7 years ago in reply to shabaz +6
    Hi Shabaz, Yes it jumped out of the page when I saw it last night.
  • shabaz
    shabaz over 7 years ago in reply to balearicdynamics +6
    Finally I found some PDF on the Phoenix Contact website with a small image too, but I kept zooming in..:
  • beacon_dave
    beacon_dave over 7 years ago +4
    There's a variation on this case which accepts the official 7" touchscreen which may also be of interest: https://www.phoenixcontact.com/online/portal/us/?uri=pxc-oc-itemdetail:pid=1104781 Spotted it in…
  • shabaz
    shabaz over 7 years ago in reply to geralds

    Hi Gerald,

     

    Thanks! I learned from your Roadtest review about the case and the prototype boards and the connectors, so it got me curious if it was still supported with the new 3B+.

    And I noticed you'd marked out the areas of the prototype board, that would be supported for components, so I decided to do the same thing in the EAGLE file : )

    Thanks for your excellent review!!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • geralds
    geralds over 7 years ago in reply to Jan Cumps

    Hi Jan Jan Cumps ,

     

    Well, well, speaks clever in this white paper.

    But, "what is not yet can still be..."

    I know Harting, so do some other smart companies, all cook with the same water.

    What is a "real-time system"? - One which consists only of knit in hardware? - Also, the SPS control has a processor too and processes the task with software, and in my opinion this is not really "" real time "".

    Modern ECUs always have a 'motherboard' with perhaps Linux, or even Windows (XP, 7, or other).

    The latency can skyrocket with "wrong" programming, and then? .... Well, the term 'real time' in more complex systems I always perceive as "relative"; as Einstein liked to express it, "everything is relative" ...

     

    The Pi comes good, but it needs a bit more time.

    I think such platform will growing up in the near future. "MICA" from Harting, image well advertising, "we are the best of the best".

     

    Is only my opinion

    Best Regards

    Gerald

    ---

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • geralds
    geralds over 7 years ago

    Hi Shabaz shabaz ,

    Thank you for the fine description and highlighting of the details.

    Yes, I can remember our roadtest and now you have described even more details perfectly.

    Nice!

    Thanks also for the Eagle lib file.

     

    Best Regards

    Gerald

    ---

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • stevesmythe
    stevesmythe over 7 years ago in reply to Jan Cumps

    I came across that one too! It's here in English. You can see if Google managed it well.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to Jan Cumps

    Jan Cumps agree but just under this point of view – I mean spare parts for example – it seems that this detail is becoming a bit outdated. Until the start of 1990, there was a choice of hardware for some kind of projects just for the availability of spare parts, repair components and so on. Nowadays, not only the situation to me seems reversed but most of my projects are built with components originally distributed as spare parts. From stepper motors to sensors and so on. Or I am wrong?

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>