• Products and Partners
    Products and Partners
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
Raspberry Pi
  • Products and Partners
  • More
Raspberry Pi
Blog Build a Raspberry Pi media center
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 8 Nov 2012 10:12 PM Date Created
  • Views 3735 views
  • Likes 3 likes
  • Comments 13 comments
Related
Recommended
  • raspberry
  • raspi
  • pi
  • video
  • rpibeginner
  • raspberry_pi
  • center
  • media
  • xbmc

Build a Raspberry Pi media center

e14 Contributor
e14 Contributor
8 Nov 2012
imageWant to build this project?
View Parts

 

Use your Raspberry Pi as an awesome media portal for listening to music, watching videos, and viewing pictures.

 

As an old-school XBOX modder, the first thing I wanted to do with my PI was turn it into a media portal. XBMC (Xbox Media Center) is an open source front end for Linux that used to only be available for the Xbox. These days, it is now available for PCs, Linux Distros, Boxee boxes, and most importantly Raspberry Pi.

 

I used a special Linux distribution built for the Raspberry Pi to build a media center, Raspmc (http://www.raspbmc.com/).

 

OpenElec is another option (http://wiki.openelec.tv/index.php?title=Building_and_Installing_OpenELEC_for_Raspberry_Pi) .

 

Setup: Flash Raspmc or OpenElec to an SD Card

Follow instructions on the respective sites to flash a version of XBMC to an SD card. I didn’t have any problems. However, I’d recommended checking searching through forums if anything comes up.  If you are having a problem, it’s possible that someone else has had the same one. Once you’ve flashed XBMC to your SD card, plug it in to the PI and power it up. You now have a Raspberry Pi Media Center.

 

Notes:

Make sure you have a wired internet connection for the first boot. Raspmc will need it to complete the installation and download updates.

 

There are some great Android and iPhone apps that you can use to control Raspmc. I use the official XBMC remote App on my iPhone. I also have a retired Droid that I use as a remote also.

 

There are add-ons for YouTube and other video/music sources. Play around with the options to find the video add-ons you want.

 

Recommended components:

SD card (4GB or larger)

Micro-usb power supply

Wireless keyword with touchpad

WiFi dongle

USB card adapter

Raspberry Pi enclosure

Powered USB hub

HDMI cable

Additional storage for media (USB flash drive, external hard drive, etc…)

Ethernet cable

 

image

Product Name*DescriptionSupplier
Raspberry Pi Model BRaspberry Pi Model BRaspberry Pi model BRaspberry Pi
Buy NowBuy Now
Raspberry Pi Power SupplyRaspberry Pi Power Supply120-240v to 5V power supply with micro USB connectorRaspberry Pi
Buy NowBuy Now
Enclosure for Raspberry PiEnclosure for Raspberry PiClear Plastic enclosure for Raspberry PiMulticomp
Buy NowBuy Now
8GB PNY Class 10 SDHC Card8GB Class 10 high performance SD memory cardPNY
Buy Now
USB 2.0 External Hard DriveUSB 2.0 self-powered external hard drive

Ethernet CableEthernet Cable9.8 ft (3m) category 5e patch cablePro Signal
Buy NowBuy Now
HDMI CableHDMI Cable6.5 ft (2m) male to male standard HDMI cableMolex
Buy NowBuy Now
Wi-PiWi-Pi802.11 b/g/n USB 2.0 Wi-Fi module for Raspberry PiElement 14
Buy NowBuy Now
Mini Wireless USB Keyboard and TrackpadMini Wireless USB Keyboard and TrackpadWireless Mini Keyboard with Trackpad and USB RecieverAdafruit
Buy NowBuy Now
USB 2.0 HubUSB 2.0 Hub7 port self powered USB 2.0 hubAdafruit
Buy NowBuy Now
USB Memory Card Reader56-in-1 USB 2.0 memory card reader / writerIOGear
Buy Now

 

*Products and resources listed are listed to help members build their own Pi Projects. They are suggestions and listed for educational purposes. For substitutions of any parts, please post a question asking the original author.

  • Sign in to reply
  • e14 Contributor
    e14 Contributor over 13 years ago

    Hello Eric,

     

    This is an interesting contribution from where I am sitting.  I am looking into finding a solution for an autonomous device that can get internet radio to my hifi via wireless without paying trough the nose.  There are several solutions off-the-shells out there but I do not need most of the functionality I am paying for...

     

    I am familiar with XBMC as I build a dedicated machine powered by openelec to handle the very large movie collection I have.  XBMC could do the netradio bit, however, I cannot mute my screen (I am still using a CRT television) and consequently, this is not an optimal solution. Unfortunately, on a different note, the system does not stabilise despite the latest updates, so I am on a new quest to find a better solution.

     

    What I really wish for is a tiny device that can live in my stereo amp for that matter (where it gets the power and connects to the aux), that is connected to wifi and can be managed with android / ios devices.  Can raspberry pi do this? Please consider the fact that I am not a developer or programmer and not very keen to fiddle with code too much...

     

    Thanks for your feedback!

     

    Ernest

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    Hi Patrick,

     

    The Android remote will only work if you are running a version of XBMC on the Raspberry Pi. There may be ways to do this with other Linux distros, but I am not familiar with them.

     

    If you are running XBMC, there are several apps in the Android market to choose from. I use the official XBMC remote, although some people prefer others. Search for "xbmc" in the market. The phone and Raspberry Pi need to be connected to the same router for the remote functionality to work.

     

    There is a qwerty keyboard within the remote control app that works well. In regards to skype, it's not possible with XBMC. I believe others have been successful running it on the Pi, but I am not well versed in that topic.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    Eric,

     

    How did you get the android to be a remote? Can you use it for a keyboard also?

     

    I use a wireless keyboard setup at present, but I type much faster with an android. If I had skype on there that's even better. Any ideas?

     

    -Patrick

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<