Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Blog Cheap portable LCD for Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fustini
  • Date Created: 4 Jul 2012 6:36 AM Date Created
  • Views 5847 views
  • Likes 2 likes
  • Comments 25 comments
Related
Recommended
  • raspberry_pi

Cheap portable LCD for Raspberry Pi

fustini
fustini
4 Jul 2012

I've been wanting a small portable display for the Pi.  Unfortunately, portable HDMI displays are quite expensive, and the DSI connector is not an option currently as far as I know.  Then I realized that there a large number of small composite LCDs available which are intended for use in vehicles for backup rearview cameras.  I bought this inexpensive LCD on Amazon, the 3.5 Inch TFT LCD Monitor for Car / Automobile by kingsmart for $21.48 (my order was sold by ePathDirect and fulfilled by Amazon):

imageimage

It arrived today, and I put the photos I took in a Picasa gallery.  I hooked it up to my bench power supply and simply connected it's yellow connector to the composite output on the Pi.  The monitor displayed the Pi's ouptut ok right at power on, through the boot process and beyond.  As I expected, the resolution is poor, especially for small text, given it is standard definition and connected with composite.  However, I'm intending to use this monitor to display tweets, so I can increase the font size as tweets are only 140 characters.  I think this monitor will also be handy for basic troubleshooting when ssh or serial won't suffice, and I don't want to bother with a regular sized monitor.

 

Anyone have any other ideas for inexpensive displays?

 

Cheers,

Drew

  • Sign in to reply

Top Comments

  • sknipas
    sknipas over 14 years ago +1
    I have a 9 inch monitor from an old mini laptop. I also bought a lvds controler from e-bay and I am planning to use this monitor and the r-pi as a car pc. Screen resolution goes up to 1024x600.
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to fustini +1
    It works quite well... But there are some minor disadvantages... 1. you have to concentrate your eyes to have the two displays properly over each other so you have a single image 2. the border region is…
  • jeffbiss
    jeffbiss over 13 years ago in reply to fustini +1
    Now that you mention it, I did the same thing and plumb forgot about it because the screen came with no information! The LCD uses about 5 VDC and has a regulator internally that reduces the car's 12 VDC…
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Very interesting David!

    However I do not find an Ipad Appstore app called TightVNC, but one (presumably with the same functionality) called PC Access;

    is this the one you use or can you guide me to the right one, please?

    Also, do you run a client, (and which) on the Rasberry?

    Thanks,

    Henrik

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    I used my IPad to view the Pi with two methods:

    1) Using tightVNC and the tightVNC ipad app.

    2) Plug the Pi into the sling Box and then transmit it to any client running the slingbox client.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fustini
    fustini over 14 years ago in reply to GeekTinker

    Yup, I'm a big fan of the lapdock! I wrote another post Raspberry Pi laptop.  I think that unless one's project requires a smaller screen, I'd recommend people not waste money on composite LCDs and get the lapdock (while they can still be bought for cheap!).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • GeekTinker
    GeekTinker over 14 years ago

    It's not nearly as small, it does cost a bit more, and you have to hack a few cables, but other threads in this forum have mentioned using the Motorola Atrix 4G Laptop Dock. The upside is that the screen on this device is connected to the Raspberry Pi via HDMI, plus you get a keyboard, a trackpad, and a battery built into it.  I'm sure most people here have seen the youtube video for it from Adafruit.

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image
     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to fustini

    Thats actully really handy as the leads wired into my screen with female RCA's of each are about 8-10" long so they would easily go from the LCD Monitor to my Pi which sits on it little open side/top stand about an inch from the desk top without even moving anything around. That little coupler would save me having 2 meters of cable wound up between the 2 devices.

    Will have to order a couple.

    Thanks for the heads up, I hadn't even thought of using a coupler in place of the only RCA lead I own.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>