Raspberry Pi
  • Products
  • More
Raspberry Pi
Blog External Antenna for Raspberry Pi 4
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: aswinvenu
  • Date Created: 22 Sep 2024 2:56 PM Date Created
  • Views 12703 views
  • Likes 10 likes
  • Comments 13 comments
Related
Recommended
  • raspberry pi 4

External Antenna for Raspberry Pi 4

aswinvenu
aswinvenu
22 Sep 2024

Introduction

     For one of the Raspberry Pi projects I have been working on had this specific requirement for an external antenna. The entire Raspberry Pi 4 needs to be placed inside a metal box. So external antenna was the only option left for me to make the Bluetooth and WiFi to work. I had two choices, One to use the compute module 4 and use the IO board or use a regular RPi and somehow add a UFL/IPEX Connector to the PCB. Considering the cost and availability I preferred to try the second option.

image

    On a closer inspection of the WiFi/BLE Module area, We can see a small provision where a UFL/IPEX Connector can fit. Ofcourse there are no expose pads for an UFL/IPEX connector. We need to create one ( Atleast the ground pads ).

imageimage

Step 1

  Remove the solder mask and prepare a nice and clean exposed copper pad for soldering the UFL/IPEX connector.

image

Step 2

    Cut the trace which goes to the on PCB Antenna and solder a 0201 0E resistor like shown below. 

image

Step 3

   Remove the capacitors used in the PCB Antenna.

image

image

Done! I connected an IPEX 4dB antenna to the my RPi 4 for a quick test.

image

Result

Everything works fine and I am getting roughly 4- 5dB difference compared to the stock PCB antenna.

image

My router was atleast 5-6 meters away from the RPi and there was a wall separation.

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 1 year ago in reply to aswinvenu +2
    That's slightly different, that's unwanted emissions (but also relevant for products for sure). Every country has a regulatory body for wireless, e.g. in the USA it is FCC, and in the UK it is Ofcom (those…
Parents
  • zip00
    zip00 8 months ago

    Hi, can you tell the pourpose to solder a 0ohm resistor between the traces and remove the capacitors used for the PCB Antenna as PCB Antenna is no more used due the trace cut? Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • zip00
    zip00 8 months ago

    Hi, can you tell the pourpose to solder a 0ohm resistor between the traces and remove the capacitors used for the PCB Antenna as PCB Antenna is no more used due the trace cut? Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • aswinvenu
    aswinvenu 8 months ago in reply to zip00

    Out of the box RPi doesn't have a continuous trace running from the antenna output to the IPEX connector. There is a provision for an 0201 0E resistor.

    This is a common technique used in the PCBs if you want to select between external antenna or a PCB/Trace antenna. (ESP32 WROVER boards for example )

    Answering your second question, You don't necessarily need to remove the caps after cutting the trace. I don't have any experimental data supporting one is better than the other. But I would like it to be removed because those 4 caps are part of the PCB antenna structure.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • zip00
    zip00 8 months ago in reply to aswinvenu

    So I will solder a mini piece of wire instead resistor, cut the trace and leave the cups (to leave the possibility of reversibility). Can you confirm that this mod will increase bluetooth signal too?