• Products and Partners
    Products and Partners
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
Raspberry Pi
  • Products and Partners
  • More
Raspberry Pi
Blog Introducing the NEW Raspberry Pi Compute Module
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: lbittner
  • Date Created: 7 Apr 2014 11:59 AM Date Created
  • Views 10255 views
  • Likes 7 likes
  • Comments 25 comments
Related
Recommended
  • raspberry
  • applications
  • raspberry_pi_compute_module_development_kit
  • industrial
  • pi
  • compute
  • embedded
  • raspberry_pi
  • io_board
  • raspberry-pi
  • development
  • kit
  • design-in
  • module

Introducing the NEW Raspberry Pi Compute Module

lbittner
lbittner
7 Apr 2014

Designing in the Future: Raspberry Pi Compute Module Development Kit

 

Coming Summer 2014!

 

The new Raspberry Pi Compute Development Kit enables design engineers

to harness the power of the Raspberry Pi for embedded applications.

 



image

  • Small and Powerful. SODIMM sized (6.5cm by 3cm) Raspberry Pi board contains the BCM2835 chip with 512MB RAM with an on board 4GB eMMC Flash memory for booting the OS.
  • Flexible and Rapid Prototype Development. A fully functional IO board is part of the development kit which supports an extensive GPIO and multiple connectors to help foster rapid prototype development with access to all of the BCM2835 functionality.
  • Custom Hardware and Software Solutions. Benefit from fully functional Linux server running on your ‘design-in’ hardware solution. This unique combination of services will help define the next generation of the ‘Internet of Things’


Compute Module Development Kit Technical Specifications:


Compute Module:

  • SODIMM sized 6.5cm by 3cm board
  • BCM2835 chip with 512MB RAM
  • On board 4GB eMMC Flash memor
  • 200 pin edge connector


IO board:

  • Multiple GPIO interfaces
  • 1 x micro USB connector type B
  • 1 x USB connector type A
  • 2 x CSI ports for camera boards
  • 2 x DSI ports for display boards
  • Full size HDMI port


Harness the power of the Raspberry Pi for your embedded applications!

 

Request Consultation...

Complete this form and one of our Design Representatives will call you to discuss your embedded design.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

See schematics for:

Compute Module

Io Board

  • Sign in to reply

Top Comments

  • raspberrystore
    raspberrystore over 12 years ago in reply to e14 Contributor +2
    Its just who develops an IO-board first, with only ethernet, GPIO (USB?) and power (on the same side). Sadly not me, Id really like to test them!
  • lbittner
    lbittner over 12 years ago in reply to jamodio +1
    Thanks for alerting us, jamodio! The two links will now take you and other members to separate documents. Best, Lauren
  • e14 Contributor
    e14 Contributor over 12 years ago +1
    Ethernet port?
  • e14 Contributor
    e14 Contributor over 12 years ago

    I do not know why Raspberry insist on using Micro USB, and not a barrel, to supply power. The USB 2.0 standard clamps to 500mA. The design requires more than that, up to 750mA at least, to be available.

     

    I would not expect Micro USB to handle 2A or tension. Obviously, nowhere near as robust as the 1/10'th pitch pin headers. 1/10" is overkill for GPIO alone. The digital video in / out interfaces are so much cleaner.

     

    Are we able to use the VCC pin on GPIO headers to supply power, without bypassing the 5v and 3.3v regulators?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    where can I pre-order this

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • raspberrystore
    raspberrystore over 12 years ago in reply to e14 Contributor

    Its just who develops an IO-board first, with only ethernet, GPIO (USB?) and power (on the same side). Sadly not me, Id really like to test them!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    I understand I can add all kind of modules and interfaces via the IO Board. Still I think it's a missed change to not add an Ethernet port to the IO Board. With it it can be used directly for most IoT projects, without it it becomes a stack of add-on boards which makes it vulnerable for errors ...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to jamodio

    jamodio wrote:

     

    When we can pre-order it ?

    and how much will it be?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>