• Products and Partners
    Products and Partners
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
Raspberry Pi
  • Products and Partners
  • More
Raspberry Pi
Blog Introducing the NEW Raspberry Pi Compute Module
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: lbittner
  • Date Created: 7 Apr 2014 11:59 AM Date Created
  • Views 10252 views
  • Likes 7 likes
  • Comments 25 comments
Related
Recommended
  • raspberry
  • applications
  • raspberry_pi_compute_module_development_kit
  • industrial
  • pi
  • compute
  • embedded
  • raspberry_pi
  • io_board
  • raspberry-pi
  • development
  • kit
  • design-in
  • module

Introducing the NEW Raspberry Pi Compute Module

lbittner
lbittner
7 Apr 2014

Designing in the Future: Raspberry Pi Compute Module Development Kit

 

Coming Summer 2014!

 

The new Raspberry Pi Compute Development Kit enables design engineers

to harness the power of the Raspberry Pi for embedded applications.

 



image

  • Small and Powerful. SODIMM sized (6.5cm by 3cm) Raspberry Pi board contains the BCM2835 chip with 512MB RAM with an on board 4GB eMMC Flash memory for booting the OS.
  • Flexible and Rapid Prototype Development. A fully functional IO board is part of the development kit which supports an extensive GPIO and multiple connectors to help foster rapid prototype development with access to all of the BCM2835 functionality.
  • Custom Hardware and Software Solutions. Benefit from fully functional Linux server running on your ‘design-in’ hardware solution. This unique combination of services will help define the next generation of the ‘Internet of Things’


Compute Module Development Kit Technical Specifications:


Compute Module:

  • SODIMM sized 6.5cm by 3cm board
  • BCM2835 chip with 512MB RAM
  • On board 4GB eMMC Flash memor
  • 200 pin edge connector


IO board:

  • Multiple GPIO interfaces
  • 1 x micro USB connector type B
  • 1 x USB connector type A
  • 2 x CSI ports for camera boards
  • 2 x DSI ports for display boards
  • Full size HDMI port


Harness the power of the Raspberry Pi for your embedded applications!

 

Request Consultation...

Complete this form and one of our Design Representatives will call you to discuss your embedded design.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

See schematics for:

Compute Module

Io Board

  • Sign in to reply

Top Comments

  • raspberrystore
    raspberrystore over 12 years ago in reply to e14 Contributor +2
    Its just who develops an IO-board first, with only ethernet, GPIO (USB?) and power (on the same side). Sadly not me, Id really like to test them!
  • lbittner
    lbittner over 12 years ago in reply to jamodio +1
    Thanks for alerting us, jamodio! The two links will now take you and other members to separate documents. Best, Lauren
  • e14 Contributor
    e14 Contributor over 12 years ago +1
    Ethernet port?
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to jamodio

    jamodio wrote:

     

    Seems that the second SD interface (SD1) can be available on the GPIO22-27 pins, so if the hooks are on the kernel it would be possible to add a second SD card socket on the carrier board, leave the bootloader on the eMMC and point to the kernel image on the external SD card.

    Where did you learn this? I would really like to have this ability, but I wasn't able to find any mention of a second SD interface in the BCM2835 datasheet or the Compute Module announcement. Booting from eMMC and using external SD for data would be good for a project I have in mind.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • karlwang
    karlwang over 12 years ago

    And there's another project based on it, on kickstarter: https://www.kickstarter.com/projects/geekroo/como-booster-launch-your-raspberry-pi-compute-modu

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    There is already project based on this module called 'Modberry 500'
    http://linuxgizmos.com/automation-controller-taps-raspberry-pi-compute-module/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    +1 on to when can we pre-order

     

    Also, how do you program the on board eMMC?  At least with a standard card you can put it into a standard machine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to jamodio

    this is the best news i've heard all day, it would be cake to connect an sdcard to gpio. any chance we can get someone to confirm that this would be possible?

     

    myself though, i like the idea of having the 4gb onboard for os and programming and then being able to add a large capacity sdcard for data storage. (i've got me an idea see)

     

    regarding alternate booting though it does say on page 3 of the schematic "BCM2835 will fail to boot from eMMC if EMMC_DISABLE_N is LOW and will therefore fall back to booting from USB." so you should at least be able to use usb.

     

    by any chance could ethernet/wifi also be made available through gpio?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>