Raspberry Pi
  • Products
  • More
Raspberry Pi
Blog Look Ma, no display: Using the Raspberry Pi serial console
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fustini
  • Date Created: 17 Jul 2012 11:23 PM Date Created
  • Views 6170 views
  • Likes 3 likes
  • Comments 8 comments
Related
Recommended
  • rpiintermediate
  • raspi
  • raspberry_pi
  • raspberrypi
  • rpi
  • ftdi

Look Ma, no display: Using the Raspberry Pi serial console

fustini
fustini
17 Jul 2012
imageWant to build this project?
View Parts

 

The serial console is a convenient way to interact with the Raspberry Pi when a display isn't handy.  From the pinout on the eLinux wiki, I can see that the serial port (aka UART) on the Pi is on GPIO Pin 14 (TX) and GPIO Pin 15 (RX):

image

This serial port can be connected to your computer via a USB to serial adapter.  However, these pins are designed for 3.3V (e.g. 3V3), so some USB to serial adapters may damage the Pi.  The simplest option is to use a 3.3V adapter such as:

 

  • FTDI TTL-232R-3V3 cable
  • SparkFun 3.3V Basic FTDI Breakout board

 

Another option is to use a logic level converter (e.g. level shifter).  This will prevent a higher voltage adapter from damaging the Pi's 3.3V pins.  I already had a 5V FTDI cable (TTL-232R-5V) and a SparkFun converter board, so I went this route:

image

Here is the pinout for my TTL-232R-5V cable (datasheet):

image

 

The SparkFun converter board is intended to be used in this configuration:

image

Here's how I wired it all up:

 

Raspberry Pi Pin
Jumper Wire

Logic Level Converter:

LV side (3.3V)

Logic Level Converter:

HV side (5V)

Jumper Wire

FTDI

cable

3V3 PowerRedLVHVRed

Red

(VCC)

GroundGreenGNDGNDGreen

Black

(GND)

TXD

(GPIO 14)

YellowTX1TX0Yellow

Yellow

(RXD)

RXD

(GPIO 15)

BlueRX0RX1Blue

Orange

(TXD)

 

Warning: make sure the Pi is turned off and FTDI cable unplugged from the PC before starting to wire up the above connections

 

Note: TXD (transmit) on the Pi needs to talk to RXD (receive) on FTDI cable, and TXD on the FTDI needs to talk to RXD on the Pi.  Otherwise, it would just be a straight-through connection, and communication wouldn't be possible.

 

Once wired up, power on the Pi and plug the FTDI cable into the PC.  Finally, a terminal emulator application will be needed to connect to the Pi.  I run Ubuntu Linux and already had gtkterm installed.  The program screen is another option for Linux and Mac (OS X).  On Windows, HyperTerm or TeraTerm should work.  The eLinux wiki has additional information.

 

In gtkterm, I selected Configuration->Port and set the Port to /dev/ttyUSB0 and Baud to 115200.  The rest of the defaults are ok (8 bits, stopbits 1, flow control and parity: none).  After clicking OK, I pressed the Enter key a few times and the Pi prompted for username.  I was able to log in and then use the shell as I normally would.  Here is the utility top running:

image

Finally, FTDI has created a cable specifically for the Raspberry Pi: TTL-232R-RPi.  It is available from the UK-based FTDI web shop, but I've not seen it stocked yet by any distributors I'm familiar with.

 

Cheers,

Drew

http://twitter.com/pdp7

 

 

Product Name*DescriptionSupplier
Raspberry Pi Model B Raspberry Pi model BRaspberry Pi
Buy Now
Optical Mouse Basic USB optical mouseIONE / Pro Signal
Buy Now
Raspberry Pi Power Supply 120-240v to 5V power supply with micro USB connectorRaspberry Pi
Buy Now
Keyboard Basic USB keyboardGear Head / A4 Tech
Buy Now
Pre-Programmed 4GB SD Card 4GB Class 4 SD card preloaded with Debian 6 LinuxSamsung
Buy Now
Adafruit Pi Cobbler GPIO breakout kit for Raspberry PiAdafruit Industries
Buy Now
Breadboard Basic breadboard with 830 connection pointsTwin Industries
Buy Now
Jumper wire bundle Jumper wires for use on breadboardBud Industries
Buy Now
FTDI USB-Serial Cable 3.3v USB to serial interface cableFTDI
Buy Now

 

*Products and resources listed are listed to help members build their own Pi Projects. They are suggestions and listed for educational purposes. For substitutions of any parts, please post a question asking the original author.

  • Sign in to reply

Top Comments

  • gpolder
    gpolder over 12 years ago +1
    A cheaper alternative is, using a cell-phone usb cable: http://www.agri-vision.nl/CMS/index.php?option=com_content&view=article&id=32
Parents
  • fustini
    fustini over 12 years ago

    FYI - the Raspberry Pi serial cable from Adafruit simplifies connecting to the console over what I show above:

     

    http://www.adafruit.com/blog/2012/08/02/new-product-usb-to-ttl-serial-cable-debug-console-cable-for-raspberry-pi-raspberrypi-raspberry_pi/

     

    Available from Newark:

    http://www.newark.com/adafruit-industries/954/usb-to-ttl-serial-console-cable/dp/44W3509?Ntt=44W3509

     

    and Farnell:

    http://uk.farnell.com/adafruit-industries/954/usb-ttl-serial-cable-raspberry/dp/2215041

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 12 years ago in reply to fustini

    Many of those "Arduino"  USB serial converters come with some fly cables  so you can connect the corresponding signals to the 'PI.

     

    May need some level shifting with say a resistor or two on the TTL out put or find a 3.3 volt variant !!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Problemchild
    Problemchild over 12 years ago in reply to fustini

    Many of those "Arduino"  USB serial converters come with some fly cables  so you can connect the corresponding signals to the 'PI.

     

    May need some level shifting with say a resistor or two on the TTL out put or find a 3.3 volt variant !!