Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Blog Pico PIO state machine implements a peripheral: CAN - 1: example
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 4 Nov 2022 11:20 PM Date Created
  • Views 13141 views
  • Likes 11 likes
  • Comments 9 comments
Related
Recommended
  • pico
  • pico_eurocard
  • rp2040
  • PIO
  • can

Pico PIO state machine implements a peripheral: CAN - 1: example

Jan Cumps
Jan Cumps
4 Nov 2022

The Pico has a set of PIO co-processors. They are real-time controllers that can execute logic with deterministic timing. Ideal to run strict-timed sequences and state machines. And to implement extra peripherals (like a CAN here).
The PIO engine is not to easy to program, not easy to learn. But there are some great examples out there. I'm reviewing Kevin O'Connor's wonderful can2040 library.
In this post: create a testbed and prove that I can receive CAN traffic.

image

The purpose of this blog isn't to write a PIO developer tutorial. I'm trying to backtrack how the developer implemented a standard protocol using the PIO instructions. I'm using C, CMake, VSCode and the Pico C SDK. Expected skill level: you can build and run the official pico-examples.

In a usual situation (skipping OSI here) CAN has two layers:

  • the logic - TTL, 5V, 3.3V, ... digital, implemented by somethings smart, like a peripheral, controller bit-banging, in this case the PIO state machine.
  • the bus, a physical layer usually implemented with driver/tranceiver ICs. I will use a physical driver IC here, an own little design that I use a lot. 
    You can also make your own Poor Man's CAN Driver, using only common resistors and diodes. 

As communication peers, I use two other CAN capable devices: A Raspberry Pi derivate with a CAN peripheral, and a Microchip CAN Bus analyser. An Arduino (MKR) with CAN shield works too. 

image

This post does not look into the code. It's just a test bed so that I can see if I can set up a CAN conversation. 

Get the can2040 library

Clone or download the sources from Kevin's github. 

git clone https://github.com/KevinOConnor/can2040.git

Set an environment variable that points to this location. This will take care that we can create a make script that's not dependent on where you keep 3rd party code. I'm using VSCode, and will define the environment variable there. You can also do it in your OS settings, shell script, ...

image

Project Folder

I created a directory with a CMake file, and a src folder to contain the very simple test file (taken from here, but I referenced the can2040 sources instead of importing them in the project).

src/main.c

// source: https://gitea.predevolution-technologies.de/anme/CAN2040_Test

#include <stdio.h>
#include <stdint.h>
#include "pico/stdlib.h"
#include "pico/binary_info.h"
#include "hardware/irq.h"
#include "can2040.h"
#include "RP2040.h"

static struct can2040 cbus;

static void can2040_cb(struct can2040 *cd, uint32_t notify, struct can2040_msg *msg)
{
    // Add message processing code here...
}

static void PIOx_IRQHandler(void)
{
    can2040_pio_irq_handler(&cbus);
}

void canbus_setup(void)
{
    uint32_t pio_num = 0;
    uint32_t sys_clock = 125000000, bitrate = 125000;
    uint32_t gpio_rx = 14, gpio_tx = 15;

    // Setup canbus
    can2040_setup(&cbus, pio_num);
    can2040_callback_config(&cbus, can2040_cb);

    // Enable irqs
    irq_set_exclusive_handler(PIO0_IRQ_0_IRQn, PIOx_IRQHandler);
    NVIC_SetPriority(PIO0_IRQ_0_IRQn, 1);
    NVIC_EnableIRQ(PIO0_IRQ_0_IRQn);

    // Start canbus
    can2040_start(&cbus, sys_clock, bitrate, gpio_rx, gpio_tx);
}

int main(void){

    const uint LED_PIN = PICO_DEFAULT_LED_PIN;
    gpio_init(LED_PIN);
    gpio_set_dir(LED_PIN, GPIO_OUT);
    int32_t ledState = 0;
    stdio_init_all();
    
    canbus_setup();

    while(1){
        printf("bla\n");
        gpio_put(LED_PIN, ledState);
        if (ledState == 0){
                ledState = 1;
            }
        else{
            ledState = 0;
        }
        sleep_ms(1000);
    }
}

./CMakeList.txt

cmake_minimum_required(VERSION 3.13)

# Pull in SDK (must be before project)
include(pico_sdk_import.cmake)

project(can2040_project0 C CXX ASM)
set(CMAKE_C_STANDARD 11)
set(CMAKE_CXX_STANDARD 17)

#I've set this to allow breakpoints on any source line
set(PICO_DEOPTIMIZED_DEBUG=1)

pico_sdk_init()


add_executable(can2040_project0
        source/main.c
        $ENV{CAN2040_LIB_PATH}/src/can2040.c
        )

target_include_directories(can2040_project0 PRIVATE
        ${CMAKE_CURRENT_LIST_DIR}/source
        $ENV{CAN2040_LIB_PATH}/src
        )


target_link_libraries(can2040_project0 pico_stdlib cmsis_core)

pico_add_extra_outputs(can2040_project0)

side bar: Pico PIO and other predictive, time critical, co-processors

The Pico PIO state machines are little co-controllers that execute each instruction at a predictable speed.
This type of controllers are never interrupted, don't listen to interrupts (but can fire them). They just clock along reliably and execute their little program.
Usually, they have fast access to some GIO pins.

There are a few other controllers and processors that have similar functionality:
The TI Hercules microcontroller has high-end timers. Very similar to the Pico PIO engines, but the Hercules instruction has additional support for angles, phases, ... (things you use for multi-phase power and for motor driving)
The (also TI) BeagleBone has PRU, a real time programmable unit. Also very close to what the Pico PIO engines have. With direct access to the memory and the DMA engine.
What all 3 have in common, is that they can not only generate well-timed signals. They can also sample input signals. And they are ultra-flexible timers that can handle counts, phase shifts, quadrature encoding, ..)

Testing

I started a debug session, with a breakpoint at the can2040_cb() callback function. From one of my other devices, I sent a CAN message:

image

The RP2040 stops at the breakpoint, and I can see the message ID, DLC (length) and payload:

image

I'm attaching a ZIP of my VSCode project. Don't forget to download the can2040 source and set the environment variable.

can2040_project0_20221104.zip

  • Sign in to reply
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to genebren

    The PIO in this example is advanced. Don't use this one as your first lesson Slight smile.

    I've written another blog, for a rotary controller. (blog in review - I'll post a link later). That one is simpler, because the problem to solve is simpler, and the author uses a known decoding schema - so it's easy to find comparable C , python , vhdl , ... examples for reference of the logic.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 3 years ago

    Very cool!  This is something that I should do a bit of experimenting with.  Maybe someday I will get the time.  Thanks for sharing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to scottiebabe

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to Jan Cumps

    I wish more manufacturers would use Wireshark for the monitoring side of things, since then logging/search/filtering is all ready-made. I've never created a plugin for it, so I don't know about the difficulty though :(

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago

    You CAN do anything! Tada Nice work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>