• Products and Partners
    Products and Partners
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
Raspberry Pi
  • Products and Partners
  • More
Raspberry Pi
Blog Pimoroni Pico Plus 2: A First Look at an RP2350 Board
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 10 Aug 2024 3:21 PM Date Created
  • Views 11694 views
  • Likes 10 likes
  • Comments 23 comments
Related
Recommended
  • RP2350
  • pico2
  • pi pico

Pimoroni Pico Plus 2: A First Look at an RP2350 Board

shabaz
shabaz
10 Aug 2024

I wanted to try to use the new RP2530 microcontroller, but the 'normal' board, the Pi Pico 2, is out of stock for a week or two.

However, there are Pimoroni Pico Plus 2 (what an awkward name) boards, and they were available. I thought they were a drop-in replacement, but there are differences.

Main Improvements compared to Pi Pico 2

  • More storage (16 Mbyte versus 4 Mbyte)
  • More RAM (8 Mbyte vs 0.5 Mbyte),
  • More normal USB connector (USB-C versus micro USB),
  • Integrated reset button.
  • Decent silkscreen, readable from the top side, versus tiny and unreadable on the underside.
  • Five extra GPIO pins are exposed (total of 31 versus 26)

Issues / Annoyances:

  • More than twice the price (£12 vs $5)
  • Debug connector required (3-pin JST-SH, vs normal 2.54mm pin header), an extra £2.10 cost
  • Castellated pads are kind of useless, since there are parts on both sides of the board.
  • There are no 'testpads' on the underside of the board that bring out the USB connections, whereas the Pico 2 has them. It is quite a niche thing, but I mention it, because at least one person (i.e. me) makes use of those.

The photo below shows Pimoroni are using the 80-pin RP2350 chip for this board.

You can see the 3-pin debug connector (which connects to PicoProbe) on the top-right. Below it is a 4-pin connector that carries I2C, 3.3V and GND. The I2C connections are already exposed on a couple of the castellated pads, they are GPIO 4 and GPIO 5.

image

The underside contains the storage, RAM (a PSRAM chip), and an 8-pin JST-SH socket, which carries five extra GPIO (GPIO 32-36), 3.3V and the VSYS (e.g. 5V) and GND signals.

image

Here's the pinout, taken from the Pimoroni website:

image

Summary

The Pimoroni Pico Plus 2 board looks great, but it is not optimal for all projects. There are benefits and disadvantages.

I will definitely find uses for the Pimoroni Pico Plus 2 board, but some of its features will be overkill unless you've got a specific application in mind. If you need extra storage, you could solder a Flash memory chip onto a normal Pico or solder on a micro SD card, so there are workarounds. But it could be very convenient to have the storage and extra RAM all integrated if your project requires it. 

To make the most use out of the board, you'll need a 3-pin JST connector if you want to more easily use the C/C++ SDK or hardware debug features, and an 8-pin JST connector if you need the extra five GPIO connections.

Thanks for reading.

  • Sign in to reply

Top Comments

  • beacon_dave
    beacon_dave over 2 years ago +2
    "...Castellated pads are kind of useless, since there are parts on both sides of the board..." Perhaps design the carrier PCB with a rectangular slot slightly narrower than the width of the board at…
  • Jan Cumps
    Jan Cumps over 2 years ago +2
    castellations with bottom side parts... ... silence
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to shabaz +2
    I'm trying out another option: - keep SDK 1.5x intact - fetch the v2 repos on another location. somewhere on your filesystem: 1: sdk git clone github.com/.../pico-sdk.git cd pico-sdk git checkout…
  • shabaz
    shabaz over 2 years ago in reply to Jan Cumps

    "This certainly looks like a deviation from convention. And a cross-platform trap waiting for its moment to pop up"

    Agree, and also just makes people think they are going down the wrong path, since they start second-guessing if it's really supposed to be an env var, or some parameter to pass on the command line. All-caps at least feels normal : )

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to shabaz

    A mixed case will work in Linux. as long as you use that exact same case when referring to it. $PATH is different than $path

    Windows is case-insensitive. %PATH and %path give the same result. So the picotool_DIR  will work, as long as no other variable conflicts.

    edit: I did a check on a few of my Linux devices, and haven't found any other variable that used mixed (or lower) case. This certainly looks like a deviation from convention. And a cross-platform trap waiting for its moment to pop up

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to shabaz

    There's a recommended method discussed here: 

    https://github.com/raspberrypi/pico-sdk/pull/1820 that uses an environment variable called picotool_DIR, which has now been confirmed working on Linux as can be seen in that thread.

    Hopefully it should work with Windows, although it looks odd seeing an env var that is mixed-case. Come to think of it, I've never noticed any Linux env var being anything other than upper-case either, that was at least a fairly common convention. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to Jan Cumps

    Solved. A more recent native windows compile, and have it on the path, fixes it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to Jan Cumps

    It was a complete nightmare. I've written it up, at the top of the CLion blog  Using CLion for Easier Coding with Pi Pico and C/C++ 

    for picotool. Not tried pioasm with the new SDK yet but will give that a shot. 

    For picotool the solution was pretty ugly, I needed to modify a file in the pico-sdk. Details here:

    https://github.com/raspberrypi/pico-sdk/issues/1818

    I've submitted a PR, no idea if they will accept it, but at least we can manually make the change to the pico-sdk ourselves.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>