Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Blog Add external SPI Flash Memory to Raspberry Pico - 1: hardware
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 19 Nov 2022 3:46 PM Date Created
  • Views 11951 views
  • Likes 9 likes
  • Comments 7 comments
Related
Recommended
  • raspberry
  • pico
  • pico_m25
  • pico_eurocard

Add external SPI Flash Memory to Raspberry Pico - 1: hardware

Jan Cumps
Jan Cumps
19 Nov 2022
Add external SPI Flash Memory to Raspberry Pico - 1: hardware

A projects to learn the SPI API of the RP2040 C SDK, and to use it to control an external Flash IC. In this post, the schematic. 

image

ST Micro M25P16-VMN6P NOR Flash 16MBit

That's the full name of the IC (datasheet). It's a common one - I used a similar one with VHDL during the Summer of FPGA. It talks SPI, with two additional lines for Write Protect and Hold functionality.

image

image

image source: data sheet

Pico pins

pin IC function PICO function GPIO PICO pin
1 S# SPI1 CSn IO9 12 has to be different than the one used by the SD Card, if sharing SPI1
2 DQ1 SPI1 RX IO12 16
3 W# GPIO IO14 19
4 VSS ground 38
5 DQ0 SPI1 TX IO11 15
6 C SPI1 SCK IO10 14
7 HOLD# GPIO IO15 20
8 VCC 3V3 (OUT) 36

I used the EuroCard dev board. The IC is soldered on the SOIC-8 proto area, and the wiring done at the underside. I tapped VSS and VCC from the rotary encoder pads, because they were conveniently nearby.

image

To make probing easy, I also soldered headers.

Next blog: software.

link to all posts in this series

  • Sign in to reply
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to Jan Cumps

    A full conversation:

    image

    command: 9Fh
    manufacturer identification: 20h
    memory type: 20h
    memory size: 15h

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago

    I have troubles writing a blog, but the firmware works. Here's a capture of checking the IC's Read Identification (RDID):

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to colporteur

    sell your tanks. SPI is beginner material.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago

    No success yet. I'm trying to read the 8-bit manufacturer identification of the external SPI EEPROM. Good news is that the SPI traffic looks healthy.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • colporteur
    colporteur over 3 years ago

    JC you're so deep I need tanks. I think it is best I just snorkel on the surface for now. I am excited about your video link. Going to do the intro shortly.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>