• Products and Partners
    Products and Partners
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
Raspberry Pi
  • Products and Partners
  • More
Raspberry Pi
Blog Raspberry PIO stepper library documentation - 5: simple ramp up and down
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 11 May 2025 10:39 AM Date Created
  • Views 3047 views
  • Likes 9 likes
  • Comments 20 comments
Related
Recommended
  • raspberry
  • pico_pio_stepper_lib
  • pico
  • PIO

Raspberry PIO stepper library documentation - 5: simple ramp up and down

Jan Cumps
Jan Cumps
11 May 2025

Raspberry PIO stepper library (pio_stepper_lib) is a C++ library that runs stepper motors in PIO state machines. It's intended to be easy to integrate and use in Pico projects.

In this post: create ramps when motor starts, stops or changes direction.

The stepper motor is controlled by a PIO state machine. The Pico ARM (or RISC) cores are free at that time. While PIO is handling a command, we can use the cores to calculate if the next command is part of a direction change (or stop). And then slow down the motor for a smooth switch.

 image

The ramp logic is part of your firmware. It's not a stepper library function. It shows how you can use the library in complex scenarios, and use the cores to calculate the ideal path while PIO looks after the motor.

Ramp Logic

A stepper motor, when under load or at high speed, performs best if you ramp its stepping speed up and down. A motor will only be able to perform at its maximum, if you give it a little bump to reach. If you don't ramp, your motor may skip steps, overstep, or not step at all. Ramping up and down also makes movements less jerky.

When is a ramp advised?

  • motor start
  • motor changes direction
  • motor stop

Because the stepper library can handle a batch of commands, we can look forward in the command stack to see if we are dealing with a direction change. And because the controller is doing nothing while a motor is running, we can do this exercise for the next command, while we're running the current command. (even if the motor has to do a single step, there's ample time to do this)

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

video: a linear stepper motor executing the example code on repeat. It ramps up and down at start, end, and at direction switching

Border conditions:

We can see inside a stack of commands if we are involved in a direction change, but we don't know how a previous batch ended, or how a new batch will start. That's why the logic has two parameters for first and last commands. If you pass true, the motor will ramp up / down. If you pass false, it will start or end at its high speed.

Software

This is the stack of commands that the motor has to perform:

    std::array<stepper::command, 12> cmd{{
        {10 * microstep_x, false},
        {40 * microstep_x, false},
        {10 * microstep_x, false},
        {10 * microstep_x, true},
        {100 * microstep_x, true},
        {10 * microstep_x, true},
        {10 * microstep_x, false},
        {100 * microstep_x, false},
        {10 * microstep_x, false},
        {10 * microstep_x, true},
        {40 * microstep_x, true},
        {10 * microstep_x, true}}};

I've prepared them for this exercise. The firmware should run every first and last command in a particular direction, at the low (ramp) speed. Commands that are in between other commands in the same direction, should run at high speed. I wrote down the direction of each command, and tried to find a pattern that's easily translated into software.

image

  • x: involved in direction change (previous, next, or both different direction
  • blank: same direction as previous and next
  • !: start or stop: we do what the programmer asks us

I chose this algorithm: If the flags of the before, current and after direction are added up for the next command, and the sum is 0 or 3, there is no direction change. Else there is.

Translated into code:

void run_with_ramp(const commands_t & cmd, uint32_t slow_delay, uint32_t fast_delay, bool start_slow, bool end_slow) {
    bool ramp = start_slow;
    bool next_ramp_found = false;
    unsigned int bits = 0U;

    for (size_t i = 0U; i < cmd.size(); i++) {
        motor1.set_delay(ramp ? slow_delay : fast_delay);
        motor1.take_steps(cmd[i]);
        while (motor1.commands() < 1) {  // motor has to complete before we can send another delay command
            // use motor run time to calculate next speed
            if (! next_ramp_found) {
                ramp = end_slow; // by default, think it's the last command
                if (i < cmd.size() - 2) { // if not, find if dir is changed or will change
                    // check if next command has different direction
                    bits = (cmd[i] & 1) + (cmd[i + 1] & 1) + (cmd[i + 2] & 1); // compare dir bits
                    if (! (bits % 3)) { // in a dir change cycle, unless prev, cur and next command identical
                        ramp = false; // go fast
                    }
                }
                next_ramp_found = true;
            }
        }
        next_ramp_found = false;
        motor1.reset_commands();
    }
}

When you look at the code, take in mind that it always tries to figure out if the next command needs to be ramped.
In that context, cmd[i] (the one that's currently being executed by PIO) is the previous step, cmd[i + 1] is the one we are investigating, and cmd[i + 2] is going to be the step after that.

To run the batch of commands:

run_with_ramp(cmd, 7000, 4300, true, true);

When you add this line in the loop, when the evaluation is done:

printf("next step: %d, checksum: %d, ramp: %s\n", i + 1, bits, bits %3 ? "yes" : "no");

You get this output (step 0 and 11 are determined by the start_slow and end_slow parameters. They aren't shown below):

delays: slow = 7000, fast = 4300
next step: 1, checksum: 3, ramp: no
next step: 2, checksum: 2, ramp: yes
next step: 3, checksum: 1, ramp: yes
next step: 4, checksum: 0, ramp: no
next step: 5, checksum: 1, ramp: yes
next step: 6, checksum: 2, ramp: yes
next step: 7, checksum: 3, ramp: no
next step: 8, checksum: 2, ramp: yes
next step: 9, checksum: 1, ramp: yes
next step: 10, checksum: 0, ramp: no

The oscilloscope capture of DIR (yellow) and STEP (blue) shows the behaviour at a direction change:

image
the black line before the last quarter of the image above is a 1ms pause I intentionally put there in my test code, to get a hint when a batch starts

image
zoom in to a direction change with slow-down before and after. The firmware defines how many steps both part of the ramp last.

This example uses a rough ramp-up: slow speed and high speed. You can define how many slow steps it takes. In many cases that's enough to get the motor going. But there's enough core time available to construct more advanced up- and down-ramps. You could even write an algorithm that pre-analyses a set of commands, and compiles them into a new set with ideal (for your scenario) ramp patterns.

CMake project, with precompiled .uf2 file: pio_a4988_stepper_ramp_20250511.zip

view all posts

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 1 year ago +1
    First attempt for a more trapezoidal(ish) ramp: https://youtu.be/AyNQrvEplDw This (very early) attempt takes core (non-PIO) processor time. How do you ramp, as a library user? {{400 * microstep_x…
  • shabaz
    shabaz over 1 year ago in reply to Jan Cumps

    I think what you mention about a change per X steps sounds realistic, e.g. no more than every 20 steps perhaps, or even every 100 steps. It's quite realistic that several hundred or more steps might simply move a machine by millimeter or so.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to shabaz

    (partial answer - I lost some due to internet issues): I'd have to check if the Pico could manage a speed change per step - and thus provide a very smooth ramp. And if it can: for how many motors in parallel? But may be a nearly-perfect ramp is enough? A speed change per 10 steps, per 50 steps, ...?

    There's a bit of margin: the Pico has two cores, and you can tell which core handles an interrupt (the one that registers it). So if optimisation is required, this would be an enabler.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 1 year ago in reply to Jan Cumps

    Indeed, I think the PIO library already has the functionality it needs, and the next layer must compile up the list in some manner which I don't understand, but must be a solved problem since CNC software exists. I wonder if there's some information format in-between. For instance, something that takes HPGL or Gerber or whatever, and spits out the motor list as a file or something.

    EDIT: Found it I think. https://en.wikipedia.org/wiki/G-code

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to shabaz

    And I've never understood, how does a n-axis machine work, where you may want several motors to be at particular turn counts at the same time, e.g. motor 1 to be at 10.5 turns, and motor 2 to be at 4.6 turns, and then later on, at two different turns values. Would ramping be used, or would one just stick to a slow speed with no ramping? 

    Because step time is deterministic, you can use math to prepare the commands. The PIO allows to start up to 4 motors at exactly the same Pico clock tick. (not that this really matters with motors, where all uncertainties have more impact than a few 100 clock ticks). Also, with PIO code modifications, you can let state machines wait/sync if desired)

    For complex constructs, it may be worth to write an optimiser that takes your wishes, and translates that into steps, speed of those steps, and direction. And feed that to the library. In the end, that's not knowledge that a motor should know - I think that the firmware (or a "business layer") should solve that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to shabaz

    Another theoretical requirement could well be to do an ad-hoc 'abort' and ramp down part-way through a list, if a user hits a button part-way. I can see all of this could get very complicated very quickly though.

    Several ways of doing that:

    • send commands one by one, and stop sending commands when the user asks This could support an "emergency ramp-down".
    • disable the state machine or PIO. This has immediately effect. This could also support an emergency ramp-down, but that's going to require real time PIO conversations. I'm confident it can be done though. You can load new code (say: an emergency pattern) at runtime.

    I deliberately didn't block raw PIO and state machine interaction. It can help in cases like this. (and I use it to change the motor speed at runtime :) )

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>