• Products and Partners
    Products and Partners
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
Raspberry Pi
  • Products and Partners
  • More
Raspberry Pi
Blog Using the PiRack
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Problemchild
  • Date Created: 26 Mar 2014 2:10 AM Date Created
  • Views 1052 views
  • Likes 2 likes
  • Comments 2 comments
Related
Recommended
  • raspberry-pi
  • pirack

Using the PiRack

Problemchild
Problemchild
26 Mar 2014

The PiRack  comes on it's own in an anti static bag with a single sheet of instructions,

there's no need for any more. The overall purpose of the PiRack is really simple

expand the Raspberry Pi's single expansion slot and duplicate it to 4 identical connectors

on the PiRack

image

The PiRack is somewhat taller than the RPi is wide this makes for some stability issues if your Pi

is unsupported  then it's likely to just fall over if you use those upper slots. image

Fullscreen contentimage_30681.html Download
<html><head><title>Jive SBS</title></head>
<body><font face="arial,helvetica,sans-serif">
<b>Error</b><br><font size="-1">
An general error occurred while processing your request.
</font></font></body></html>

Using the lower slots  fine  remember to bolt the Pi down to your project board!

Fullscreen contentimage_30682.html Download
<html><head><title>Jive SBS</title></head>
<body><font face="arial,helvetica,sans-serif">
<b>Error</b><br><font size="-1">
An general error occurred while processing your request.
</font></font></body></html>

This is probably just plain daft don't do it ..remember to support your expansion boards!

 

Other than the 4 expansion connectors the DC jack is the most obvious feature you can supply your boards

5Volt requirements either from the PI or from this jack. Note that this is Unregulated and the any supply used

needs to provide the regulated 5V. Jumpers on the left (JP9-12) allow you to select which power supply

is used on a board by board basis. Many expansion peripherals for the Pi are SPI based, the Pi has two

channels brought out to the expansion connector but most do not allow you to select which channel to

use. This would obviously be a showstopper for running multiple boards if it wasn't for the links provided

on the right of each expansion connector(JP1-8) these allow you to select the SPI channel for each board.

(see table below)

Fullscreen contentimage_30683.html Download
<html><head><title>Jive SBS</title></head>
<body><font face="arial,helvetica,sans-serif">
<b>Error</b><br><font size="-1">
An general error occurred while processing your request.
</font></font></body></html>

 

Fullscreen contentimage_30684.html Download
<html><head><title>Jive SBS</title></head>
<body><font face="arial,helvetica,sans-serif">
<b>Error</b><br><font size="-1">
An general error occurred while processing your request.
</font></font></body></html>

Obviously been able to swap the CS lines allows boards to use both SPI ports but does not

increase the number of channels so in many instances you can only have 2 boards in use anyway

and also the driver software for the board also needs to know that the device is now on the other channel!

 

Other Use Cases!!!

     I have found the rack to be more useful to me in working on new prototype boards allowing me to

separatelypower the board(s) whilst most importantly gain access to the pins on the expansion port

so I can diagnose problems using my scope/logic analyser etc. Gaining access to the expansion slot

whilst having a prototype already installed would simply be too awkward without the PiRack.

reason alone

image

PiRack saves the day this alone is well worth the £8!!!!


PiRack is available from Farnell/E14, if you are doing any dev work with the Pi it's well worth the click!!

  • Sign in to reply
  • Problemchild
    Problemchild over 12 years ago in reply to shabaz

    Personally I think the ease of access when making stuff is really it's main feature Shabaz.

    It's a bit awkward to use if you are going to stack more than two boards and really

    you need to have some form of base on the Pi to stop it falling over

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 12 years ago

    Using this board for prototyping and testing is a great idea.

    So far I've been just half-plugging in boards to SBCs to be able to get at the pins from the sides, but that method is flaky at best and the probes unclip by themselves regularly : ( There were headers and sockets with long pins (for wire-wrap) but they are not cheap. Also with this board, while prototyping the extra pins on the unused headers for 0V and supply would help too.