Raspberry Pi
  • Products
  • More
Raspberry Pi
Blog Why Should the RP2040 MCU be Specified in Your Next Design? The Heart of the Raspberry Pi Pico
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: cstanton
  • Date Created: 11 Jan 2023 12:39 PM Date Created
  • Views 6075 views
  • Likes 13 likes
  • Comments 24 comments
Related
Recommended
  • Rapid development and deployment
  • raspberry pi pico
  • Microcontroller-based applications
  • Arm Cortex-M0+
  • rp2040
  • mcu
  • Programmable I/O

Why Should the RP2040 MCU be Specified in Your Next Design? The Heart of the Raspberry Pi Pico

cstanton
cstanton
11 Jan 2023
RP2040 Chip Close-Up

It is a challenge to design low-cost microcontroller-based applications. The designer must balance power and performance with price. It is difficult to decide which instruction set architecture is the best fit for the application. Design and manufacturing concerns also come into play: who will design the system, and who will fabricate it? The answers determine the value and cost-effectiveness of the end product. In this context, the price-to-performance ratio of the RP 2040 microcontroller makes it an obvious choice for the Raspberry Pi Pico. 

What are the specifications of the RP2040 and the Pi Pico?

The RP2040  SoC is a powerful, low-cost microcontroller packing a dual-core Arm® Cortex-M0+ processor that clocks in at a decent 133MHz. It is one of the most energy-saving Arm® processors available. The microcontroller has six banks crammed with 264 kB of embedded SRAM. The RP2040 SoC consumes a low amount of power but yields high performance with minimum leakage.

The Raspberry Pi Pico  board operates over a wide ~1.8 to 5.5V input voltage range and comes with different low-power modes that support battery-powered operation for extended durations. The RP2040 has 30 GPIO pins (four for analogue input), two SPI and I2C controllers, two UART and 16 PWM channels, one USB 1.1 controller, and eight Programmable I/O (PIO). You can set pins opposite the Micro-USB port and connect another Raspberry Pi to program the board directly. The uploaded program automatically runs when turned on.

Raspberry Pi Pico on a breadboard

Fig. 1: Temperature and humidity monitoring using Raspberry Pi PICO (Source)

Figure 1 represents a room temperature monitoring system based on the Raspberry Pi Pico board. This application uses Pico’s internal storage to store the data. The data is given a time stamp and stored in a new line format, thus saving the cost of an external SD card module and memory card. Pico gives you the freedom to select the file type, allowing you to store the data in a user-friendly format. It also eliminates the need for proprietary libraries or drivers.

The RP2040 allows rapid code generation in MicroPython or C/C++ with your preferred IDE. The result is a unique platform that supports the rapid development and deployment of endpoint Artificial Intelligence (AI) based applications. You can use TinyML to implement machine learning (ML) models such as voice or image recognition and accelerometer-based gesture recognition or gearbox fault prediction.


Arduino versus the Raspberry Pi Pico - Which to Go For?

Arduino, a microcontroller, is an open-source prototype platform that enables users to create interactive electronic projects. The arrival of the new RP2040 SoC and the Raspberry Pi Pico microcontroller has blurred the line between the Raspberry Pi (a mini-computer) and Arduino ecosystems.

Raspberry Pi Pico uses the improved RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller RP2040 microcontroller . The Arm® Cortex M0+ in the RP2040 runs at a much faster speed than the Arduino UNO's 16 MHz Atmega328P. The RP2040’s 264 kB SRAM and 2 MB of flash storage are much greater than the Arduino Uno’s 2 kB SRAM and 32 kB flash memory.

Both the Pico and Uno can interact with sensors, motors, display devices, and other physical devices. The Uno operates at 5 V, with six analogue input pins and 14 digital pins for general-purpose input/output (GPIO). Out of 14 pins, six provide PWM output. The Pico operates at 3.3 V, with 26 GPIO pins. The analogue inputs use four pins, and the PWM outputs 16 out of 26 pins. The Pico has an edge on analogue-to-digital conversion (ADC), a faster sampling rate (500 kHz vs. 125 kHz), and a greater resolution (12-bit vs. 10-bit).

The use of serial communication is on the rise in peripheral devices. For example, the Uno has one channel for each UART, I2C, and SPI functionality, while the Pico has twice this number. Pico's programmable IO (PIO) feature supports user-programmable high-speed IO to do tasks such as video output implementation. PIO enables the SD card to interface with software at the hardware level efficiently.

You can code the Arduino Uno in C++ "sketches." The Arduino IDE processes and then compiles and loads the machine code onto the board. In contrast, the RP2040 uses MicroPython, a version of the Python language for small devices. Beginners can use MicroPython for easier and faster coding, while more advanced users have their preference for MicroPython or C/C++.

Have you made your Decision?

The powerful processor and rich functionality of the RP2040 make it a compelling entry into the MCU market. Combined with MicroPython programming, the RP2040 offers an easily accessible gateway for people who want to explore physical computing and microcontrollers at a low cost. The technology, with high-quality documentation and development tools, enables a new generation of hardware and software developers to fill the skills gap in a rapidly growing market.

  • Sign in to reply

Top Comments

  • michaelkellett
    michaelkellett over 3 years ago +1
    I think I should correct a matter of detail on current consumption of the RP2040. One of the key differences between it and most other "low power" ARM M0 based microcontrollers is that it has no on chip…
  • misaz
    misaz over 3 years ago +1
    For me it is mainly cost, in-stock availability at distributors and PIO, but there are several disadvantages when using this MCU like need for external Flash.
  • Jan Cumps
    Jan Cumps over 3 years ago

    After using these for a few months now, my favourites

    Hardware:

    • The ways the two cores can interact (or be segregated)

    Software:

    • The c sdk
    • The dual core FreeRTOS port
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to cstanton

    Hehe that's similar to what I want to use it for! It could make the Pi Pico really handy for pulling information off loads of modern electronics. I was going to use a level converter, but since the RP2040 can support 1.8V I/O, it could be nice to have such a version, especially because bidirectional level converters get awkward to use for some serial buses.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to shabaz

    (Can't edit. It's MAX19777. Image source: Google Images).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to beacon_dave

    Interesting situation is that it's currently far cheaper (at least on Farnell website) to buy a 500MSPS or higher 12-bit ADC than 10-bit ADCs (which are all likely still better than the one in the Pico). 

    This one looks interesting:

    image

    For about £1.80, it has two multiplexed inputs, is 12-bit, and 2MSPS (and also looks easy to drive). But it's tiny, the pin spacing is 0.35 mm : ) The width of the entire chip is less than a millimetre basically. However, this might actually be manageable since it's not a lot of pins. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 3 years ago

    I have yet used the RP2040.

    I like the Arduino for quick project testing because it is fast enough and most of my other tools are 5V devices.

    I have been following the posts for RP2040 projects and if I need that extra power, I might break down and try one, though I have several RPI 2, 3 and 4 boards around, so having A/D capability is a plus.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>